![]() |
![]() |
|
BLE-Stack APIs
3.00.00
|
GAPBondMgr layer interface.
Go to the source code of this file.
Data Structures | |
| struct | gapBondEccKeys_t |
| Public and Private ECC Keys. More... | |
| struct | gapBondOobSC_t |
| Secure Connections Out of Band. More... | |
Macros | |
| #define | ECC_KEYLEN 32 |
| 256 bit keys | |
| #define | GAP_BONDINGS_MAX 10 |
| Maximum number of bonds that can be saved in NV. | |
| #define | GAP_CHAR_CFG_MAX 4 |
| Maximum number of characteristic configuration that can be saved in NV. | |
| #define | GAPBOND_AUTO_SYNC_WL 0x40D |
| Synchronize the whitelist with bonded devices (Read/Write) More... | |
| #define | GAPBOND_BOND_COUNT 0x40E |
| Gets the total number of bonds stored in NV (Read-only) More... | |
| #define | GAPBOND_BOND_FAIL_ACTION 0x40F |
| The action that the device takes after an unsuccessful bonding attempt (Write-only) More... | |
| #define | GAPBOND_BONDING_ENABLED 0x406 |
| Whether to request bonding during pairing (Read/Write) More... | |
| #define | GAPBOND_DEFAULT_PASSCODE 0x408 |
| The default passcode to use for passcode pairing (Read/Write) More... | |
| #define | GAPBOND_ECC_KEYS 0x413 |
| The private and public keys to use for Secure Connections pairing (Read/Write) More... | |
| #define | GAPBOND_ECCKEY_REGEN_POLICY 0x412 |
| ECC Key Regeneration Policy (Read/Write) More... | |
| #define | GAPBOND_ERASE_ALLBONDS 0x409 |
| Erase all bonds from SNV and remove all bonded devices (Write) More... | |
| #define | GAPBOND_ERASE_SINGLEBOND 0x410 |
| Erase a single bonded device (Write-only) More... | |
| #define | GAPBOND_FAIL_INITIATE_PAIRING 0x01 |
| Initiate pairing upon unsuccessful bonding. | |
| #define | GAPBOND_FAIL_NO_ACTION 0x00 |
| Take no action upon unsuccessful bonding. | |
| #define | GAPBOND_FAIL_TERMINATE_ERASE_BONDS 0x03 |
| Terminate link and erase all existing bonds on device upon unsuccessful bonding. | |
| #define | GAPBOND_FAIL_TERMINATE_LINK 0x02 |
| Terminate link upon unsuccessful bonding. | |
| #define | GAPBOND_INITIATE_WAIT 0x401 |
| The amount of time (in ms) to wait for a pairing request before sending the slave initiate request (Read/Write) More... | |
| #define | GAPBOND_IO_CAP_DISPLAY_ONLY 0x00 |
| Display Only Device. | |
| #define | GAPBOND_IO_CAP_DISPLAY_YES_NO 0x01 |
| Display and Yes and No Capable. | |
| #define | GAPBOND_IO_CAP_KEYBOARD_DISPLAY 0x04 |
| Both Keyboard and Display Capable. | |
| #define | GAPBOND_IO_CAP_KEYBOARD_ONLY 0x02 |
| Keyboard Only. | |
| #define | GAPBOND_IO_CAP_NO_INPUT_NO_OUTPUT 0x03 |
| No Display or Input Device. | |
| #define | GAPBOND_IO_CAPABILITIES 0x403 |
| The I/O capabilities of the local device (Read/Write) More... | |
| #define | GAPBOND_KEY_DIST_LIST 0x407 |
| Key distribution list for pairing (Read/Write) More... | |
| #define | GAPBOND_KEYDIST_MENCKEY 0x10 |
| Master Encrypton Key. | |
| #define | GAPBOND_KEYDIST_MIDKEY 0x20 |
| Master IRK and ID information. | |
| #define | GAPBOND_KEYDIST_MLINK 0x80 |
| Master Link Key. | |
| #define | GAPBOND_KEYDIST_MSIGN 0x40 |
| Master CSRK. | |
| #define | GAPBOND_KEYDIST_SENCKEY 0x01 |
| Slave Encryption Key. | |
| #define | GAPBOND_KEYDIST_SIDKEY 0x02 |
| Slave IRK and ID information. | |
| #define | GAPBOND_KEYDIST_SLINK 0x08 |
| Slave Link Key. | |
| #define | GAPBOND_KEYDIST_SSIGN 0x04 |
| Slave CSRK. | |
| #define | GAPBOND_KEYSIZE 0x40C |
| Key Size used in pairing. (Read/Write) More... | |
| #define | GAPBOND_LOCAL_OOB_SC_DATA 0x417 |
| Local OOB Secure Connections Data (Read/Write) More... | |
| #define | GAPBOND_LOCAL_OOB_SC_ENABLED 0x416 |
| Validate Local OOB Secure Connections Data (Read/Write) More... | |
| #define | GAPBOND_LRU_BOND_REPLACEMENT 0x418 |
| Enable / Disable LRU Bond Replacement Scheme (Read/Write) More... | |
| #define | GAPBOND_MITM_PROTECTION 0x402 |
| Whether to use authenticated pairing (Read/Write) More... | |
| #define | GAPBOND_OOB_DATA 0x405 |
| OOB data to use for pairing (Read/Write) More... | |
| #define | GAPBOND_OOB_ENABLED 0x404 |
| Whether to use OOB for pairing (Read/Write) More... | |
| #define | GAPBOND_PAIRING_MODE 0x400 |
| Whether to allow pairing, and if so, whether to initiate pairing. (Read/Write) More... | |
| #define | GAPBOND_PAIRING_MODE_INITIATE 0x02 |
| Don't wait, initiate a pairing request or slave security request. | |
| #define | GAPBOND_PAIRING_MODE_NO_PAIRING 0x00 |
| Pairing is not allowed. | |
| #define | GAPBOND_PAIRING_MODE_WAIT_FOR_REQ 0x01 |
| Wait for a pairing request or slave security request. | |
| #define | GAPBOND_PAIRING_STATE_BOND_SAVED 0x03 |
| Bonding record saved in NV. | |
| #define | GAPBOND_PAIRING_STATE_BONDED 0x02 |
| Bonding Complete. More... | |
| #define | GAPBOND_PAIRING_STATE_CAR_READ 0x04 |
| Central Address Resolution Characteristic Read. | |
| #define | GAPBOND_PAIRING_STATE_COMPLETE 0x01 |
| Pairing Complete. More... | |
| #define | GAPBOND_PAIRING_STATE_STARTED 0x00 |
| Pairing Started. More... | |
| #define | GAPBOND_REGENERATE_ALWAYS 0x00 |
| Regenerate after each usage. | |
| #define | GAPBOND_REGENERATE_NEVER 0xFF |
| Never regenerate, always use the same pair. | |
| #define | GAPBOND_REMOTE_OOB_SC_DATA 0x415 |
| Remote OOB Secure Connections Data (Read/Write) More... | |
| #define | GAPBOND_REMOTE_OOB_SC_ENABLED 0x414 |
| Validate Remote OOB Secure Connections Data (Read/Write) More... | |
| #define | GAPBOND_SECURE_CONNECTION 0x411 |
| Define Secure Connections Usage during Pairing (Read/Write) More... | |
| #define | GAPBOND_SECURE_CONNECTION_ALLOW 0x01 |
| Secure Connections are supported. | |
| #define | GAPBOND_SECURE_CONNECTION_NONE 0x00 |
| Secure Connections not supported. | |
| #define | GAPBOND_SECURE_CONNECTION_ONLY 0x02 |
| Secure Connections Only Mode. | |
| #define | SMP_PAIRING_FAILED_AUTH_REQ 0x03 |
| The pairing procedure can't be performed as authentication requirements can't be met due to IO capabilities of one or both devices. | |
| #define | SMP_PAIRING_FAILED_CMD_NOT_SUPPORTED 0x07 |
| The SMP command received is not supported on this device. | |
| #define | SMP_PAIRING_FAILED_CONFIRM_VALUE 0x04 |
| The confirm value doesn't match the calculated compare value. | |
| #define | SMP_PAIRING_FAILED_DHKEY_CHECK_FAILED 0x0B |
| Indicates to the remote device that the DHKey Check value received does not match the one calculated by the local device. | |
| #define | SMP_PAIRING_FAILED_ENC_KEY_SIZE 0x06 |
| The resultant encryption key size is insufficient for the security requirements of this device. | |
| #define | SMP_PAIRING_FAILED_INVALID_PARAMETERS 0x0A |
| Indicates that the command length is invalid or that a parameter is outside of the specified range. | |
| #define | SMP_PAIRING_FAILED_NOT_SUPPORTED 0x05 |
| Pairing isn't supported by the device. | |
| #define | SMP_PAIRING_FAILED_NUM_COMPARISON_FAILED 0x0C |
| Indicates that the confirm value in the numeric comparison protocol do not match. | |
| #define | SMP_PAIRING_FAILED_OOB_NOT_AVAIL 0x02 |
| The OOB data is not available. | |
| #define | SMP_PAIRING_FAILED_PASSKEY_ENTRY_FAILED 0x01 |
| The user input of the passkey failed, for example, the user cancelled the operation. | |
| #define | SMP_PAIRING_FAILED_REPEATED_ATTEMPTS 0x09 |
| Pairing or authentication procedure is disallowed because too little time has elapsed since the last pairing request or security request. | |
| #define | SMP_PAIRING_FAILED_UNSPECIFIED 0x08 |
| Pairing failed due to an unspecified reason. | |
Typedefs | |
| typedef void(* | pfnPairStateCB_t )(uint16 connectionHandle, uint8 state, uint8 status) |
| Pairing State Callback Function. More... | |
| typedef void(* | pfnPasscodeCB_t )(uint8 *deviceAddr, uint16 connectionHandle, uint8 uiInputs, uint8 uiOutputs, uint32 numComparison) |
| Passcode and Numeric Comparison Callback Function. More... | |
Functions | |
| uint8 | GAPBondMgr_CheckNVLen (uint8 id, uint8 len) |
| This function will check the length of a Bond Manager NV Item. More... | |
| bStatus_t | GAPBondMgr_GetParameter (uint16 param, void *pValue) |
| Get a GAP Bond Manager parameter. More... | |
| bStatus_t | GAPBondMgr_LinkEst (uint8 addrType, uint8 *pDevAddr, uint16 connHandle, uint8 role) |
| Notify the Bond Manager that a connection has been made. More... | |
| void | GAPBondMgr_LinkTerm (uint16 connHandle) |
| Notify the Bond Manager that a connection has been terminated. More... | |
| bStatus_t | GAPBondMgr_PasscodeRsp (uint16 connectionHandle, uint8 status, uint32 passcode) |
| Respond to a passcode request. More... | |
| uint8 | GAPBondMgr_ProcessGAPMsg (gapEventHdr_t *pMsg) |
| This is a bypass mechanism to allow the bond manager to process GAP messages. More... | |
| bStatus_t | GAPBondMgr_ReadCentAddrResChar (uint16 connectionHandle) |
| Read Central Address Resolution Characteristic. More... | |
| void | GAPBondMgr_Register (gapBondCBs_t *pCB) |
| Register callback functions with the bond manager. More... | |
| uint8 | GAPBondMgr_ResolveAddr (uint8 addrType, uint8 *pDevAddr, uint8 *pResolvedAddr) |
| Resolve an address from bonding information. More... | |
| bStatus_t | GAPBondMgr_ServiceChangeInd (uint16 connectionHandle, uint8 setParam) |
| Set/clear the service change indication in a bond record. More... | |
| bStatus_t | GAPBondMgr_SetParameter (uint16 param, uint8 len, void *pValue) |
| Set a GAP Bond Manager parameter. More... | |
| void | GAPBondMgr_SlaveReqSecurity (uint16 connHandle, uint8 authReq) |
| Notify the Bond Manager that a Slave Security Request is received. More... | |
| uint8 | GAPBondMgr_SupportsEnhancedPriv (uint8 *pPeerIdAddr) |
| Determine if peer device supports enhanced privacy by checking the Enhanced Privacy state flag of the bond record that corresponds to the peer's identity address. More... | |
| bStatus_t | GAPBondMgr_syncResolvingList (void) |
| This function will add all device address and IRK pairs from bond records to the Controller. Used with PRIVACY_1_2_CFG. More... | |
| bStatus_t | GAPBondMgr_UpdateCharCfg (uint16 connectionHandle, uint16 attrHandle, uint16 value) |
| Update the Characteristic Configuration in a bond record. More... | |