![]() |
![]() |
Macros | |
| #define | SDSPI_STATUS_SUCCESS (0) |
| Successful status code returned by SDSPI_control(). More... | |
| #define | SDSPI_STATUS_ERROR (-1) |
| Generic error status code returned by SDSPI_control(). More... | |
| #define | SDSPI_STATUS_UNDEFINEDCMD (-2) |
| An error status code returned by SDSPI_control() for undefined command codes. More... | |
SDSPI_STATUS_* macros are general status codes returned by SDSPI_control()
| #define SDSPI_STATUS_SUCCESS (0) |
Successful status code returned by SDSPI_control().
SDSPI_control() returns SDSPI_STATUS_SUCCESS if the control code was executed successfully.
| #define SDSPI_STATUS_ERROR (-1) |
Generic error status code returned by SDSPI_control().
SDSPI_control() returns SDSPI_STATUS_ERROR if the control code was not executed successfully.
| #define SDSPI_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by SDSPI_control() for undefined command codes.
SDSPI_control() returns SDSPI_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.