![]() |
![]() |
AESCCM driver header.
============================================================================
The Counter with CBC-MAC (CCM) mode of operation is a generic authenticated encryption block cipher mode. It can be used with any 128-bit block cipher. AESCCM combines CBC-MAC with an AES block cipher in CTR mode of operation.
This combination of block cipher modes enables CCM to encrypt messages of any length and not only multiples of the block cipher block size.
AESCCM encryption has the following inputs and outputs:
| Encryption | Decryption |
|---|---|
| Input | |
| Shared AES key | Shared AES key |
| Nonce | Nonce |
| Cleartext | Ciphertext (encrypted plaintext + MAC) |
| AAD (optional) | AAD (optional) |
| Output | |
| Ciphertext (encrypted plaintext + MAC) | Cleartext |
The AES key is a shared secret between the two parties and has a length between 128 and 256 bits.
The nonce is generated by the party performing the authenticated encryption operation. Within the scope of any authenticated encryption key, the nonce value must be unique. That is, the set of nonce values used with any given key must not contain any duplicate values. Using the same nonce for two different messages encrypted with the same key destroys the security properties.
The optional additional authentication data (AAD) is authenticated, but not encrypted. Thus, the AAD is not included in the AES-CCM output. It can be used to authenticate packet headers.
After the encryption operation, the ciphertext contains the encrypted data and the message authentication code (MAC). The MAC can be seen as an encrypted fingerprint of the message header and content.
Before starting a CCM operation, the application must do the following:
There are two general ways to execute a CCM operation. In one call or multiple.
The AESCCM_oneStepEncrypt and AESCCM_oneStepDecrypt functions do a CCM operation in a single call. They will always be the most highly optimized routines with the least overhead and the fastest runtime. However, they require all AAD and plaintext or ciphertext data to be available to the function at the start of the call. When trying to operate on data that is too large to fit into available memory, partial processing would be more advisable. All devices support single call operations. When performing a decryption operation with AESCCM_oneStepDecrypt(), the MAC is automatically verified when using AESCCM_RETURN_BEHAVIOR_BLOCKING or AESCCM_RETURN_BEHAVIOR_POLLING. When using AESCCM_RETURN_BEHAVIOR_CALLBACK however, the application's registered callback function must call AESCCM_verifyMac() itself to ensure that the computed and transmitted MACs match.
The partial processing functions split the setup, processing of the AAD, processing of the plaintext or ciphertext, and computation or verification of the MAC into multiple calls. The AAD and payload processing functions may be called on buffers smaller than the total AAD and payload sizes. Not all devices support partial processing. The hardware or software implementations of the CCM mode of operation available on a specific device may not be designed to support partial processing.
After the CCM operation completes, the application should either start another operation or close the driver by calling AESCCM_close()
In order to use the AESCCM APIs, the application is required to provide device-specific AESCCM configuration in the Board.c file. The AESCCM driver interface defines a configuration data structure:
The application must declare an array of AESCCM_Config elements, named AESCCM_config[]. Each element of AESCCM_config[] must be populated with pointers to a device specific AESCCM driver implementation's driver object and hardware attributes. The hardware attributes define properties such as the AESCCM peripheral's base address. Each element in AESCCM_config[] corresponds to an AESCCM instance and none of the elements should have NULL pointers. There is no correlation between the index and the peripheral designation (such as AESCCM0 or AESCCM1). For example, it is possible to use AESCCM_config[0] for AESCCM1. Multiple drivers and driver instances may all access the same underlying hardware. This is transparent to the application. Mutual exclusion is performed automatically by the drivers as necessary.
Because the AESCCM configuration is very device dependent, you will need to check the doxygen for the device specific AESCCM implementation. There you will find a description of the AESCCM hardware attributes. Please also refer to the Board.c file of any of your examples to see the AESCCM configuration.
The AESCCM_Params structure is passed to the AESCCM_open() call. If NULL is passed for the parameters, AESCCM_open() uses default parameters. A AESCCM_Params structure is initialized with default values by passing it to AESCCM_Params_init(). Some of the AESCCM parameters are described below. To see brief descriptions of all the parameters, see AESCCM_Params.
The AESCCM driver supports three return behaviors when processing data: blocking, polling, and callback. The return behavior is determined by the returnBehavior parameter in the AESCCM_Params data structure. The AESCCM driver defaults to blocking mode, if the application does not set it. Once an AESCCM driver is opened, the only way to change the return behavior is to close and re-open the AESCCM instance with the new return behavior.
In blocking mode, a task's code execution is blocked until an AESCCM operation has completed. This ensures that only one AESCCM operation operates at a given time. Other tasks requesting AESCCM operations while a operation is currently taking place are also placed into a blocked state. AESCCM operations are executed in the order in which they were received. In blocking mode, you cannot perform AESCCM operations in the context of a software or hardware ISR.
In callback mode, an AESCCM operation functions asynchronously, which means that it does not block code execution. After an AESCCM operation has been completed, the AESCCM driver calls a user-provided hook function. Callback mode is supported in the task, SWI, and HWI execution context, However, if an AESCCM operation is requested while a operation is taking place, the call returns an error code.
In polling mode, an AESCCM operation behaves the almost the same way as in blocking mode. Instead of pending on a semaphore and letting other scheduled tasks run, the application task, SWI, or HWI continuously polls a flag until the operation completes. If an AESCCM operation is requested while a operation is taking place, the call returns an error code. When starting an AESCCM operation in polling mode from HWI or SWI context, the AESCCM HWI and SWI must be configured to have a higher priority to pre-empt the polling context.
### Single call CCM encryption + authentication with plaintext CryptoKey in blocking return mode #
#include <stdbool.h>#include <stddef.h>#include <stdint.h>#include <ti/drivers/cryptoutils/cryptokey/CryptoKey.h>Go to the source code of this file.
Data Structures | |
| struct | AESCCM_Params_ |
| CCM Parameters. More... | |
| struct | AESCCM_Config_ |
| AESCCM Global configuration. More... | |
Macros | |
| #define | AESCCM_CMD_RESERVED (32) |
| #define | AESCCM_STATUS_RESERVED (-32) |
| #define | AESCCM_STATUS_SUCCESS (0) |
| Successful status code. More... | |
| #define | AESCCM_STATUS_ERROR (-1) |
| Generic error status code. More... | |
| #define | AESCCM_STATUS_UNDEFINEDCMD (-2) |
| An error status code returned by AESCCM_control() for undefined command codes. More... | |
| #define | AESCCM_STATUS_RESOURCE_UNAVAILABLE (-3) |
| An error status code returned if the hardware or software resource is currently unavailable. More... | |
| #define | AESCCM_STATUS_MAC_INVALID (-4) |
| An error status code returned if the MAC provided by the application for a decryption operation does not match the one calculated during the operation. More... | |
Typedefs | |
| typedef struct AESCCM_Config_ * | AESCCM_Handle |
| A handle that is returned from an AESCCM_open() call. More... | |
| typedef void(* | AESCCM_CallbackFxn) (AESCCM_Handle handle, CryptoKey *processedKey) |
| The definition of a callback function used by the AESCCM driver when used in AESCCM_RETURN_BEHAVIOR_CALLBACK. More... | |
| typedef enum AESCCM_ReturnBehavior_ | AESCCM_ReturnBehavior |
| The way in which CCM function calls return after performing an encryption + authentication or decryption + verification operation. More... | |
| typedef enum AESCCM_Mode_ | AESCCM_Mode |
| Enum for the direction of the CCM operation. More... | |
| typedef struct AESCCM_Params_ | AESCCM_Params |
| CCM Parameters. More... | |
| typedef struct AESCCM_Config_ | AESCCM_Config |
| AESCCM Global configuration. More... | |
Enumerations | |
| enum | AESCCM_ReturnBehavior_ { AESCCM_RETURN_BEHAVIOR_CALLBACK = 1, AESCCM_RETURN_BEHAVIOR_BLOCKING = 2, AESCCM_RETURN_BEHAVIOR_POLLING = 4 } |
| The way in which CCM function calls return after performing an encryption + authentication or decryption + verification operation. More... | |
| enum | AESCCM_Mode_ { AESCCM_MODE_ENCRYPT = 1, AESCCM_MODE_DECRYPT = 2 } |
| Enum for the direction of the CCM operation. More... | |
Functions | |
| void | AESCCM_init (void) |
| This function initializes the CCM module. More... | |
| void | AESCCM_Params_init (AESCCM_Params *params) |
| Function to initialize the AESCCM_Params struct to its defaults. More... | |
| AESCCM_Handle | AESCCM_open (uint_least8_t index, AESCCM_Params *params) |
| This function opens a given CCM peripheral. More... | |
| void | AESCCM_close (AESCCM_Handle handle) |
| Function to close a CCM peripheral specified by the CCM handle. More... | |
| int_fast16_t | AESCCM_control (AESCCM_Handle handle, uint32_t cmd, void *args) |
| Function performs implementation specific features on a given AESCCM_Handle. More... | |
| int_fast16_t | AESCCM_setupEncrypt (AESCCM_Handle handle, CryptoKey *key, uint8_t *nonce, uint8_t nonceLength, size_t aadTotalLength, size_t plaintextTotalLength, uint8_t macLength) |
| Function to set up an AESCCM encryption + authentication operation in multiple calls. More... | |
| int_fast16_t | AESCCM_setupDecrypt (AESCCM_Handle handle, CryptoKey *key, uint8_t *nonce, uint8_t nonceLength, size_t aadTotalLength, size_t ciphertextTotalLength, uint8_t macLength) |
| Function to set up an AESCCM decryption + verification operation in multiple calls. More... | |
| int_fast16_t | AESCCM_processAAD (AESCCM_Handle handle, uint8_t *aad, size_t length) |
| Function to process the additional authentication data in one or more calls. More... | |
| int_fast16_t | AESCCM_processPayload (AESCCM_Handle handle, uint8_t *input, size_t length, uint8_t *output) |
| Function to process the input data in one or more calls. More... | |
| int_fast16_t | AESCCM_computeMAC (AESCCM_Handle handle, uint8_t *mac) |
| Function to compute the message authentication code. More... | |
| int_fast16_t | AESCCM_verifyMAC (AESCCM_Handle handle, uint8_t *mac) |
| Function to verify the provided message authentication code. More... | |
| int_fast16_t | AESCCM_oneStepEncrypt (AESCCM_Handle handle, CryptoKey *key, uint8_t *aad, size_t aadLength, uint8_t *plaintext, size_t plaintextLength, uint8_t *nonce, uint8_t nonceLength, uint8_t *mac, uint8_t macLength, uint8_t *ciphertext) |
| Function to perform an AESCCM encryption + authentication operation in one call. More... | |
| int_fast16_t | AESCCM_oneStepDecrypt (AESCCM_Handle handle, CryptoKey *key, uint8_t *aad, size_t aadLength, uint8_t *ciphertext, size_t ciphertextLength, uint8_t *nonce, uint8_t nonceLength, uint8_t *mac, uint8_t macLength, uint8_t *plaintext) |
| Function to perform an AESCCM decryption + verification operation in one call. More... | |
| int_fast16_t | AESCCM_getMode (AESCCM_Handle handle, AESCCM_Mode *mode) |
| Returns the AESCCM_Mode of an AESCCM operation in progress. More... | |
| int_fast16_t | AESCCM_getCryptoKey (AESCCM_Handle handle, CryptoKey **key) |
| Returns a pointer to the CryptoKey used for an AESCCM operation in progress. More... | |
| int_fast16_t | AESCCM_getNonce (AESCCM_Handle handle, uint8_t **nonce, uint8_t *nonceLength) |
| Returns a pointer to the nonce and the nonce length of an AESCCM operation in progress. More... | |
| int_fast16_t | AESCCM_getAAD (AESCCM_Handle handle, uint8_t **aad, size_t *aadLength) |
| Returns a pointer to the AAD and the AAD length of an AESCCM operation in progress. More... | |
| int_fast16_t | AESCCM_getInput (AESCCM_Handle handle, uint8_t **input, size_t *inputLength, size_t *totalInputLength) |
| Returns a pointer to the input (plaintext or ciphertext) and the input length of an AESCCM operation in progress. More... | |
| int_fast16_t | AESCCM_getOutput (AESCCM_Handle handle, uint8_t **output, size_t *outputLength, size_t *totalOutputLength) |
| Returns a pointer to the output (plaintext or ciphertext) and the output length of an AESCCM operation in progress. More... | |
| int_fast16_t | AESCCM_getMAC (AESCCM_Handle handle, uint8_t *mac, uint8_t *macLength) |
| Returns a pointer to the MAC and the MAC length of the last completed AESCCM operation. More... | |
| int_fast16_t | AESCCM_setMACReturnPointer (AESCCM_Handle handle, uint8_t *mac) |
Variables | |
| const AESCCM_Params | AESCCM_defaultParams |
| Default AESCCM_Params structure. More... | |
| typedef struct AESCCM_Config_* AESCCM_Handle |
A handle that is returned from an AESCCM_open() call.
| typedef void(* AESCCM_CallbackFxn) (AESCCM_Handle handle, CryptoKey *processedKey) |
The definition of a callback function used by the AESCCM driver when used in AESCCM_RETURN_BEHAVIOR_CALLBACK.
| handle | Handle of the client that started the CCM operation. |
| processedKey | The CryptoKey that the CCM operation was performed with. |
| typedef enum AESCCM_ReturnBehavior_ AESCCM_ReturnBehavior |
The way in which CCM function calls return after performing an encryption + authentication or decryption + verification operation.
Not all CCM operations exhibit the specified return behavor. Functions that do not require significant computation and cannot offload that computation to a background thread behave like regular functions. Which functions exhibit the specfied return behavior is not implementation dependent. Specifically, a software-backed implementation run on the same CPU as the application will emulate the return behavior while not actually offloading the computation to the background thread.
AESCCM functions exhibiting the specified return behavior have restrictions on the context from which they may be called.
| Task | Hwi | Swi | |
|---|---|---|---|
| AESCCM_RETURN_BEHAVIOR_CALLBACK | X | X | X |
| AESCCM_RETURN_BEHAVIOR_BLOCKING | X | ||
| AESCCM_RETURN_BEHAVIOR_POLLING | X | X | X |
| typedef enum AESCCM_Mode_ AESCCM_Mode |
Enum for the direction of the CCM operation.
| typedef struct AESCCM_Params_ AESCCM_Params |
CCM Parameters.
CCM Parameters are used to with the AESCCM_open() call. Default values for these parameters are set using AESCCM_Params_init().
| typedef struct AESCCM_Config_ AESCCM_Config |
AESCCM Global configuration.
The AESCCM_Config structure contains a set of pointers used to characterize the AESCCM driver implementation.
This structure needs to be defined before calling AESCCM_init() and it must not be changed thereafter.
The way in which CCM function calls return after performing an encryption + authentication or decryption + verification operation.
Not all CCM operations exhibit the specified return behavor. Functions that do not require significant computation and cannot offload that computation to a background thread behave like regular functions. Which functions exhibit the specfied return behavior is not implementation dependent. Specifically, a software-backed implementation run on the same CPU as the application will emulate the return behavior while not actually offloading the computation to the background thread.
AESCCM functions exhibiting the specified return behavior have restrictions on the context from which they may be called.
| Task | Hwi | Swi | |
|---|---|---|---|
| AESCCM_RETURN_BEHAVIOR_CALLBACK | X | X | X |
| AESCCM_RETURN_BEHAVIOR_BLOCKING | X | ||
| AESCCM_RETURN_BEHAVIOR_POLLING | X | X | X |
| enum AESCCM_Mode_ |
| void AESCCM_init | ( | void | ) |
This function initializes the CCM module.
| void AESCCM_Params_init | ( | AESCCM_Params * | params | ) |
Function to initialize the AESCCM_Params struct to its defaults.
| params | An pointer to AESCCM_Params structure for initialization |
Defaults values are: returnBehavior = AESCCM_RETURN_BEHAVIOR_BLOCKING callbackFxn = NULL nonceInternallyGenerated = false timeout = SemaphoreP_WAIT_FOREVER custom = NULL
| AESCCM_Handle AESCCM_open | ( | uint_least8_t | index, |
| AESCCM_Params * | params | ||
| ) |
This function opens a given CCM peripheral.
| index | Logical peripheral number for the CCM indexed into the AESCCM_config table |
| params | Pointer to an parameter block, if NULL it will use default values. |
| void AESCCM_close | ( | AESCCM_Handle | handle | ) |
Function to close a CCM peripheral specified by the CCM handle.
| handle | A CCM handle returned from AESCCM_open() |
| int_fast16_t AESCCM_control | ( | AESCCM_Handle | handle, |
| uint32_t | cmd, | ||
| void * | args | ||
| ) |
Function performs implementation specific features on a given AESCCM_Handle.
Commands for AESCCM_control can originate from AESCCM.h or from implementation specific AESCCM*.h (AESCCMCC26XX.h, AESCCMMSP432.h, etc.. ) files. While commands from AESCCM.h are API portable across driver implementations, not all implementations may support all these commands. Conversely, commands from driver implementation specific AESCCM*.h files add unique driver capabilities but are not API portable across all AESCCM driver implementations.
Commands supported by AESCCM.h follow an AESCCM_CMD_<cmd> naming convention.
Commands supported by AESCCM*.h follow an AESCCM*_CMD_<cmd> naming convention.
Each control command defines arg differently. The types of arg are documented with each command.
See AESCCM_control command codes for command codes.
See AESCCM_control return status codes for status codes.
| handle | A AESCCM handle returned from AESCCM_open() |
| cmd | AESCCM.h or AESCCM*.h commands. |
| args | An optional R/W (read/write) command argument accompanied with cmd |
| int_fast16_t AESCCM_setupEncrypt | ( | AESCCM_Handle | handle, |
| CryptoKey * | key, | ||
| uint8_t * | nonce, | ||
| uint8_t | nonceLength, | ||
| size_t | aadTotalLength, | ||
| size_t | plaintextTotalLength, | ||
| uint8_t | macLength | ||
| ) |
Function to set up an AESCCM encryption + authentication operation in multiple calls.
| [in] | handle | A CCM handle returned from AESCCM_open() |
| [in] | key | A previously initialized CryptoKey |
| [in] | aadTotalLength | Total length of the additional authentication data in bytes. Either aadTotalLength or plaintextTotalLength must be non-zero. |
| [in] | plaintextTotalLength | Total length of the plaintext in bytes. Either aadTotalLength or plaintextTotalLength must be non-zero. |
| [in,out] | nonce | A buffer containing a nonce. Nonces must be unique to each CCM operation and may not be reused. If nonceInternallyGenerated was set in the AESCCM_Params, the nonce will be generated by this function call and copied to this buffer. |
| [in] | nonceLength | Length of nonce in bytes. Valid nonce lengths are {7, 8, 9, 10, 11, 12, 13}. |
| [in] | macLength | Length of the message authentication code in bytes. Valid MAC lengths are [0, 1, ... 16]. |
| int_fast16_t AESCCM_setupDecrypt | ( | AESCCM_Handle | handle, |
| CryptoKey * | key, | ||
| uint8_t * | nonce, | ||
| uint8_t | nonceLength, | ||
| size_t | aadTotalLength, | ||
| size_t | ciphertextTotalLength, | ||
| uint8_t | macLength | ||
| ) |
Function to set up an AESCCM decryption + verification operation in multiple calls.
| [in] | handle | A CCM handle returned from AESCCM_open() |
| [in] | key | A previously initialized CryptoKey |
| [in] | aadTotalLength | Total length of the additional authentication data in bytes. Either aadTotalLength or plaintextTotalLength must be non-zero. |
| [in] | ciphertextTotalLength | Total length of the ciphertext in bytes. Either aadTotalLength or ciphertextTotalLength must be non-zero. |
| [in] | nonce | A buffer containing the nonce transmitted with the ciphertext and AAD. |
| [in] | nonceLength | Length of nonce in bytes. Valid nonce lengths are {7, 8, 9, 10, 11, 12, 13}. |
| [in] | macLength | Length of the message authentication code in bytes. Valid MAC lengths are [0, 1, ... 16]. |
| int_fast16_t AESCCM_processAAD | ( | AESCCM_Handle | handle, |
| uint8_t * | aad, | ||
| size_t | length | ||
| ) |
Function to process the additional authentication data in one or more calls.
| [in] | handle | A CCM handle returned from AESCCM_open() |
| [in] | aad | A buffer of length length containing additional authentication data to be authenticated but not encrypted. |
| [in] | length | Length of aad in bytes. Must be non-zero. May be smaller than the total AAD length provided in the setup call. This enables partial processing of longer AAD. |
| int_fast16_t AESCCM_processPayload | ( | AESCCM_Handle | handle, |
| uint8_t * | input, | ||
| size_t | length, | ||
| uint8_t * | output | ||
| ) |
Function to process the input data in one or more calls.
| [in] | handle | A CCM handle returned from AESCCM_open() |
| [in] | input | A buffer of length length containing either plaintext or ciphertext depending on the AESCCM_Mode. |
| [in] | length | Length of input and output in bytes. Must be non-zero. May be smaller than the total input length provided in the setup call. This enables partial processing of longer inputs. |
| [out] | output | A buffer of length length that is filled with either ciphertext or plaintext depending on the AESCCM_Mode after processing. |
| int_fast16_t AESCCM_computeMAC | ( | AESCCM_Handle | handle, |
| uint8_t * | mac | ||
| ) |
Function to compute the message authentication code.
| [in] | handle | A CCM handle returned from AESCCM_open() |
| [out] | mac | A buffer that the computed MAC is copied to. |
| int_fast16_t AESCCM_verifyMAC | ( | AESCCM_Handle | handle, |
| uint8_t * | mac | ||
| ) |
Function to verify the provided message authentication code.
| [in] | handle | A CCM handle returned from AESCCM_open() |
| [in] | mac | A buffer containing the MAC that the computed one will be verified against. |
| int_fast16_t AESCCM_oneStepEncrypt | ( | AESCCM_Handle | handle, |
| CryptoKey * | key, | ||
| uint8_t * | aad, | ||
| size_t | aadLength, | ||
| uint8_t * | plaintext, | ||
| size_t | plaintextLength, | ||
| uint8_t * | nonce, | ||
| uint8_t | nonceLength, | ||
| uint8_t * | mac, | ||
| uint8_t | macLength, | ||
| uint8_t * | ciphertext | ||
| ) |
Function to perform an AESCCM encryption + authentication operation in one call.
| [in] | handle | A CCM handle returned from AESCCM_open() |
| [in] | key | A previously initialized CryptoKey |
| [in] | aad | A buffer of length aadLength containing additional authentication data to be authenticated but not encrypted. |
| [in] | aadLength | Length of aad in bytes. Either aadLength or plaintextLength must be non-zero. |
| [in] | plaintext | The plaintext buffer to be encrypted and authenticated in the CCM operation. |
| [in] | plaintextLength | Length of plaintext in bytes. Either aadLength or plaintextLength must be non-zero. |
| [in,out] | nonce | A buffer containing a nonce. Nonces must be unique to each CCM operation and may not be reused. If nonceInternallyGenerated was set in the AESCCM_Params, the nonce will be generated by this function call and copied to this buffer. |
| [in] | nonceLength | Length of nonce in bytes. Valid nonce lengths are {7, 8, 9, 10, 11, 12, 13}. |
| [out] | mac | The message authentication code buffer to store the encrypted authentication tag. |
| [in] | macLength | Length of mac in bytes. Valid MAC lengths are [0, 1, ... 16]. |
| [out] | ciphertext | The output ciphertext buffer that the encrypted plaintext is copied to. It is of length plaintextLength. |
| int_fast16_t AESCCM_oneStepDecrypt | ( | AESCCM_Handle | handle, |
| CryptoKey * | key, | ||
| uint8_t * | aad, | ||
| size_t | aadLength, | ||
| uint8_t * | ciphertext, | ||
| size_t | ciphertextLength, | ||
| uint8_t * | nonce, | ||
| uint8_t | nonceLength, | ||
| uint8_t * | mac, | ||
| uint8_t | macLength, | ||
| uint8_t * | plaintext | ||
| ) |
Function to perform an AESCCM decryption + verification operation in one call.
| [in] | handle | A CCM handle returned from AESCCM_open() |
| [in] | key | A previously initialized CryptoKey |
| [in] | aad | A buffer of length aadLength containing additional authentication data to be verified but not decrypted. |
| [in] | aadLength | Length of aad in bytes. Either aadLength or plaintextLength must be non-zero. |
| [in] | ciphertext | The ciphertext buffer to be decrypted and verified in the CCM operation. |
| [in] | ciphertextLength | Length of plaintext in bytes. Either aadLength or plaintextLength must be non-zero. |
| [in] | nonce | A buffer containing the nonce transmitted with the ciphertext and AAD. |
| [in] | nonceLength | Length of nonce in bytes. Valid nonce lengths are {7, 8, 9, 10, 11, 12, 13}. |
| [in] | mac | The message authentication code buffer containing the encrypted authentication tag. |
| [in] | macLength | Length of mac in bytes. Valid MAC lengths are [0, 1, ... 16]. |
| [out] | plaintext | The output plaintext buffer that the decrypted ciphertext is copied to. It is of length ciphertexttextLength. |
| int_fast16_t AESCCM_getMode | ( | AESCCM_Handle | handle, |
| AESCCM_Mode * | mode | ||
| ) |
Returns the AESCCM_Mode of an AESCCM operation in progress.
| [in] | handle | A CCM handle returned from AESCCM_open() |
| [out] | mode | Whether the operation in progress is a decryption or encryption operation |
| int_fast16_t AESCCM_getCryptoKey | ( | AESCCM_Handle | handle, |
| CryptoKey ** | key | ||
| ) |
Returns a pointer to the CryptoKey used for an AESCCM operation in progress.
| [in] | handle | A CCM handle returned from AESCCM_open() |
| [out] | key | The CryptoKey used in the operation |
| int_fast16_t AESCCM_getNonce | ( | AESCCM_Handle | handle, |
| uint8_t ** | nonce, | ||
| uint8_t * | nonceLength | ||
| ) |
Returns a pointer to the nonce and the nonce length of an AESCCM operation in progress.
| [in] | handle | A CCM handle returned from AESCCM_open() |
| [out] | nonce | The nonce used in the operation |
| [out] | nonceLength | The length of the nonce used in the operation |
| int_fast16_t AESCCM_getAAD | ( | AESCCM_Handle | handle, |
| uint8_t ** | aad, | ||
| size_t * | aadLength | ||
| ) |
Returns a pointer to the AAD and the AAD length of an AESCCM operation in progress.
| [in] | handle | A CCM handle returned from AESCCM_open() |
| [out] | aad | The AAD used in the operation |
| [out] | aadLength | The length of the AAD used in the operation |
| int_fast16_t AESCCM_getInput | ( | AESCCM_Handle | handle, |
| uint8_t ** | input, | ||
| size_t * | inputLength, | ||
| size_t * | totalInputLength | ||
| ) |
Returns a pointer to the input (plaintext or ciphertext) and the input length of an AESCCM operation in progress.
| [in] | handle | A CCM handle returned from AESCCM_open() |
| [out] | input | The last input buffer used in the operation |
| [out] | inputLength | The length of the last input buffer used in the operation |
| [out] | totalInputLength | The total length of the input specified in the setup call. It is the same as the total length of the input. |
| int_fast16_t AESCCM_getOutput | ( | AESCCM_Handle | handle, |
| uint8_t ** | output, | ||
| size_t * | outputLength, | ||
| size_t * | totalOutputLength | ||
| ) |
Returns a pointer to the output (plaintext or ciphertext) and the output length of an AESCCM operation in progress.
| [in] | handle | A CCM handle returned from AESCCM_open() |
| [out] | output | The output buffer used in the operation |
| [out] | outputLength | The output of the input used in the operation |
| [out] | totalOutputLength | The total length of the output specified in the setup call. It is the same as the total length of the input. |
| int_fast16_t AESCCM_getMAC | ( | AESCCM_Handle | handle, |
| uint8_t * | mac, | ||
| uint8_t * | macLength | ||
| ) |
Returns a pointer to the MAC and the MAC length of the last completed AESCCM operation.
| [in] | handle | A CCM handle returned from AESCCM_open() |
| [out] | mac | The MAC verified or calculated in the operation |
| [out] | macLength | The length of the MAC |
| int_fast16_t AESCCM_setMACReturnPointer | ( | AESCCM_Handle | handle, |
| uint8_t * | mac | ||
| ) |
| const AESCCM_Params AESCCM_defaultParams |
Default AESCCM_Params structure.