CC26xx Driver Library
setup.c File Reference
#include "../inc/hw_types.h"
#include "../inc/hw_memmap.h"
#include "../inc/hw_adi.h"
#include "../inc/hw_adi_2_refsys.h"
#include "../inc/hw_adi_3_refsys.h"
#include "../inc/hw_aon_ioc.h"
#include "../inc/hw_aon_sysctl.h"
#include "../inc/hw_aon_wuc.h"
#include "../inc/hw_aux_wuc.h"
#include "../inc/hw_ccfg.h"
#include "../inc/hw_fcfg1.h"
#include "../inc/hw_flash.h"
#include "../inc/hw_prcm.h"
#include "../inc/hw_vims.h"
#include "aon_wuc.h"
#include "aux_wuc.h"
#include "chipinfo.h"
#include "setup.h"
#include "setup_rom.h"

Macros

#define CPU_DELAY_MICRO_SECONDS(x)   CPUdelay(((uint32_t)((( x ) * 48.0 ) / 5.0 )) - 1 )
 

Functions

static void TrimAfterColdReset (void)
 Trims to be applied when coming from PIN_RESET. More...
 
static void TrimAfterColdResetWakeupFromShutDown (uint32_t ui32Fcfg1Revision)
 Trims to be applied when coming from SHUTDOWN (also called when coming from PIN_RESET). More...
 
static void TrimAfterColdResetWakeupFromShutDownWakeupFromPowerDown (void)
 Trims to be applied when coming from POWER_DOWN (also called when coming from SHUTDOWN and PIN_RESET). More...
 
void SetupTrimDevice (void)
 Performs the necessary trim of the device which is not done in boot code. More...
 

Macro Definition Documentation

#define CPU_DELAY_MICRO_SECONDS (   x)    CPUdelay(((uint32_t)((( x ) * 48.0 ) / 5.0 )) - 1 )

Function Documentation

static void TrimAfterColdReset ( void  )
static

Trims to be applied when coming from PIN_RESET.

Returns
None

Referenced by SetupTrimDevice().

328 {
329  // Currently no specific trim for Cold Reset
330 }
static void TrimAfterColdResetWakeupFromShutDown ( uint32_t  ui32Fcfg1Revision)
static

Trims to be applied when coming from SHUTDOWN (also called when coming from PIN_RESET).

Parameters
ui32Fcfg1Revision
Returns
None

Referenced by SetupTrimDevice().

252 {
253  uint32_t ccfg_ModeConfReg ;
254 
255  // Force AUX on and enable clocks
256  //
257  // No need to save the current status of the power/clock registers.
258  // At this point both AUX and AON should have been reset to 0x0.
259  HWREG(AON_WUC_BASE + AON_WUC_O_AUXCTL) = AON_WUC_AUXCTL_AUX_FORCE_ON;
260 
261  // Wait for power on on the AUX domain
262  while( ! ( HWREGBITW( AON_WUC_BASE + AON_WUC_O_PWRSTAT, AON_WUC_PWRSTAT_AUX_PD_ON_BITN )));
263 
264  // Enable the clocks for AUX_DDI0_OSC and AUX_ADI4
265  HWREG(AUX_WUC_BASE + AUX_WUC_O_MODCLKEN0) = AUX_WUC_MODCLKEN0_AUX_DDI0_OSC |
266  AUX_WUC_MODCLKEN0_AUX_ADI4;
267 
268  // Check in CCFG for alternative DCDC setting
269  if (( HWREG( CCFG_BASE + CCFG_O_SIZE_AND_DIS_FLAGS ) & CCFG_SIZE_AND_DIS_FLAGS_DIS_ALT_DCDC_SETTING ) == 0 ) {
270  // ADI_3_REFSYS:DCDCCTL5[3] (=DITHER_EN) = CCFG_MODE_CONF_1[19] (=ALT_DCDC_DITHER_EN)
271  // ADI_3_REFSYS:DCDCCTL5[2:0](=IPEAK ) = CCFG_MODE_CONF_1[18:16](=ALT_DCDC_IPEAK )
272  // Using a single 4-bit masked write since layout is equal for both source and destination
273  HWREGB( ADI3_BASE + ADI_O_MASK4B + ( ADI_3_REFSYS_O_DCDCCTL5 * 2 )) = ( 0xF0 |
274  ( HWREG( CCFG_BASE + CCFG_O_MODE_CONF_1 ) >> CCFG_MODE_CONF_1_ALT_DCDC_IPEAK_S ));
275 
276  }
277 
278  //
279  // Enable for JTAG to be powered down (will still be powered on if debugger is connected)
281 
282  // read the MODE_CONF register in CCFG
283  ccfg_ModeConfReg = HWREG( CCFG_BASE + CCFG_O_MODE_CONF );
284 
285  // First part of trim done after cold reset and wakeup from shutdown:
286  // -Adjust the VDDR_TRIM_SLEEP value.
287  // -Configure DCDC.
288  SetupAfterColdResetWakeupFromShutDownCfg1( ccfg_ModeConfReg );
289 
290  // Second part of trim done after cold reset and wakeup from shutdown:
291  // -Configure XOSC.
292 #if ( CCFG_BASE == CCFG_BASE_DEFAULT )
293  SetupAfterColdResetWakeupFromShutDownCfg2( ui32Fcfg1Revision, ccfg_ModeConfReg );
294 #else
295  NOROM_SetupAfterColdResetWakeupFromShutDownCfg2( ui32Fcfg1Revision, ccfg_ModeConfReg );
296 #endif
297 
298  // Third part of trim done after cold reset and wakeup from shutdown:
299  // -Configure HPOSC.
300  // -Setup the LF clock.
301 #if ( CCFG_BASE == CCFG_BASE_DEFAULT )
302  SetupAfterColdResetWakeupFromShutDownCfg3( ccfg_ModeConfReg );
303 #else
304  NOROM_SetupAfterColdResetWakeupFromShutDownCfg3( ccfg_ModeConfReg );
305 #endif
306 
307  //
308  // Allow AUX to power down
310 
311  // Leaving on AUX and clock for AUX_DDI0_OSC on but turn off clock for AUX_ADI4
312  HWREG( AUX_WUC_BASE + AUX_WUC_O_MODCLKEN0 ) = AUX_WUC_MODCLKEN0_AUX_DDI0_OSC;
313 
314  // Disable EFUSE clock
315  HWREGBITW( FLASH_BASE + FLASH_O_CFG, FLASH_CFG_DIS_EFUSECLK_BITN ) = 1;
316 }
void SetupAfterColdResetWakeupFromShutDownCfg3(uint32_t ccfg_ModeConfReg)
Third part of configuration required when waking up from shutdown.
Definition: setup_rom.c:283
#define AUX_WUC_POWER_DOWN
Definition: aux_wuc.h:95
void AUXWUCPowerCtrl(uint32_t ui32PowerMode)
Control the power to the AUX domain.
Definition: aux_wuc.c:254
void SetupAfterColdResetWakeupFromShutDownCfg1(uint32_t ccfg_ModeConfReg)
First part of configuration required when waking up from shutdown.
Definition: setup_rom.c:123
void SetupAfterColdResetWakeupFromShutDownCfg2(uint32_t ui32Fcfg1Revision, uint32_t ccfg_ModeConfReg)
Second part of configuration required when waking up from shutdown.
Definition: setup_rom.c:178
static void AONWUCJtagPowerOff(void)
Request power off of the JTAG domain.
Definition: aon_wuc.h:792

Here is the call graph for this function:

static void TrimAfterColdResetWakeupFromShutDownWakeupFromPowerDown ( void  )
static

Trims to be applied when coming from POWER_DOWN (also called when coming from SHUTDOWN and PIN_RESET).

Returns
None

Referenced by SetupTrimDevice().

236 {
237  // Currently no specific trim for Powerdown
238 }