#include <stdbool.h>#include <stdint.h>#include "../inc/hw_types.h"#include "../inc/hw_memmap.h"#include "../inc/hw_ints.h"#include "../inc/hw_prcm.h"#include "../inc/hw_nvic.h"#include "../inc/hw_aon_rtc.h"#include "interrupt.h"#include "debug.h"#include "cpu.h"Macros | |
| #define | PRCM_RUN_MODE 0x00000001 |
| #define | PRCM_SLEEP_MODE 0x00000002 |
| #define | PRCM_DEEP_SLEEP_MODE 0x00000004 |
| #define | PRCM_CLOCK_DIV_1 PRCM_GPTCLKDIV_RATIO_DIV1 |
| #define | PRCM_CLOCK_DIV_2 PRCM_GPTCLKDIV_RATIO_DIV2 |
| #define | PRCM_CLOCK_DIV_4 PRCM_GPTCLKDIV_RATIO_DIV4 |
| #define | PRCM_CLOCK_DIV_8 PRCM_GPTCLKDIV_RATIO_DIV8 |
| #define | PRCM_CLOCK_DIV_16 PRCM_GPTCLKDIV_RATIO_DIV16 |
| #define | PRCM_CLOCK_DIV_32 PRCM_GPTCLKDIV_RATIO_DIV32 |
| #define | PRCM_CLOCK_DIV_64 PRCM_GPTCLKDIV_RATIO_DIV64 |
| #define | PRCM_CLOCK_DIV_128 PRCM_GPTCLKDIV_RATIO_DIV128 |
| #define | PRCM_CLOCK_DIV_256 PRCM_GPTCLKDIV_RATIO_DIV256 |
| #define | PRCM_DOMAIN_RFCORE 0x00000001 |
| #define | PRCM_DOMAIN_SERIAL 0x00000002 |
| #define | PRCM_DOMAIN_PERIPH 0x00000004 |
| #define | PRCM_DOMAIN_SYSBUS 0x00000008 |
| #define | PRCM_DOMAIN_VIMS 0x00000010 |
| #define | PRCM_DOMAIN_CPU 0x00000020 |
| #define | PRCM_DOMAIN_TIMER 0x00000040 |
| #define | PRCM_DOMAIN_CLKCTRL 0x00000080 |
| #define | PRCM_DOMAIN_MCU 0x00000100 |
| #define | PRCM_DOMAIN_POWER_OFF 0x00000002 |
| #define | PRCM_DOMAIN_POWER_ON 0x00000001 |
| #define | PRCM_DOMAIN_POWER_DOWN_READY 0x00000000 |
| #define | PRCM_WCLK_NEG_EDGE 0x00000008 |
| #define | PRCM_WCLK_POS_EDGE 0x00000000 |
| #define | PRCM_WCLK_SINGLE_PHASE 0x00000000 |
| #define | PRCM_WCLK_DUAL_PHASE 0x00000002 |
| #define | PRCM_WCLK_USER_DEF 0x00000004 |
| #define | I2S_SAMPLE_RATE_16K 0x00000001 |
| #define | I2S_SAMPLE_RATE_24K 0x00000002 |
| #define | I2S_SAMPLE_RATE_32K 0x00000004 |
| #define | I2S_SAMPLE_RATE_48K 0x00000008 |
| #define | PRCM_PERIPH_TIMER0 ( 0x00000000 | ( PRCM_GPTCLKGR_CLK_EN_S )) |
| #define | PRCM_PERIPH_TIMER1 ( 0x00000000 | ( PRCM_GPTCLKGR_CLK_EN_S + 1 )) |
| #define | PRCM_PERIPH_TIMER2 ( 0x00000000 | ( PRCM_GPTCLKGR_CLK_EN_S + 2 )) |
| #define | PRCM_PERIPH_TIMER3 ( 0x00000000 | ( PRCM_GPTCLKGR_CLK_EN_S + 3 )) |
| #define | PRCM_PERIPH_SSI0 ( 0x00000100 | ( PRCM_SSICLKGR_CLK_EN_S )) |
| #define | PRCM_PERIPH_SSI1 ( 0x00000100 | ( PRCM_SSICLKGR_CLK_EN_S + 1 )) |
| #define | PRCM_PERIPH_UART0 ( 0x00000200 | ( PRCM_UARTCLKGR_CLK_EN_S )) |
| #define | PRCM_PERIPH_I2C0 ( 0x00000300 | ( PRCM_I2CCLKGR_CLK_EN_S )) |
| #define | PRCM_PERIPH_CRYPTO ( 0x00000400 | ( PRCM_SECDMACLKGR_CRYPTO_CLK_EN_S )) |
| #define | PRCM_PERIPH_TRNG ( 0x00000400 | ( PRCM_SECDMACLKGR_TRNG_CLK_EN_S )) |
| #define | PRCM_PERIPH_UDMA ( 0x00000400 | ( PRCM_SECDMACLKGR_DMA_CLK_EN_S )) |
| #define | PRCM_PERIPH_GPIO ( 0x00000500 | ( PRCM_GPIOCLKGR_CLK_EN_S )) |
| #define | PRCM_PERIPH_I2S ( 0x00000600 | ( PRCM_I2SCLKGR_CLK_EN_S )) |
Functions | |
| void | PRCMInfClockConfigureSet (uint32_t ui32ClkDiv, uint32_t ui32PowerMode) |
| Configure the infrastructure clock. More... | |
| uint32_t | PRCMInfClockConfigureGet (uint32_t ui32PowerMode) |
| Use this function to get the infrastructure clock configuration. More... | |
| static void | PRCMMcuPowerOff (void) |
| Request a power off of the MCU voltage domain. More... | |
| static void | PRCMMcuPowerOffCancel (void) |
| Cancel a request for a power off of the MCU voltage domain. More... | |
| static void | PRCMMcuUldoConfigure (uint32_t ui32Enable) |
| Assert or de-assert a request for the uLDO. More... | |
| static void | PRCMGPTimerClockDivisionSet (uint32_t clkDiv) |
| Setup the clock division factor for the GP-Timer domain. More... | |
| static uint32_t | PRCMGPTimerClockDivisionGet (void) |
| Get the clock division factor for the GP-Timer domain. More... | |
| static void | PRCMAudioClockEnable (void) |
| Enable the audio clock generation. More... | |
| static void | PRCMAudioClockDisable (void) |
| Disable the audio clock generation. More... | |
| void | PRCMAudioClockConfigSet (uint32_t ui32ClkConfig, uint32_t ui32SampleRate) |
| Configure the audio clock generation. More... | |
| void | PRCMAudioClockConfigSetOverride (uint32_t ui32ClkConfig, uint32_t ui32MstDiv, uint32_t ui32BitDiv, uint32_t ui32WordDiv) |
| Configure the audio clock generation with manual setting of clock divider. More... | |
| static void | PRCMLoadSet (void) |
| Use this function to synchronize the load settings. More... | |
| static bool | PRCMLoadGet (void) |
| Check if any of the load sensitive register has been updated. More... | |
| static void | PRCMDomainEnable (uint32_t ui32Domains) |
| Enable clock domains in the MCU voltage domain. More... | |
| static void | PRCMDomainDisable (uint32_t ui32Domains) |
| Disable clock domains in the MCU voltage domain. More... | |
| void | PRCMPowerDomainOn (uint32_t ui32Domains) |
| Turn power on in power domains in the MCU domain. More... | |
| void | PRCMPowerDomainOff (uint32_t ui32Domains) |
| Turn off a specific power domain. More... | |
| static void | PRCMRfPowerDownWhenIdle (void) |
| Configure RF core to power down when idle. More... | |
| void | PRCMPeripheralRunEnable (uint32_t ui32Peripheral) |
| Enables a peripheral in Run mode. More... | |
| void | PRCMPeripheralRunDisable (uint32_t ui32Peripheral) |
| void | PRCMPeripheralSleepEnable (uint32_t ui32Peripheral) |
| Enables a peripheral in sleep mode. More... | |
| void | PRCMPeripheralSleepDisable (uint32_t ui32Peripheral) |
| Disables a peripheral in sleep mode. More... | |
| void | PRCMPeripheralDeepSleepEnable (uint32_t ui32Peripheral) |
| Enables a peripheral in deep-sleep mode. More... | |
| void | PRCMPeripheralDeepSleepDisable (uint32_t ui32Peripheral) |
| Disables a peripheral in deep-sleep mode. More... | |
| uint32_t | PRCMPowerDomainStatus (uint32_t ui32Domains) |
| Get the status for a specific power domain. More... | |
| static bool | PRCMRfReady (void) |
| Return the access status of the RF Core. More... | |
| static void | PRCMSleep (void) |
| Put the processor into sleep mode. More... | |
| void | PRCMDeepSleep (void) |
| Put the processor into deep-sleep mode. More... | |
| static void | PRCMCacheRetentionEnable (void) |
| Enable CACHE RAM retention. More... | |
| static void | PRCMCacheRetentionDisable (void) |
| Disable CACHE RAM retention. More... | |