|
| void | I2CMasterInitExpClk (uint32_t ui32Base, uint32_t ui32I2CClk, bool bFast) |
| | Initializes the I2C Master block. More...
|
| |
| static void | I2CMasterControl (uint32_t ui32Base, uint32_t ui32Cmd) |
| | Controls the state of the I2C Master module. More...
|
| |
| static void | I2CMasterSlaveAddrSet (uint32_t ui32Base, uint8_t ui8SlaveAddr, bool bReceive) |
| | Sets the address that the I2C Master will place on the bus. More...
|
| |
| static void | I2CMasterEnable (uint32_t ui32Base) |
| | Enables the I2C Master block. More...
|
| |
| static void | I2CMasterDisable (uint32_t ui32Base) |
| | Disables the I2C master block. More...
|
| |
| static bool | I2CMasterBusy (uint32_t ui32Base) |
| | Indicates whether or not the I2C Master is busy. More...
|
| |
| static bool | I2CMasterBusBusy (uint32_t ui32Base) |
| | Indicates whether or not the I2C bus is busy. More...
|
| |
| static uint32_t | I2CMasterDataGet (uint32_t ui32Base) |
| | Receives a byte that has been sent to the I2C Master. More...
|
| |
| static void | I2CMasterDataPut (uint32_t ui32Base, uint8_t ui8Data) |
| | Transmits a byte from the I2C Master. More...
|
| |
| uint32_t | I2CMasterErr (uint32_t ui32Base) |
| | Gets the error status of the I2C Master module. More...
|
| |
| static void | I2CMasterIntEnable (uint32_t ui32Base) |
| | Enables the I2C Master interrupt. More...
|
| |
| static void | I2CMasterIntDisable (uint32_t ui32Base) |
| | Disables the I2C Master interrupt. More...
|
| |
| static void | I2CMasterIntClear (uint32_t ui32Base) |
| | Clears I2C Master interrupt sources. More...
|
| |
| static bool | I2CMasterIntStatus (uint32_t ui32Base, bool bMasked) |
| | Gets the current I2C Master interrupt status. More...
|
| |
| static void | I2CSlaveEnable (uint32_t ui32Base) |
| | Enables the I2C Slave block. More...
|
| |
| static void | I2CSlaveInit (uint32_t ui32Base, uint8_t ui8SlaveAddr) |
| | Initializes the I2C Slave block. More...
|
| |
| static void | I2CSlaveAddressSet (uint32_t ui32Base, uint8_t ui8SlaveAddr) |
| | Sets the I2C slave address. More...
|
| |
| static void | I2CSlaveDisable (uint32_t ui32Base) |
| | Disables the I2C slave block. More...
|
| |
| static uint32_t | I2CSlaveStatus (uint32_t ui32Base) |
| | Gets the I2C Slave module status. More...
|
| |
| static uint32_t | I2CSlaveDataGet (uint32_t ui32Base) |
| | Receives a byte that has been sent to the I2C Slave. More...
|
| |
| static void | I2CSlaveDataPut (uint32_t ui32Base, uint8_t ui8Data) |
| | Transmits a byte from the I2C Slave. More...
|
| |
| static void | I2CSlaveIntEnable (uint32_t ui32Base, uint32_t ui32IntFlags) |
| | Enables individual I2C Slave interrupt sources. More...
|
| |
| static void | I2CSlaveIntDisable (uint32_t ui32Base, uint32_t ui32IntFlags) |
| | Disables individual I2C Slave interrupt sources. More...
|
| |
| static void | I2CSlaveIntClear (uint32_t ui32Base, uint32_t ui32IntFlags) |
| | Clears I2C Slave interrupt sources. More...
|
| |
| static uint32_t | I2CSlaveIntStatus (uint32_t ui32Base, bool bMasked) |
| | Gets the current I2C Slave interrupt status. More...
|
| |
| void | I2CIntRegister (uint32_t ui32Base, void(*pfnHandler)(void)) |
| | Registers an interrupt handler for the I2C module. More...
|
| |
| void | I2CIntUnregister (uint32_t ui32Base) |
| | Unregisters an interrupt handler for the I2C module. More...
|
| |