CC26xx Driver Library
[uart] Universal Asynchronous Receiver/Transmitter

Functions

static void UARTParityModeSet (uint32_t ui32Base, uint32_t ui32Parity)
 Sets the type of parity. More...
 
static uint32_t UARTParityModeGet (uint32_t ui32Base)
 Gets the type of parity currently being used. More...
 
static void UARTFIFOLevelSet (uint32_t ui32Base, uint32_t ui32TxLevel, uint32_t ui32RxLevel)
 Sets the FIFO level at which interrupts are generated. More...
 
void UARTFIFOLevelGet (uint32_t ui32Base, uint32_t *pui32TxLevel, uint32_t *pui32RxLevel)
 Gets the FIFO level at which interrupts are generated. More...
 
void UARTConfigSetExpClk (uint32_t ui32Base, uint32_t ui32UARTClk, uint32_t ui32Baud, uint32_t ui32Config)
 Sets the configuration of a UART. More...
 
void UARTConfigGetExpClk (uint32_t ui32Base, uint32_t ui32UARTClk, uint32_t *pui32Baud, uint32_t *pui32Config)
 Gets the current configuration of a UART. More...
 
static void UARTEnable (uint32_t ui32Base)
 Enables transmitting and receiving. More...
 
void UARTDisable (uint32_t ui32Base)
 Disables transmitting and receiving. More...
 
static void UARTFIFOEnable (uint32_t ui32Base)
 Enables the transmit and receive FIFOs. More...
 
static void UARTFIFODisable (uint32_t ui32Base)
 Disables the transmit and receive FIFOs. More...
 
static bool UARTCharsAvail (uint32_t ui32Base)
 Determines if there are any characters in the receive FIFO. More...
 
static bool UARTSpaceAvail (uint32_t ui32Base)
 Determines if there is any space in the transmit FIFO. More...
 
int32_t UARTCharGetNonBlocking (uint32_t ui32Base)
 Receives a character from the specified port. More...
 
int32_t UARTCharGet (uint32_t ui32Base)
 Waits for a character from the specified port. More...
 
bool UARTCharPutNonBlocking (uint32_t ui32Base, uint8_t ui8Data)
 Sends a character to the specified port. More...
 
void UARTCharPut (uint32_t ui32Base, uint8_t ui8Data)
 Waits to send a character from the specified port. More...
 
static bool UARTBusy (uint32_t ui32Base)
 Determines whether the UART transmitter is busy or not. More...
 
static void UARTBreakCtl (uint32_t ui32Base, bool bBreakState)
 Causes a BREAK to be sent. More...
 
void UARTIntRegister (uint32_t ui32Base, void(*pfnHandler)(void))
 Registers an interrupt handler for a UART interrupt. More...
 
void UARTIntUnregister (uint32_t ui32Base)
 Unregisters an interrupt handler for a UART interrupt. More...
 
static void UARTIntEnable (uint32_t ui32Base, uint32_t ui32IntFlags)
 Enables individual UART interrupt sources. More...
 
static void UARTIntDisable (uint32_t ui32Base, uint32_t ui32IntFlags)
 Disables individual UART interrupt sources. More...
 
static uint32_t UARTIntStatus (uint32_t ui32Base, bool bMasked)
 Gets the current interrupt status. More...
 
static void UARTIntClear (uint32_t ui32Base, uint32_t ui32IntFlags)
 Clears UART interrupt sources. More...
 
static void UARTDMAEnable (uint32_t ui32Base, uint32_t ui32DMAFlags)
 Enable UART DMA operation. More...
 
static void UARTDMADisable (uint32_t ui32Base, uint32_t ui32DMAFlags)
 Disable UART DMA operation. More...
 
static uint32_t UARTRxErrorGet (uint32_t ui32Base)
 Gets current receiver errors. More...
 
static void UARTRxErrorClear (uint32_t ui32Base)
 Clears all reported receiver errors. More...
 
static void UARTHwFlowControlEnable (uint32_t ui32Base)
 Enables hardware flow control for both CTS and RTS. More...
 
static void UARTHwFlowControlDisable (uint32_t ui32Base)
 Disables hardware flow control for both CTS and RTS. More...
 

Detailed Description

Function Documentation

static void UARTBreakCtl ( uint32_t  ui32Base,
bool  bBreakState 
)
inlinestatic

Causes a BREAK to be sent.

Note
For proper transmission of a break command, the break must be asserted for at least two complete frames.
Parameters
ui32Baseis the base address of the UART port.
bBreakStatecontrols the output level.
  • true : Asserts a break condition on the UART.
  • false : Removes the break condition.
Returns
None
663 {
664  // Check the arguments.
665  ASSERT(UARTBaseValid(ui32Base));
666 
667  // Set the break condition as requested.
668  HWREG(ui32Base + UART_O_LCRH) =
669  (bBreakState ?
670  (HWREG(ui32Base + UART_O_LCRH) | UART_LCRH_BRK) :
671  (HWREG(ui32Base + UART_O_LCRH) & ~(UART_LCRH_BRK)));
672 }
#define ASSERT(expr)
Definition: debug.h:73
static bool UARTBusy ( uint32_t  ui32Base)
inlinestatic

Determines whether the UART transmitter is busy or not.

Allows the caller to determine whether all transmitted bytes have cleared the transmitter hardware. If false is returned, the transmit FIFO is empty and all bits of the last transmitted character, including all stop bits, have left the hardware shift register.

Parameters
ui32Baseis the base address of the UART port.
Returns
Returns status of UART transmitter.
  • true : UART is transmitting.
  • false : All transmissions are complete.
637 {
638  // Check the argument.
639  ASSERT(UARTBaseValid(ui32Base));
640 
641  // Determine if the UART is busy.
642  return((HWREG(ui32Base + UART_O_FR) & UART_FR_BUSY) ?
643  UART_BUSY : UART_IDLE);
644 }
#define UART_BUSY
Definition: uart.h:184
#define ASSERT(expr)
Definition: debug.h:73
#define UART_IDLE
Definition: uart.h:185
int32_t UARTCharGet ( uint32_t  ui32Base)

Waits for a character from the specified port.

This function gets a character from the receive FIFO for the specified port. If there are no characters available, this function waits until a character is received before returning.

Parameters
ui32Baseis the base address of the UART port.
Returns
Returns the character read from the specified port, cast as an int32_t.
202 {
203  // Check the arguments.
204  ASSERT(UARTBaseValid(ui32Base));
205 
206  // Wait until a char is available.
207  while(HWREG(ui32Base + UART_O_FR) & UART_FR_RXFE)
208  {
209  }
210 
211  // Now get the character.
212  return(HWREG(ui32Base + UART_O_DR));
213 }
#define ASSERT(expr)
Definition: debug.h:73
int32_t UARTCharGetNonBlocking ( uint32_t  ui32Base)

Receives a character from the specified port.

This function gets a character from the receive FIFO for the specified port.

Note
The UARTCharsAvail() function should be called before attempting to call this function.
Parameters
ui32Baseis the base address of the UART port.
Returns
Returns the character read from the specified port, cast as an int32_t. A -1 is returned if there are no characters present in the receive FIFO.
See also
UARTCharsAvail()
178 {
179  // Check the arguments.
180  ASSERT(UARTBaseValid(ui32Base));
181 
182  // See if there are any characters in the receive FIFO.
183  if(!(HWREG(ui32Base + UART_O_FR) & UART_FR_RXFE))
184  {
185  // Read and return the next character.
186  return(HWREG(ui32Base + UART_O_DR));
187  }
188  else
189  {
190  // There are no characters, so return a failure.
191  return(-1);
192  }
193 }
#define ASSERT(expr)
Definition: debug.h:73
void UARTCharPut ( uint32_t  ui32Base,
uint8_t  ui8Data 
)

Waits to send a character from the specified port.

This function sends the character ui8Data to the transmit FIFO for the specified port. If there is no space available in the transmit FIFO, this function waits until there is space available before returning.

Parameters
ui32Baseis the base address of the UART port.
ui8Datais the character to be transmitted.
Returns
None
249 {
250  // Check the arguments.
251  ASSERT(UARTBaseValid(ui32Base));
252 
253  // Wait until space is available.
254  while(HWREG(ui32Base + UART_O_FR) & UART_FR_TXFF)
255  {
256  }
257 
258  // Send the char.
259  HWREG(ui32Base + UART_O_DR) = ui8Data;
260 }
#define ASSERT(expr)
Definition: debug.h:73
bool UARTCharPutNonBlocking ( uint32_t  ui32Base,
uint8_t  ui8Data 
)

Sends a character to the specified port.

This function writes the character ui8Data to the transmit FIFO for the specified port. This function does not block, so if there is no space available, then a false is returned, and the application must retry the function later.

Parameters
ui32Baseis the base address of the UART port.
ui8Datais the character to be transmitted.
Returns
Returns status of the character transmit.
  • true : The character was successfully placed in the transmit FIFO.
  • false : There was no space available in the transmit FIFO. Try again later.
222 {
223  // Check the arguments.
224  ASSERT(UARTBaseValid(ui32Base));
225 
226  // See if there is space in the transmit FIFO.
227  if(!(HWREG(ui32Base + UART_O_FR) & UART_FR_TXFF))
228  {
229  // Write this character to the transmit FIFO.
230  HWREG(ui32Base + UART_O_DR) = ui8Data;
231 
232  // Success.
233  return(true);
234  }
235  else
236  {
237  // There is no space in the transmit FIFO, so return a failure.
238  return(false);
239  }
240 }
#define ASSERT(expr)
Definition: debug.h:73
static bool UARTCharsAvail ( uint32_t  ui32Base)
inlinestatic

Determines if there are any characters in the receive FIFO.

This function returns a flag indicating whether or not there is data available in the receive FIFO.

Parameters
ui32Baseis the base address of the UART port.
Returns
Returns status of the receive FIFO.
  • true : There is data in the receive FIFO.
  • false : There is no data in the receive FIFO.
515 {
516  // Check the arguments.
517  ASSERT(UARTBaseValid(ui32Base));
518 
519  // Return the availability of characters.
520  return((HWREG(ui32Base + UART_O_FR) & UART_FR_RXFE) ? false : true);
521 }
#define ASSERT(expr)
Definition: debug.h:73
void UARTConfigGetExpClk ( uint32_t  ui32Base,
uint32_t  ui32UARTClk,
uint32_t *  pui32Baud,
uint32_t *  pui32Config 
)

Gets the current configuration of a UART.

The baud rate and data format for the UART is determined, given an explicitly provided peripheral clock (hence the ExpClk suffix). The returned baud rate is the actual baud rate; it may not be the exact baud rate requested or an "official" baud rate. The data format returned in pui32Config is enumerated the same as the ui32Config parameter of UARTConfigSetExpClk().

Note
The peripheral clock is not necessarily the same as the processor clock. The frequency of the peripheral clock is set by the system control.
Parameters
ui32Baseis the base address of the UART port.
ui32UARTClkis the rate of the clock supplied to the UART module.
pui32Baudis a pointer to storage for the baud rate.
pui32Configis a pointer to storage for the data format.
Returns
None
129 {
130  uint32_t ui32Int, ui32Frac;
131 
132  // Check the arguments.
133  ASSERT(UARTBaseValid(ui32Base));
134 
135  // Compute the baud rate.
136  ui32Int = HWREG(ui32Base + UART_O_IBRD);
137  ui32Frac = HWREG(ui32Base + UART_O_FBRD);
138  *pui32Baud = (ui32UARTClk * 4) / ((64 * ui32Int) + ui32Frac);
139 
140  // Get the parity, data length, and number of stop bits.
141  *pui32Config = (HWREG(ui32Base + UART_O_LCRH) &
144 }
#define ASSERT(expr)
Definition: debug.h:73
void UARTConfigSetExpClk ( uint32_t  ui32Base,
uint32_t  ui32UARTClk,
uint32_t  ui32Baud,
uint32_t  ui32Config 
)

Sets the configuration of a UART.

This function configures the UART for operation in the specified data format.

Note
The peripheral clock is not necessarily the same as the processor clock. The frequency of the peripheral clock is set by the system control.
Parameters
ui32Baseis the base address of the UART port.
ui32UARTClkis the rate of the clock supplied to the UART module.
ui32Baudis the desired baud rate.
  • Minimum baud rate: ui32Baud >= ceil(ui32UARTClk / 1,048,559.875)
  • Maximum baud rate: ui32Baud <= floor(ui32UARTClk / 15.875)
ui32Configis the data format for the port. The parameter is the bitwise OR of three values:
Returns
None
100 {
101  uint32_t ui32Div;
102 
103  // Check the arguments.
104  ASSERT(UARTBaseValid(ui32Base));
105  ASSERT(ui32Baud != 0);
106 
107  // Stop the UART.
108  UARTDisable(ui32Base);
109 
110  // Compute the fractional baud rate divider.
111  ui32Div = (((ui32UARTClk * 8) / ui32Baud) + 1) / 2;
112 
113  // Set the baud rate.
114  HWREG(ui32Base + UART_O_IBRD) = ui32Div / 64;
115  HWREG(ui32Base + UART_O_FBRD) = ui32Div % 64;
116 
117  // Set parity, data length, and number of stop bits.
118  HWREG(ui32Base + UART_O_LCRH) = ui32Config;
119 }
void UARTDisable(uint32_t ui32Base)
Disables transmitting and receiving.
Definition: uart.c:152
#define ASSERT(expr)
Definition: debug.h:73

Here is the call graph for this function:

void UARTDisable ( uint32_t  ui32Base)

Disables transmitting and receiving.

This function clears the UARTEN, TXE, and RXE bits, waits for the end of transmission of the current character, and flushes the transmit FIFO.

Parameters
ui32Baseis the base address of the UART port.
Returns
None

Referenced by UARTConfigSetExpClk().

153 {
154 
155  // Check the arguments.
156  ASSERT(UARTBaseValid(ui32Base));
157 
158  // Wait for end of TX.
159  while(HWREG(ui32Base + UART_O_FR) & UART_FR_BUSY)
160  {
161  }
162 
163  // Disable the FIFO.
164  HWREG(ui32Base + UART_O_LCRH) &= ~(UART_LCRH_FEN);
165 
166  // Disable the UART.
167  HWREG(ui32Base + UART_O_CTL) &= ~(UART_CTL_UARTEN | UART_CTL_TXE |
168  UART_CTL_RXE);
169 }
#define ASSERT(expr)
Definition: debug.h:73
static void UARTDMADisable ( uint32_t  ui32Base,
uint32_t  ui32DMAFlags 
)
inlinestatic

Disable UART DMA operation.

This function is used to disable UART DMA features that were enabled by UARTDMAEnable(). The specified UART DMA features are disabled.

Parameters
ui32Baseis the base address of the UART port.
ui32DMAFlagsis a bit mask of the DMA features to disable. The parameter is the bitwise OR of any of the following values:
  • UART_DMA_RX : Enable DMA for receive.
  • UART_DMA_TX : Enable DMA for transmit.
  • UART_DMA_ERR_RXSTOP : Disable DMA receive on UART error.
Returns
None
918 {
919  // Check the arguments.
920  ASSERT(UARTBaseValid(ui32Base));
921 
922  // Clear the requested bits in the UART DMA control register.
923  HWREG(ui32Base + UART_O_DMACTL) &= ~ui32DMAFlags;
924 }
#define ASSERT(expr)
Definition: debug.h:73
static void UARTDMAEnable ( uint32_t  ui32Base,
uint32_t  ui32DMAFlags 
)
inlinestatic

Enable UART DMA operation.

The specified UART DMA features are enabled. The UART can be configured to use DMA for transmit or receive, and to disable receive if an error occurs.

Note
The uDMA controller must also be set up before DMA can be used with the UART.
Parameters
ui32Baseis the base address of the UART port.
ui32DMAFlagsis a bit mask of the DMA features to enable. The parameter is the bitwise OR of any of the following values:
  • UART_DMA_RX : Enable DMA for receive.
  • UART_DMA_TX : Enable DMA for transmit.
  • UART_DMA_ERR_RXSTOP : Disable DMA receive on UART error.
Returns
None
891 {
892  // Check the arguments.
893  ASSERT(UARTBaseValid(ui32Base));
894 
895  // Set the requested bits in the UART DMA control register.
896  HWREG(ui32Base + UART_O_DMACTL) |= ui32DMAFlags;
897 }
#define ASSERT(expr)
Definition: debug.h:73
static void UARTEnable ( uint32_t  ui32Base)
inlinestatic

Enables transmitting and receiving.

This function sets the UARTEN, TXE, and RXE bits, and enables the transmit and receive FIFOs.

Parameters
ui32Baseis the base address of the UART port.
Returns
None
431 {
432  // Check the arguments.
433  ASSERT(UARTBaseValid(ui32Base));
434 
435  // Enable the FIFO.
436  HWREG(ui32Base + UART_O_LCRH) |= UART_LCRH_FEN;
437 
438  // Enable RX, TX, and the UART.
439  HWREG(ui32Base + UART_O_CTL) |= (UART_CTL_UARTEN | UART_CTL_TXE |
440  UART_CTL_RXE);
441 }
#define ASSERT(expr)
Definition: debug.h:73
static void UARTFIFODisable ( uint32_t  ui32Base)
inlinestatic

Disables the transmit and receive FIFOs.

This functions disables the transmit and receive FIFOs in the UART.

Parameters
ui32Baseis the base address of the UART port.
Returns
None
491 {
492  // Check the arguments.
493  ASSERT(UARTBaseValid(ui32Base));
494 
495  // Disable the FIFO.
496  HWREG(ui32Base + UART_O_LCRH) &= ~(UART_LCRH_FEN);
497 }
#define ASSERT(expr)
Definition: debug.h:73
static void UARTFIFOEnable ( uint32_t  ui32Base)
inlinestatic

Enables the transmit and receive FIFOs.

This functions enables the transmit and receive FIFOs in the UART.

Parameters
ui32Baseis the base address of the UART port.
Returns
None
470 {
471  // Check the arguments.
472  ASSERT(UARTBaseValid(ui32Base));
473 
474  // Enable the FIFO.
475  HWREG(ui32Base + UART_O_LCRH) |= UART_LCRH_FEN;
476 }
#define ASSERT(expr)
Definition: debug.h:73
void UARTFIFOLevelGet ( uint32_t  ui32Base,
uint32_t *  pui32TxLevel,
uint32_t *  pui32RxLevel 
)

Gets the FIFO level at which interrupts are generated.

This function gets the FIFO level at which transmit and receive interrupts are generated.

Parameters
ui32Baseis the base address of the UART port.
pui32TxLevelis a pointer to storage for the transmit FIFO level, returned as one of:
pui32RxLevelis a pointer to storage for the receive FIFO level, returned as one of:
Returns
None
78 {
79  uint32_t ui32Temp;
80 
81  // Check the arguments.
82  ASSERT(UARTBaseValid(ui32Base));
83 
84  // Read the FIFO level register.
85  ui32Temp = HWREG(ui32Base + UART_O_IFLS);
86 
87  // Extract the transmit and receive FIFO levels.
88  *pui32TxLevel = ui32Temp & UART_IFLS_TXSEL_M;
89  *pui32RxLevel = ui32Temp & UART_IFLS_RXSEL_M;
90 }
#define ASSERT(expr)
Definition: debug.h:73
static void UARTFIFOLevelSet ( uint32_t  ui32Base,
uint32_t  ui32TxLevel,
uint32_t  ui32RxLevel 
)
inlinestatic

Sets the FIFO level at which interrupts are generated.

This function sets the FIFO level at which transmit and receive interrupts are generated.

Parameters
ui32Baseis the base address of the UART port.
ui32TxLevelis the transmit FIFO interrupt level, specified as one of:
ui32RxLevelis the receive FIFO interrupt level, specified as one of:
Returns
None
307 {
308  // Check the arguments.
309  ASSERT(UARTBaseValid(ui32Base));
310  ASSERT((ui32TxLevel == UART_FIFO_TX1_8) ||
311  (ui32TxLevel == UART_FIFO_TX2_8) ||
312  (ui32TxLevel == UART_FIFO_TX4_8) ||
313  (ui32TxLevel == UART_FIFO_TX6_8) ||
314  (ui32TxLevel == UART_FIFO_TX7_8));
315  ASSERT((ui32RxLevel == UART_FIFO_RX1_8) ||
316  (ui32RxLevel == UART_FIFO_RX2_8) ||
317  (ui32RxLevel == UART_FIFO_RX4_8) ||
318  (ui32RxLevel == UART_FIFO_RX6_8) ||
319  (ui32RxLevel == UART_FIFO_RX7_8));
320 
321  // Set the FIFO interrupt levels.
322  HWREG(ui32Base + UART_O_IFLS) = ui32TxLevel | ui32RxLevel;
323 }
#define UART_FIFO_RX2_8
Definition: uart.h:155
#define UART_FIFO_TX7_8
Definition: uart.h:146
#define UART_FIFO_RX6_8
Definition: uart.h:157
#define UART_FIFO_RX7_8
Definition: uart.h:158
#define ASSERT(expr)
Definition: debug.h:73
#define UART_FIFO_TX6_8
Definition: uart.h:145
#define UART_FIFO_TX4_8
Definition: uart.h:144
#define UART_FIFO_TX1_8
Definition: uart.h:142
#define UART_FIFO_RX4_8
Definition: uart.h:156
#define UART_FIFO_RX1_8
Definition: uart.h:154
#define UART_FIFO_TX2_8
Definition: uart.h:143
static void UARTHwFlowControlDisable ( uint32_t  ui32Base)
inlinestatic

Disables hardware flow control for both CTS and RTS.

Hardware flow control is disabled by default.

Parameters
ui32Baseis the base address of the UART port.
Returns
None
1013 {
1014  // Check the arguments.
1015  ASSERT( UARTBaseValid( ui32Base ));
1016 
1017  HWREG( ui32Base + UART_O_CTL ) &= ~( UART_CTL_CTSEN | UART_CTL_RTSEN );
1018 }
#define ASSERT(expr)
Definition: debug.h:73
static void UARTHwFlowControlEnable ( uint32_t  ui32Base)
inlinestatic

Enables hardware flow control for both CTS and RTS.

Hardware flow control is disabled by default.

Parameters
ui32Baseis the base address of the UART port.
Returns
None
993 {
994  // Check the arguments.
995  ASSERT( UARTBaseValid( ui32Base ));
996 
997  HWREG( ui32Base + UART_O_CTL ) |= ( UART_CTL_CTSEN | UART_CTL_RTSEN );
998 }
#define ASSERT(expr)
Definition: debug.h:73
static void UARTIntClear ( uint32_t  ui32Base,
uint32_t  ui32IntFlags 
)
inlinestatic

Clears UART interrupt sources.

The specified UART interrupt sources are cleared, so that they no longer assert. This function must be called in the interrupt handler to keep the interrupt from being recognized again immediately upon exit.

Note
Due to write buffers and synchronizers in the system it may take several clock cycles from a register write clearing an event in a module and until the event is actually cleared in the NVIC of the system CPU. It is recommended to clear the event source early in the interrupt service routine (ISR) to allow the event clear to propagate to the NVIC before returning from the ISR. At the same time, an early event clear allows new events of the same type to be pended instead of ignored if the event is cleared later in the ISR. It is the responsibility of the programmer to make sure that enough time has passed before returning from the ISR to avoid false re-triggering of the cleared event. A simple, although not necessarily optimal, way of clearing an event before returning from the ISR is:
  1. Write to clear event (interrupt source). (buffered write)
  2. Dummy read from the event source module. (making sure the write has propagated)
  3. Wait two system CPU clock cycles (user code or two NOPs). (allowing cleared event to propagate through any synchronizers)
Parameters
ui32Baseis the base address of the UART port.
ui32IntFlagsis a bit mask of the interrupt sources to be cleared.
Returns
None
860 {
861  // Check the arguments
862  ASSERT(UARTBaseValid(ui32Base));
863 
864  // Clear the requested interrupt sources
865  HWREG(ui32Base + UART_O_ICR) = ui32IntFlags;
866 }
#define ASSERT(expr)
Definition: debug.h:73
static void UARTIntDisable ( uint32_t  ui32Base,
uint32_t  ui32IntFlags 
)
inlinestatic

Disables individual UART interrupt sources.

This function disables the indicated UART interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.

Parameters
ui32Baseis the base address of the UART port.
ui32IntFlagsis the bit mask of the interrupt sources to be disabled.
Returns
None
771 {
772  // Check the arguments.
773  ASSERT(UARTBaseValid(ui32Base));
774 
775  // Disable the specified interrupts.
776  HWREG(ui32Base + UART_O_IMSC) &= ~(ui32IntFlags);
777 }
#define ASSERT(expr)
Definition: debug.h:73
static void UARTIntEnable ( uint32_t  ui32Base,
uint32_t  ui32IntFlags 
)
inlinestatic

Enables individual UART interrupt sources.

This function enables the indicated UART interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.

Parameters
ui32Baseis the base address of the UART port.
ui32IntFlagsis the bit mask of the interrupt sources to be enabled. The parameter is the bitwise OR of any of the following:
Returns
None
739 {
740  // Check the arguments.
741  ASSERT(UARTBaseValid(ui32Base));
742 
743  // Enable the specified interrupts.
744  HWREG(ui32Base + UART_O_IMSC) |= ui32IntFlags;
745 }
#define ASSERT(expr)
Definition: debug.h:73
void UARTIntRegister ( uint32_t  ui32Base,
void(*)(void)  pfnHandler 
)

Registers an interrupt handler for a UART interrupt.

This function does the actual registering of the interrupt handler. This function enables the global interrupt in the interrupt controller; specific UART interrupts must be enabled via UARTIntEnable(). It is the interrupt handler's responsibility to clear the interrupt source.

Parameters
ui32Baseis the base address of the UART port.
pfnHandleris a pointer to the function to be called when the UART interrupt occurs.
Returns
None
See also
IntRegister() for important information about registering interrupt handlers.
269 {
270  // Check the arguments.
271  ASSERT(UARTBaseValid(ui32Base));
272 
273  // Register the interrupt handler.
274  IntRegister(INT_UART0_COMB, pfnHandler);
275 
276  // Enable the UART interrupt.
277  IntEnable(INT_UART0_COMB);
278 }
#define ASSERT(expr)
Definition: debug.h:73
void IntRegister(uint32_t ui32Interrupt, void(*pfnHandler)(void))
Registers a function to be called when an interrupt occurs.
Definition: interrupt.c:152
void IntEnable(uint32_t ui32Interrupt)
Enables an interrupt.
Definition: interrupt.c:282

Here is the call graph for this function:

static uint32_t UARTIntStatus ( uint32_t  ui32Base,
bool  bMasked 
)
inlinestatic

Gets the current interrupt status.

This function returns the interrupt status for the specified UART. Either the raw interrupt status or the status of interrupts that are allowed to reflect to the processor can be returned.

Parameters
ui32Baseis the base address of the UART port.
bMaskedselects either raw or masked interrupt.
  • true : Masked interrupt status is required.
  • false : Raw interrupt status is required.
Returns
Returns the current interrupt status, enumerated as a bit field of:
805 {
806  // Check the arguments.
807  ASSERT(UARTBaseValid(ui32Base));
808 
809  // Return either the interrupt status or the raw interrupt status as
810  // requested.
811  if(bMasked)
812  {
813  return(HWREG(ui32Base + UART_O_MIS));
814  }
815  else
816  {
817  return(HWREG(ui32Base + UART_O_RIS));
818  }
819 }
#define ASSERT(expr)
Definition: debug.h:73
void UARTIntUnregister ( uint32_t  ui32Base)

Unregisters an interrupt handler for a UART interrupt.

This function does the actual unregistering of the interrupt handler. It clears the handler to be called when a UART interrupt occurs. This function also masks off the interrupt in the interrupt controller so that the interrupt handler no longer is called.

Parameters
ui32Baseis the base address of the UART port.
Returns
None
See also
IntRegister() for important information about registering interrupt handlers.
287 {
288  // Check the arguments.
289  ASSERT(UARTBaseValid(ui32Base));
290 
291  // Disable the interrupt.
292  IntDisable(INT_UART0_COMB);
293 
294  // Unregister the interrupt handler.
295  IntUnregister(INT_UART0_COMB);
296 }
#define ASSERT(expr)
Definition: debug.h:73
void IntUnregister(uint32_t ui32Interrupt)
Unregisters the function to be called when an interrupt occurs.
Definition: interrupt.c:188
void IntDisable(uint32_t ui32Interrupt)
Disables an interrupt.
Definition: interrupt.c:326

Here is the call graph for this function:

static uint32_t UARTParityModeGet ( uint32_t  ui32Base)
inlinestatic

Gets the type of parity currently being used.

This function gets the type of parity used for transmitting data and expected when receiving data.

Parameters
ui32Baseis the base address of the UART port.
Returns
Returns the current parity settings, specified as one of:
271 {
272  // Check the arguments.
273  ASSERT(UARTBaseValid(ui32Base));
274 
275  // Return the current parity setting
276  return(HWREG(ui32Base + UART_O_LCRH) &
278 }
#define ASSERT(expr)
Definition: debug.h:73
static void UARTParityModeSet ( uint32_t  ui32Base,
uint32_t  ui32Parity 
)
inlinestatic

Sets the type of parity.

This function sets the type of parity to use for transmitting and expect when receiving.

Parameters
ui32Baseis the base address of the UART port.
ui32Parityspecifies the type of parity to use. The last two allow direct control of the parity bit; it is always either one or zero based on the mode.
Returns
None
237 {
238  // Check the arguments.
239  ASSERT(UARTBaseValid(ui32Base));
240  ASSERT((ui32Parity == UART_CONFIG_PAR_NONE) ||
241  (ui32Parity == UART_CONFIG_PAR_EVEN) ||
242  (ui32Parity == UART_CONFIG_PAR_ODD) ||
243  (ui32Parity == UART_CONFIG_PAR_ONE) ||
244  (ui32Parity == UART_CONFIG_PAR_ZERO));
245 
246  // Set the parity mode.
247  HWREG(ui32Base + UART_O_LCRH) = ((HWREG(ui32Base + UART_O_LCRH) &
249  UART_LCRH_PEN)) | ui32Parity);
250 }
#define UART_CONFIG_PAR_ODD
Definition: uart.h:132
#define UART_CONFIG_PAR_EVEN
Definition: uart.h:131
#define ASSERT(expr)
Definition: debug.h:73
#define UART_CONFIG_PAR_NONE
Definition: uart.h:130
#define UART_CONFIG_PAR_ZERO
Definition: uart.h:134
#define UART_CONFIG_PAR_ONE
Definition: uart.h:133
static void UARTRxErrorClear ( uint32_t  ui32Base)
inlinestatic

Clears all reported receiver errors.

This function is used to clear all receiver error conditions reported via UARTRxErrorGet(). If using the overrun, framing error, parity error or break interrupts, this function must be called after clearing the interrupt to ensure that later errors of the same type trigger another interrupt.

Parameters
ui32Baseis the base address of the UART port.
Returns
None
971 {
972  // Check the arguments.
973  ASSERT(UARTBaseValid(ui32Base));
974 
975  // Any write to the Error Clear Register will clear all bits which are
976  // currently set.
977  HWREG(ui32Base + UART_O_ECR) = 0;
978 }
#define ASSERT(expr)
Definition: debug.h:73
static uint32_t UARTRxErrorGet ( uint32_t  ui32Base)
inlinestatic

Gets current receiver errors.

This function returns the current state of each of the 4 receiver error sources. The returned errors are equivalent to the four error bits returned via the previous call to UARTCharGet() or UARTCharGetNonBlocking() with the exception that the overrun error is set immediately the overrun occurs rather than when a character is next read.

Parameters
ui32Baseis the base address of the UART port.
Returns
Returns a bitwise OR combination of the receiver error flags:
947 {
948  // Check the arguments.
949  ASSERT(UARTBaseValid(ui32Base));
950 
951  // Return the current value of the receive status register.
952  return(HWREG(ui32Base + UART_O_RSR) & 0x0000000F);
953 }
#define ASSERT(expr)
Definition: debug.h:73
static bool UARTSpaceAvail ( uint32_t  ui32Base)
inlinestatic

Determines if there is any space in the transmit FIFO.

This function returns a flag indicating whether or not there is space available in the transmit FIFO.

Parameters
ui32Baseis the base address of the UART port.
Returns
Returns status of the transmit FIFO.
  • true : There is space available in the transmit FIFO.
  • false : There is no space available in the transmit FIFO.
539 {
540  // Check the arguments.
541  ASSERT(UARTBaseValid(ui32Base));
542 
543  // Return the availability of space.
544  return((HWREG(ui32Base + UART_O_FR) & UART_FR_TXFF) ? false : true);
545 }
#define ASSERT(expr)
Definition: debug.h:73

Macro Definition Documentation

#define UART_BUSY   0x00000001

Referenced by UARTBusy().

#define UART_CONFIG_PAR_EVEN   0x00000006

Referenced by UARTParityModeSet().

#define UART_CONFIG_PAR_MASK   0x00000086
#define UART_CONFIG_PAR_NONE   0x00000000

Referenced by UARTParityModeSet().

#define UART_CONFIG_PAR_ODD   0x00000002

Referenced by UARTParityModeSet().

#define UART_CONFIG_PAR_ONE   0x00000082

Referenced by UARTParityModeSet().

#define UART_CONFIG_PAR_ZERO   0x00000086

Referenced by UARTParityModeSet().

#define UART_CONFIG_STOP_MASK   0x00000008
#define UART_CONFIG_STOP_ONE   0x00000000
#define UART_CONFIG_STOP_TWO   0x00000008
#define UART_CONFIG_WLEN_5   0x00000000
#define UART_CONFIG_WLEN_6   0x00000020
#define UART_CONFIG_WLEN_7   0x00000040
#define UART_CONFIG_WLEN_8   0x00000060
#define UART_CONFIG_WLEN_MASK   0x00000060
#define UART_DMA_ERR_RXSTOP   0x00000004
#define UART_DMA_RX   0x00000001
#define UART_DMA_TX   0x00000002
#define UART_FIFO_RX1_8   0x00000000

Referenced by UARTFIFOLevelSet().

#define UART_FIFO_RX2_8   0x00000008

Referenced by UARTFIFOLevelSet().

#define UART_FIFO_RX4_8   0x00000010

Referenced by UARTFIFOLevelSet().

#define UART_FIFO_RX6_8   0x00000018

Referenced by UARTFIFOLevelSet().

#define UART_FIFO_RX7_8   0x00000020

Referenced by UARTFIFOLevelSet().

#define UART_FIFO_TX1_8   0x00000000

Referenced by UARTFIFOLevelSet().

#define UART_FIFO_TX2_8   0x00000001

Referenced by UARTFIFOLevelSet().

#define UART_FIFO_TX4_8   0x00000002

Referenced by UARTFIFOLevelSet().

#define UART_FIFO_TX6_8   0x00000003

Referenced by UARTFIFOLevelSet().

#define UART_FIFO_TX7_8   0x00000004

Referenced by UARTFIFOLevelSet().

#define UART_IDLE   0x00000000

Referenced by UARTBusy().

#define UART_INT_BE   ( UART_IMSC_BEIM )
#define UART_INT_CTS   ( UART_IMSC_CTSMIM )
#define UART_INT_FE   ( UART_IMSC_FEIM )
#define UART_INT_OE   ( UART_IMSC_OEIM )
#define UART_INT_PE   ( UART_IMSC_PEIM )
#define UART_INT_RT   ( UART_IMSC_RTIM )
#define UART_INT_RX   ( UART_IMSC_RXIM )
#define UART_INT_TX   ( UART_IMSC_TXIM )
#define UART_RXERROR_BREAK   0x00000004
#define UART_RXERROR_FRAMING   0x00000001
#define UART_RXERROR_OVERRUN   0x00000008
#define UART_RXERROR_PARITY   0x00000002