#include <stdbool.h>#include <stdint.h>#include "../inc/hw_types.h"#include "../inc/hw_ints.h"#include "../inc/hw_memmap.h"#include "../inc/hw_wdt.h"#include "debug.h"#include "interrupt.h"Macros | |
| #define | WATCHDOG_LOCK_UNLOCKED 0x00000000 |
| #define | WATCHDOG_LOCK_LOCKED 0x00000001 |
| #define | WATCHDOG_LOCK_UNLOCK 0x1ACCE551 |
| #define | WATCHDOG_INT_TIMEOUT 0x00000001 |
| #define | WATCHDOG_INT_TYPE_INT 0x00000000 |
| #define | WATCHDOG_INT_TYPE_NMI 0x00000004 |
Functions | |
| static bool | WatchdogRunning (void) |
| Determines if the watchdog timer is enabled. More... | |
| static void | WatchdogEnable (void) |
| Enables the watchdog timer. More... | |
| static void | WatchdogResetEnable (void) |
| Enables the watchdog timer reset. More... | |
| static void | WatchdogResetDisable (void) |
| Disables the watchdog timer reset. More... | |
| static void | WatchdogLock (void) |
| Enables the watchdog timer lock mechanism. More... | |
| static void | WatchdogUnlock (void) |
| Disables the watchdog timer lock mechanism. More... | |
| static bool | WatchdogLockState (void) |
| Gets the state of the watchdog timer lock mechanism. More... | |
| static void | WatchdogReloadSet (uint32_t ui32LoadVal) |
| Sets the watchdog timer reload value. More... | |
| static uint32_t | WatchdogReloadGet (void) |
| Gets the watchdog timer reload value. More... | |
| static uint32_t | WatchdogValueGet (void) |
| Gets the current watchdog timer value. More... | |
| static void | WatchdogIntRegister (void(*pfnHandler)(void)) |
| Registers an interrupt handler for the watchdog timer interrupt. More... | |
| static void | WatchdogIntUnregister (void) |
| Unregisters an interrupt handler for the watchdog timer interrupt. More... | |
| static void | WatchdogIntEnable (void) |
| Enables the watchdog timer. More... | |
| static uint32_t | WatchdogIntStatus (void) |
| Gets the current watchdog timer interrupt status. More... | |
| static void | WatchdogIntClear (void) |
| Clears the watchdog timer interrupt. More... | |
| static void | WatchdogIntTypeSet (uint32_t ui32Type) |
| Sets the type of interrupt generated by the watchdog. More... | |
| static void | WatchdogStallEnable (void) |
| Enables stalling of the watchdog timer during debug events. More... | |
| static void | WatchdogStallDisable (void) |
| Disables stalling of the watchdog timer during debug events. More... | |