#include "../inc/hw_types.h"#include "../inc/hw_ccfg.h"#include "aon_batmon.h"#include "sys_ctrl.h"#include "setup_rom.h"Data Structures | |
| struct | PowerQualGlobals_t |
Macros | |
| #define | PD_STATE_CACHE_RET 1 |
| #define | PD_STATE_RFMEM_RET 2 |
| #define | PD_STATE_XOSC_LPM 4 |
| #define | PD_STATE_EXT_REG_MODE 8 |
Functions | |
| void | SysCtrlSetRechargeBeforePowerDown (uint32_t xoscPowerMode) |
| Set Recharge values before entering Power Down. More... | |
| void | SysCtrlAdjustRechargeAfterPowerDown (void) |
| Adjust Recharge calculations to be used next. More... | |
| void | SysCtrl_DCDC_VoltageConditionalControl (void) |
| Turns DCDC on or off depending of what is considered to be optimal usage. More... | |
| uint32_t | SysCtrlResetSourceGet (void) |
| Returns last reset source (including "wakeup from shutdown"). More... | |
Variables | |
| static PowerQualGlobals_t | powerQualGlobals |
| #define PD_STATE_CACHE_RET 1 |
Referenced by SysCtrlSetRechargeBeforePowerDown().
| #define PD_STATE_EXT_REG_MODE 8 |
Referenced by SysCtrlSetRechargeBeforePowerDown().
| #define PD_STATE_RFMEM_RET 2 |
Referenced by SysCtrlSetRechargeBeforePowerDown().
| #define PD_STATE_XOSC_LPM 4 |
Referenced by SysCtrlSetRechargeBeforePowerDown().
|
static |