#include <stdint.h>#include <string.h>Data Structures | |
| struct | dataQueue_t |
| Type definition for a data queue. More... | |
Macros | |
RF mode values | |
Defines used to indicate mode of operation to radio core. | |
| #define | RF_MODE_PROPRIETARY_SUB_1 0x00 |
| #define | RF_MODE_BLE 0x01 |
| #define | RF_MODE_IEEE_15_4 0x02 |
| #define | RF_MODE_PROPRIETARY_2_4 0x03 |
| #define | RF_MODE_PROPRIETARY RF_MODE_PROPRIETARY_2_4 |
| #define | RF_MODE_MULTIPLE 0x05 |
CPE interrupt definitions | |
Interrupt masks for the CPE interrupt in RDBELL. | |
| #define | IRQN_COMMAND_DONE 0 |
| Radio operation command finished. More... | |
| #define | IRQN_LAST_COMMAND_DONE 1 |
| Last radio operation command in a chain finished. More... | |
| #define | IRQN_FG_COMMAND_DONE 2 |
| FG level Radio operation command finished. More... | |
| #define | IRQN_LAST_FG_COMMAND_DONE 3 |
| Last FG level radio operation command in a chain finished. More... | |
| #define | IRQN_TX_DONE 4 |
| Packet transmitted. More... | |
| #define | IRQN_TX_ACK 5 |
| ACK packet transmitted. More... | |
| #define | IRQN_TX_CTRL 6 |
| Control packet transmitted. More... | |
| #define | IRQN_TX_CTRL_ACK 7 |
| Acknowledgement received on a transmitted control packet. More... | |
| #define | IRQN_TX_CTRL_ACK_ACK 8 |
| Acknowledgement received on a transmitted control packet, and acknowledgement transmitted for that packet. More... | |
| #define | IRQN_TX_RETRANS 9 |
| Packet retransmitted. More... | |
| #define | IRQN_TX_ENTRY_DONE 10 |
| Tx queue data entry state changed to Finished. More... | |
| #define | IRQN_TX_BUFFER_CHANGED 11 |
| A buffer change is complete. More... | |
| #define | IRQN_RX_OK 16 |
| Packet received with CRC OK, payload, and not to be ignored. More... | |
| #define | IRQN_RX_NOK 17 |
| Packet received with CRC error. More... | |
| #define | IRQN_RX_IGNORED 18 |
| Packet received with CRC OK, but to be ignored. More... | |
| #define | IRQN_RX_EMPTY 19 |
| Packet received with CRC OK, not to be ignored, no payload. More... | |
| #define | IRQN_RX_CTRL 20 |
| Control packet received with CRC OK, not to be ignored. More... | |
| #define | IRQN_RX_CTRL_ACK 21 |
| Control packet received with CRC OK, not to be ignored, then ACK sent. More... | |
| #define | IRQN_RX_BUF_FULL 22 |
| Packet received that did not fit in the Rx queue. More... | |
| #define | IRQN_RX_ENTRY_DONE 23 |
| Rx queue data entry changing state to Finished. More... | |
| #define | IRQN_RX_DATA_WRITTEN 24 |
| Data written to partial read Rx buffer. More... | |
| #define | IRQN_RX_N_DATA_WRITTEN 25 |
| Specified number of bytes written to partial read Rx buffer. More... | |
| #define | IRQN_RX_ABORTED 26 |
| Packet reception stopped before packet was done. More... | |
| #define | IRQN_RX_COLLISION_DETECTED 27 |
| A collision was indicated during packet reception. More... | |
| #define | IRQN_SYNTH_NO_LOCK 28 |
| The synth has gone out of lock after calibration. More... | |
| #define | IRQN_MODULES_UNLOCKED 29 |
| As part of the boot process, the CM0 has opened access to RF core modules and memories. More... | |
| #define | IRQN_BOOT_DONE 30 |
| The RF core CPU boot is finished. More... | |
| #define | IRQN_INTERNAL_ERROR 31 |
| Internal error observed. More... | |
| #define | IRQ_COMMAND_DONE (1U << IRQN_COMMAND_DONE) |
| #define | IRQ_LAST_COMMAND_DONE (1U << IRQN_LAST_COMMAND_DONE) |
| #define | IRQ_FG_COMMAND_DONE (1U << IRQN_FG_COMMAND_DONE) |
| #define | IRQ_LAST_FG_COMMAND_DONE (1U << IRQN_LAST_FG_COMMAND_DONE) |
| #define | IRQ_TX_DONE (1U << IRQN_TX_DONE) |
| #define | IRQ_TX_ACK (1U << IRQN_TX_ACK) |
| #define | IRQ_TX_CTRL (1U << IRQN_TX_CTRL) |
| #define | IRQ_TX_CTRL_ACK (1U << IRQN_TX_CTRL_ACK) |
| #define | IRQ_TX_CTRL_ACK_ACK (1U << IRQN_TX_CTRL_ACK_ACK) |
| #define | IRQ_TX_RETRANS (1U << IRQN_TX_RETRANS) |
| #define | IRQ_TX_ENTRY_DONE (1U << IRQN_TX_ENTRY_DONE) |
| #define | IRQ_TX_BUFFER_CHANGED (1U << IRQN_TX_BUFFER_CHANGED) |
| #define | IRQ_RX_OK (1U << IRQN_RX_OK) |
| #define | IRQ_RX_NOK (1U << IRQN_RX_NOK) |
| #define | IRQ_RX_IGNORED (1U << IRQN_RX_IGNORED) |
| #define | IRQ_RX_EMPTY (1U << IRQN_RX_EMPTY) |
| #define | IRQ_RX_CTRL (1U << IRQN_RX_CTRL) |
| #define | IRQ_RX_CTRL_ACK (1U << IRQN_RX_CTRL_ACK) |
| #define | IRQ_RX_BUF_FULL (1U << IRQN_RX_BUF_FULL) |
| #define | IRQ_RX_ENTRY_DONE (1U << IRQN_RX_ENTRY_DONE) |
| #define | IRQ_RX_DATA_WRITTEN (1U << IRQN_RX_DATA_WRITTEN) |
| #define | IRQ_RX_N_DATA_WRITTEN (1U << IRQN_RX_N_DATA_WRITTEN) |
| #define | IRQ_RX_ABORTED (1U << IRQN_RX_ABORTED) |
| #define | IRQ_RX_COLLISION_DETECTED (1U << IRQN_RX_COLLISION_DETECTED) |
| #define | IRQ_SYNTH_NO_LOCK (1U << IRQN_SYNTH_NO_LOCK) |
| #define | IRQ_MODULES_UNLOCKED (1U << IRQN_MODULES_UNLOCKED) |
| #define | IRQ_BOOT_DONE (1U << IRQN_BOOT_DONE) |
| #define | IRQ_INTERNAL_ERROR (1U << IRQN_INTERNAL_ERROR) |
CMDSTA values | |
Values returned in result byte of CMDSTA | |
| #define | CMDSTA_Pending 0x00 |
| The command has not yet been parsed. More... | |
| #define | CMDSTA_Done 0x01 |
| Command successfully parsed. More... | |
| #define | CMDSTA_IllegalPointer 0x81 |
| The pointer signaled in CMDR is not valid. More... | |
| #define | CMDSTA_UnknownCommand 0x82 |
| The command number in the command structure is unknown. More... | |
| #define | CMDSTA_UnknownDirCommand 0x83 |
| command is not a direct command More... | |
| #define | CMDSTA_ContextError 0x85 |
| where it is not supported More... | |
| #define | CMDSTA_SchedulingError 0x86 |
| while another operation was already running in the RF core More... | |
| #define | CMDSTA_ParError 0x87 |
| on submission. More... | |
| #define | CMDSTA_QueueError 0x88 |
| not supported by the queue in its current state More... | |
| #define | CMDSTA_QueueBusy 0x89 |
Macros for sending direct commands | |
Direct command with no parameter | |
| #define | CMDR_DIR_CMD(cmdId) (((cmdId) << 16) | 1) |
| #define | CMDR_DIR_CMD_1BYTE(cmdId, par) (((cmdId) << 16) | ((par) << 8) | 1) |
| Direct command with 1-byte parameter. More... | |
| #define | CMDR_DIR_CMD_2BYTE(cmdId, par) (((cmdId) << 16) | ((par) & 0xFFFC) | 1) |
| Direct command with 2-byte parameter. More... | |
Definitions for trigger types | |
| #define | TRIG_NOW 0 |
| Triggers immediately. More... | |
| #define | TRIG_NEVER 1 |
| Never trigs. More... | |
| #define | TRIG_ABSTIME 2 |
| Trigs at an absolute time. More... | |
| #define | TRIG_REL_SUBMIT 3 |
| Trigs at a time relative to the command was submitted. More... | |
| #define | TRIG_REL_START 4 |
| Trigs at a time relative to the command started. More... | |
| #define | TRIG_REL_PREVSTART 5 |
| Trigs at a time relative to the previous command in the chain started. More... | |
| #define | TRIG_REL_FIRSTSTART 6 |
| Trigs at a time relative to the first command in the chain started. More... | |
| #define | TRIG_REL_PREVEND 7 |
| Trigs at a time relative to the previous command in the chain ended. More... | |
| #define | TRIG_REL_EVT1 8 |
| Trigs at a time relative to the context defined "Event 1". More... | |
| #define | TRIG_REL_EVT2 9 |
| Trigs at a time relative to the context defined "Event 2". More... | |
| #define | TRIG_EXTERNAL 10 |
| Trigs at an external event to the radio timer. More... | |
| #define | TRIG_PAST_BM 0x80 |
Definitions for conditional execution | |
| #define | COND_ALWAYS 0 |
| Always run next command (except in case of Abort) More... | |
| #define | COND_NEVER 1 |
| Never run next command. More... | |
| #define | COND_STOP_ON_FALSE 2 |
| False. More... | |
| #define | COND_STOP_ON_TRUE 3 |
| False. More... | |
| #define | COND_SKIP_ON_FALSE 4 |
| commands if it returned False More... | |
| #define | COND_SKIP_ON_TRUE 5 |
Operation not finished | |
| #define | IDLE 0x0000 |
| Operation not started. More... | |
| #define | PENDING 0x0001 |
| Start of command is pending. More... | |
| #define | ACTIVE 0x0002 |
| Running. More... | |
| #define | SKIPPED 0x0003 |
Operation finished normally | |
| #define | DONE_OK 0x0400 |
| Operation ended normally. More... | |
| #define | DONE_COUNTDOWN 0x0401 |
| Counter reached zero. More... | |
| #define | DONE_RXERR 0x0402 |
| Operation ended with CRC error. More... | |
| #define | DONE_TIMEOUT 0x0403 |
| Operation ended with timeout. More... | |
| #define | DONE_STOPPED 0x0404 |
| Operation stopped after CMD_STOP command. More... | |
| #define | DONE_ABORT 0x0405 |
| Operation aborted by CMD_ABORT command. More... | |
| #define | DONE_FAILED 0x0406 |
Operation finished with error | |
| #define | ERROR_PAST_START 0x0800 |
| The start trigger occurred in the past. More... | |
| #define | ERROR_START_TRIG 0x0801 |
| Illegal start trigger parameter. More... | |
| #define | ERROR_CONDITION 0x0802 |
| Illegal condition for next operation. More... | |
| #define | ERROR_PAR 0x0803 |
| Error in a command specific parameter. More... | |
| #define | ERROR_POINTER 0x0804 |
| Invalid pointer to next operation. More... | |
| #define | ERROR_CMDID 0x0805 |
| operation command More... | |
| #define | ERROR_WRONG_BG 0x0806 |
| FG level command not compatible with running BG level command. More... | |
| #define | ERROR_NO_SETUP 0x0807 |
| Operation using Rx or Tx attemted without CMD_RADIO_SETUP. More... | |
| #define | ERROR_NO_FS 0x0808 |
| Operation using Rx or Tx attemted without frequency synth configured. More... | |
| #define | ERROR_SYNTH_PROG 0x0809 |
| Synthesizer calibration failed. More... | |
| #define | ERROR_TXUNF 0x080A |
| Tx underflow observed. More... | |
| #define | ERROR_RXOVF 0x080B |
| Rx overflow observed. More... | |
| #define | ERROR_NO_RX 0x080C |
| Attempted to access data from Rx when no such data was yet received. More... | |
| #define | ERROR_PENDING 0x080D |
Data entry types | |
| #define | DATA_ENTRY_TYPE_GEN 0 |
| General type: Tx entry or single element Rx entry. More... | |
| #define | DATA_ENTRY_TYPE_MULTI 1 |
| Multi-element Rx entry type. More... | |
| #define | DATA_ENTRY_TYPE_PTR 2 |
| Pointer entry type. More... | |
| #define | DATA_ENTRY_TYPE_PARTIAL 3 |
Data entry statuses | |
@ | |
| #define | DATA_ENTRY_PENDING 0 |
| Entry not yet used. More... | |
| #define | DATA_ENTRY_ACTIVE 1 |
| Entry in use by radio CPU. More... | |
| #define | DATA_ENTRY_BUSY 2 |
| Entry being updated. More... | |
| #define | DATA_ENTRY_FINISHED 3 |
| Radio CPU is finished accessing the entry. More... | |
| #define | DATA_ENTRY_UNFINISHED 4 |
Macros for RF register override | |
Macro for ADI half-size value-mask combination | |
| #define | ADI_VAL_MASK(addr, mask, value) |
| #define | HW_REG_OVERRIDE(addr, val) ((((uintptr_t) (addr)) & 0xFFFC) | ((uint32_t)(val) << 16)) |
| 32-bit write of 16-bit value More... | |
| #define | ADI_REG_OVERRIDE(adiNo, addr, val) |
| ADI register, full-size write. More... | |
| #define | ADI_2REG_OVERRIDE(adiNo, addr, val, addr2, val2) |
| 2 ADI registers, full-size write More... | |
| #define | ADI_HALFREG_OVERRIDE(adiNo, addr, mask, val) |
| ADI register, half-size read-modify-write. More... | |
| #define | ADI_2HALFREG_OVERRIDE(adiNo, addr, mask, val, addr2, mask2, val2) |
| 2 ADI registers, half-size read-modify-write More... | |
| #define | SW_REG_OVERRIDE(cmd, field, val) (3 | ((_POSITION_##cmd##_##field) << 4) | ((uint32_t)(val) << 16)) |
| 16-bit SW register as defined in radio_par_def.txt More... | |
| #define | SW_REG_IND_OVERRIDE(cmd, field, offset, val) |
| SW register as defined in radio_par_def.txt with added index (for use with registers > 16 bits). More... | |
| #define | SW_REG_BYTE_OVERRIDE(cmd, field, val) |
| 8-bit SW register as defined in radio_par_def.txt More... | |
| #define | SW_REG_2BYTE_OVERRIDE(cmd, field, val0, val1) |
| Two 8-bit SW registers as defined in radio_par_def.txt; the one given by field and the next byte. More... | |
| #define | HW16_ARRAY_OVERRIDE(addr, length) (1 | (((uintptr_t) (addr)) & 0xFFFC) | ((uint32_t)(length) << 16)) |
| #define | HW32_ARRAY_OVERRIDE(addr, length) |
| #define | ADI_ARRAY_OVERRIDE(adiNo, addr, bHalfSize, length) |
| #define | SW_ARRAY_OVERRIDE(cmd, firstfield, length) |
| #define | MCE_RFE_OVERRIDE(bMceRam, mceRomBank, mceMode, bRfeRam, rfeRomBank, rfeMode) |
| #define | NEW_OVERRIDE_SEGMENT(address) |
| #define | END_OVERRIDE 0xFFFFFFFF |
| End of string for override register. More... | |
| #define | ADI_ADDR_VAL(addr, value) ((((addr) & 0x7F) << 8) | ((value) & 0xFF)) |
| ADI address-value pair. More... | |
| #define | ADI_ADDR_VAL_MASK(addr, mask, value) ((((addr) & 0x7F) << 8) | ADI_VAL_MASK(addr, mask, value)) |
| #define | LOWORD(value) ((value) & 0xFFFF) |
| Low half-word. More... | |
| #define | HIWORD(value) ((value) >> 16) |
| High half-word. More... | |
Typedefs | |
| typedef uint32_t | ratmr_t |
| Type definition for RAT. More... | |
| #define ACTIVE 0x0002 |
Running.
| #define ADI_2HALFREG_OVERRIDE | ( | adiNo, | |
| addr, | |||
| mask, | |||
| val, | |||
| addr2, | |||
| mask2, | |||
| val2 | |||
| ) |
2 ADI registers, half-size read-modify-write
| #define ADI_2REG_OVERRIDE | ( | adiNo, | |
| addr, | |||
| val, | |||
| addr2, | |||
| val2 | |||
| ) |
2 ADI registers, full-size write
| #define ADI_ADDR_VAL | ( | addr, | |
| value | |||
| ) | ((((addr) & 0x7F) << 8) | ((value) & 0xFF)) |
ADI address-value pair.
| #define ADI_ADDR_VAL_MASK | ( | addr, | |
| mask, | |||
| value | |||
| ) | ((((addr) & 0x7F) << 8) | ADI_VAL_MASK(addr, mask, value)) |
| #define ADI_ARRAY_OVERRIDE | ( | adiNo, | |
| addr, | |||
| bHalfSize, | |||
| length | |||
| ) |
| #define ADI_HALFREG_OVERRIDE | ( | adiNo, | |
| addr, | |||
| mask, | |||
| val | |||
| ) |
ADI register, half-size read-modify-write.
| #define ADI_REG_OVERRIDE | ( | adiNo, | |
| addr, | |||
| val | |||
| ) |
ADI register, full-size write.
| #define ADI_VAL_MASK | ( | addr, | |
| mask, | |||
| value | |||
| ) |
| #define CMDR_DIR_CMD | ( | cmdId | ) | (((cmdId) << 16) | 1) |
| #define CMDR_DIR_CMD_1BYTE | ( | cmdId, | |
| par | |||
| ) | (((cmdId) << 16) | ((par) << 8) | 1) |
Direct command with 1-byte parameter.
| #define CMDR_DIR_CMD_2BYTE | ( | cmdId, | |
| par | |||
| ) | (((cmdId) << 16) | ((par) & 0xFFFC) | 1) |
Direct command with 2-byte parameter.
| #define CMDSTA_ContextError 0x85 |
where it is not supported
An immediate or direct command was issued in a context
| #define CMDSTA_Done 0x01 |
Command successfully parsed.
| #define CMDSTA_IllegalPointer 0x81 |
The pointer signaled in CMDR is not valid.
| #define CMDSTA_ParError 0x87 |
on submission.
There were errors in the command parameters that are parsed
| #define CMDSTA_Pending 0x00 |
The command has not yet been parsed.
| #define CMDSTA_QueueBusy 0x89 |
An operation on a data entry was attempted while that entry was busy
| #define CMDSTA_QueueError 0x88 |
not supported by the queue in its current state
An operation on a data entry queue was attempted that was
| #define CMDSTA_SchedulingError 0x86 |
while another operation was already running in the RF core
A radio operation command was attempted to be scheduled
| #define CMDSTA_UnknownCommand 0x82 |
The command number in the command structure is unknown.
| #define CMDSTA_UnknownDirCommand 0x83 |
command is not a direct command
The command number for a direct command is unknown, or the
| #define COND_ALWAYS 0 |
Always run next command (except in case of Abort)
| #define COND_NEVER 1 |
Never run next command.
| #define COND_SKIP_ON_FALSE 4 |
commands if it returned False
Run next command if this command returned True, skip a number of
| #define COND_SKIP_ON_TRUE 5 |
Skip a number of commands if this command returned True, run next command if it returned False
| #define COND_STOP_ON_FALSE 2 |
False.
Run next command if this command returned True, stop if it returned
| #define COND_STOP_ON_TRUE 3 |
False.
Stop if this command returned True, run next command if it returned
| #define DATA_ENTRY_ACTIVE 1 |
Entry in use by radio CPU.
| #define DATA_ENTRY_BUSY 2 |
Entry being updated.
| #define DATA_ENTRY_FINISHED 3 |
Radio CPU is finished accessing the entry.
| #define DATA_ENTRY_PENDING 0 |
Entry not yet used.
| #define DATA_ENTRY_TYPE_GEN 0 |
General type: Tx entry or single element Rx entry.
| #define DATA_ENTRY_TYPE_MULTI 1 |
Multi-element Rx entry type.
| #define DATA_ENTRY_TYPE_PARTIAL 3 |
Partial read entry type
| #define DATA_ENTRY_TYPE_PTR 2 |
Pointer entry type.
| #define DATA_ENTRY_UNFINISHED 4 |
Radio CPU is finished accessing the entry, but packet could not be finished
| #define DONE_ABORT 0x0405 |
Operation aborted by CMD_ABORT command.
| #define DONE_COUNTDOWN 0x0401 |
Counter reached zero.
| #define DONE_FAILED 0x0406 |
Scheduled immediate command failed
| #define DONE_OK 0x0400 |
Operation ended normally.
| #define DONE_RXERR 0x0402 |
Operation ended with CRC error.
| #define DONE_STOPPED 0x0404 |
Operation stopped after CMD_STOP command.
| #define DONE_TIMEOUT 0x0403 |
Operation ended with timeout.
| #define END_OVERRIDE 0xFFFFFFFF |
End of string for override register.
| #define ERROR_CMDID 0x0805 |
operation command
Next operation has a command ID that is undefined or not a radio
| #define ERROR_CONDITION 0x0802 |
Illegal condition for next operation.
| #define ERROR_NO_FS 0x0808 |
Operation using Rx or Tx attemted without frequency synth configured.
| #define ERROR_NO_RX 0x080C |
Attempted to access data from Rx when no such data was yet received.
| #define ERROR_NO_SETUP 0x0807 |
Operation using Rx or Tx attemted without CMD_RADIO_SETUP.
| #define ERROR_PAR 0x0803 |
Error in a command specific parameter.
| #define ERROR_PAST_START 0x0800 |
The start trigger occurred in the past.
| #define ERROR_PENDING 0x080D |
Command submitted in the future with another command at different level pending
| #define ERROR_POINTER 0x0804 |
Invalid pointer to next operation.
| #define ERROR_RXOVF 0x080B |
Rx overflow observed.
| #define ERROR_START_TRIG 0x0801 |
Illegal start trigger parameter.
| #define ERROR_SYNTH_PROG 0x0809 |
Synthesizer calibration failed.
| #define ERROR_TXUNF 0x080A |
Tx underflow observed.
| #define ERROR_WRONG_BG 0x0806 |
FG level command not compatible with running BG level command.
| #define HIWORD | ( | value | ) | ((value) >> 16) |
High half-word.
| #define HW16_ARRAY_OVERRIDE | ( | addr, | |
| length | |||
| ) | (1 | (((uintptr_t) (addr)) & 0xFFFC) | ((uint32_t)(length) << 16)) |
| #define HW32_ARRAY_OVERRIDE | ( | addr, | |
| length | |||
| ) |
| #define HW_REG_OVERRIDE | ( | addr, | |
| val | |||
| ) | ((((uintptr_t) (addr)) & 0xFFFC) | ((uint32_t)(val) << 16)) |
32-bit write of 16-bit value
| #define IDLE 0x0000 |
Operation not started.
| #define IRQ_BOOT_DONE (1U << IRQN_BOOT_DONE) |
| #define IRQ_COMMAND_DONE (1U << IRQN_COMMAND_DONE) |
| #define IRQ_FG_COMMAND_DONE (1U << IRQN_FG_COMMAND_DONE) |
| #define IRQ_INTERNAL_ERROR (1U << IRQN_INTERNAL_ERROR) |
| #define IRQ_LAST_COMMAND_DONE (1U << IRQN_LAST_COMMAND_DONE) |
| #define IRQ_LAST_FG_COMMAND_DONE (1U << IRQN_LAST_FG_COMMAND_DONE) |
| #define IRQ_MODULES_UNLOCKED (1U << IRQN_MODULES_UNLOCKED) |
| #define IRQ_RX_ABORTED (1U << IRQN_RX_ABORTED) |
| #define IRQ_RX_BUF_FULL (1U << IRQN_RX_BUF_FULL) |
| #define IRQ_RX_COLLISION_DETECTED (1U << IRQN_RX_COLLISION_DETECTED) |
| #define IRQ_RX_CTRL (1U << IRQN_RX_CTRL) |
| #define IRQ_RX_CTRL_ACK (1U << IRQN_RX_CTRL_ACK) |
| #define IRQ_RX_DATA_WRITTEN (1U << IRQN_RX_DATA_WRITTEN) |
| #define IRQ_RX_EMPTY (1U << IRQN_RX_EMPTY) |
| #define IRQ_RX_ENTRY_DONE (1U << IRQN_RX_ENTRY_DONE) |
| #define IRQ_RX_IGNORED (1U << IRQN_RX_IGNORED) |
| #define IRQ_RX_N_DATA_WRITTEN (1U << IRQN_RX_N_DATA_WRITTEN) |
| #define IRQ_RX_NOK (1U << IRQN_RX_NOK) |
| #define IRQ_RX_OK (1U << IRQN_RX_OK) |
| #define IRQ_SYNTH_NO_LOCK (1U << IRQN_SYNTH_NO_LOCK) |
| #define IRQ_TX_ACK (1U << IRQN_TX_ACK) |
| #define IRQ_TX_BUFFER_CHANGED (1U << IRQN_TX_BUFFER_CHANGED) |
| #define IRQ_TX_CTRL (1U << IRQN_TX_CTRL) |
| #define IRQ_TX_CTRL_ACK (1U << IRQN_TX_CTRL_ACK) |
| #define IRQ_TX_CTRL_ACK_ACK (1U << IRQN_TX_CTRL_ACK_ACK) |
| #define IRQ_TX_DONE (1U << IRQN_TX_DONE) |
| #define IRQ_TX_ENTRY_DONE (1U << IRQN_TX_ENTRY_DONE) |
| #define IRQ_TX_RETRANS (1U << IRQN_TX_RETRANS) |
| #define IRQN_BOOT_DONE 30 |
The RF core CPU boot is finished.
| #define IRQN_COMMAND_DONE 0 |
Radio operation command finished.
| #define IRQN_FG_COMMAND_DONE 2 |
FG level Radio operation command finished.
| #define IRQN_INTERNAL_ERROR 31 |
Internal error observed.
| #define IRQN_LAST_COMMAND_DONE 1 |
Last radio operation command in a chain finished.
| #define IRQN_LAST_FG_COMMAND_DONE 3 |
Last FG level radio operation command in a chain finished.
| #define IRQN_MODULES_UNLOCKED 29 |
As part of the boot process, the CM0 has opened access to RF core modules and memories.
| #define IRQN_RX_ABORTED 26 |
Packet reception stopped before packet was done.
| #define IRQN_RX_BUF_FULL 22 |
Packet received that did not fit in the Rx queue.
| #define IRQN_RX_COLLISION_DETECTED 27 |
A collision was indicated during packet reception.
| #define IRQN_RX_CTRL 20 |
Control packet received with CRC OK, not to be ignored.
| #define IRQN_RX_CTRL_ACK 21 |
Control packet received with CRC OK, not to be ignored, then ACK sent.
| #define IRQN_RX_DATA_WRITTEN 24 |
Data written to partial read Rx buffer.
| #define IRQN_RX_EMPTY 19 |
Packet received with CRC OK, not to be ignored, no payload.
| #define IRQN_RX_ENTRY_DONE 23 |
Rx queue data entry changing state to Finished.
| #define IRQN_RX_IGNORED 18 |
Packet received with CRC OK, but to be ignored.
| #define IRQN_RX_N_DATA_WRITTEN 25 |
Specified number of bytes written to partial read Rx buffer.
| #define IRQN_RX_NOK 17 |
Packet received with CRC error.
| #define IRQN_RX_OK 16 |
Packet received with CRC OK, payload, and not to be ignored.
| #define IRQN_SYNTH_NO_LOCK 28 |
The synth has gone out of lock after calibration.
| #define IRQN_TX_ACK 5 |
ACK packet transmitted.
| #define IRQN_TX_BUFFER_CHANGED 11 |
A buffer change is complete.
| #define IRQN_TX_CTRL 6 |
Control packet transmitted.
| #define IRQN_TX_CTRL_ACK 7 |
Acknowledgement received on a transmitted control packet.
| #define IRQN_TX_CTRL_ACK_ACK 8 |
Acknowledgement received on a transmitted control packet, and acknowledgement transmitted for that packet.
| #define IRQN_TX_DONE 4 |
Packet transmitted.
| #define IRQN_TX_ENTRY_DONE 10 |
Tx queue data entry state changed to Finished.
| #define IRQN_TX_RETRANS 9 |
Packet retransmitted.
| #define LOWORD | ( | value | ) | ((value) & 0xFFFF) |
Low half-word.
| #define MCE_RFE_OVERRIDE | ( | bMceRam, | |
| mceRomBank, | |||
| mceMode, | |||
| bRfeRam, | |||
| rfeRomBank, | |||
| rfeMode | |||
| ) |
| #define NEW_OVERRIDE_SEGMENT | ( | address | ) |
| #define PENDING 0x0001 |
Start of command is pending.
| #define RF_MODE_BLE 0x01 |
| #define RF_MODE_IEEE_15_4 0x02 |
| #define RF_MODE_MULTIPLE 0x05 |
| #define RF_MODE_PROPRIETARY RF_MODE_PROPRIETARY_2_4 |
| #define RF_MODE_PROPRIETARY_2_4 0x03 |
| #define RF_MODE_PROPRIETARY_SUB_1 0x00 |
| #define SKIPPED 0x0003 |
Operation skipped due to condition in another command
| #define SW_ARRAY_OVERRIDE | ( | cmd, | |
| firstfield, | |||
| length | |||
| ) |
| #define SW_REG_2BYTE_OVERRIDE | ( | cmd, | |
| field, | |||
| val0, | |||
| val1 | |||
| ) |
Two 8-bit SW registers as defined in radio_par_def.txt; the one given by field and the next byte.
| #define SW_REG_BYTE_OVERRIDE | ( | cmd, | |
| field, | |||
| val | |||
| ) |
8-bit SW register as defined in radio_par_def.txt
| #define SW_REG_IND_OVERRIDE | ( | cmd, | |
| field, | |||
| offset, | |||
| val | |||
| ) |
SW register as defined in radio_par_def.txt with added index (for use with registers > 16 bits).
| #define SW_REG_OVERRIDE | ( | cmd, | |
| field, | |||
| val | |||
| ) | (3 | ((_POSITION_##cmd##_##field) << 4) | ((uint32_t)(val) << 16)) |
16-bit SW register as defined in radio_par_def.txt
| #define TRIG_ABSTIME 2 |
Trigs at an absolute time.
| #define TRIG_EXTERNAL 10 |
Trigs at an external event to the radio timer.
| #define TRIG_NEVER 1 |
Never trigs.
| #define TRIG_NOW 0 |
Triggers immediately.
| #define TRIG_PAST_BM 0x80 |
Bitmask for setting pastTrig bit in order to trig immediately if trigger happened in the past
| #define TRIG_REL_EVT1 8 |
Trigs at a time relative to the context defined "Event 1".
| #define TRIG_REL_EVT2 9 |
Trigs at a time relative to the context defined "Event 2".
| #define TRIG_REL_FIRSTSTART 6 |
Trigs at a time relative to the first command in the chain started.
| #define TRIG_REL_PREVEND 7 |
Trigs at a time relative to the previous command in the chain ended.
| #define TRIG_REL_PREVSTART 5 |
Trigs at a time relative to the previous command in the chain started.
| #define TRIG_REL_START 4 |
Trigs at a time relative to the command started.
| #define TRIG_REL_SUBMIT 3 |
Trigs at a time relative to the command was submitted.
| typedef uint32_t ratmr_t |
Type definition for RAT.