#include <stdbool.h>#include <stdint.h>#include "../inc/hw_types.h"#include "../inc/hw_memmap.h"#include "../inc/hw_ints.h"#include "../inc/hw_aux_tdc.h"#include "debug.h"Macros | |
| #define | AUX_TDC_BUSY 0x00000001 |
| #define | AUX_TDC_TIMEOUT 0x00000002 |
| #define | AUX_TDC_DONE 0x00000004 |
| #define | AUX_TDC_RUNSYNC 0x00000001 |
| #define | AUX_TDC_RUN 0x00000002 |
| #define | AUX_TDC_ABORT 0x00000003 |
| #define | AUXTDC_WAIT_START (AUX_TDC_STAT_STATE_WAIT_START) |
| #define | AUXTDC_WAIT_START_CNTEN (AUX_TDC_STAT_STATE_WAIT_START_STOP_CNT_EN) |
| #define | AUXTDC_IDLE (AUX_TDC_STAT_STATE_IDLE) |
| #define | AUXTDC_CLRCNT (AUX_TDC_STAT_STATE_CLR_CNT) |
| #define | AUXTDC_WAIT_STOP (AUX_TDC_STAT_STATE_WAIT_STOP) |
| #define | AUXTDC_WAIT_STOP_CNTDOWN (AUX_TDC_STAT_STATE_WAIT_STOP_CNTDWN) |
| #define | AUXTDC_GETRESULTS (AUX_TDC_STAT_STATE_GET_RESULT) |
| #define | AUXTDC_POR (AUX_TDC_STAT_STATE_POR) |
| #define | AUXTDC_WAIT_CLRCNT_DONE (AUX_TDC_STAT_STATE_WAIT_CLR_CNT_DONE) |
| #define | AUXTDC_START_FALL (AUX_TDC_STAT_STATE_START_FALL) |
| #define | AUXTDC_FORCE_STOP (AUX_TDC_STAT_STATE_FORCE_STOP) |
| #define | AUXTDC_STOPPOL_RIS (AUX_TDC_TRIGSRC_STOP_POL_HIGH) |
| #define | AUXTDC_STOPPOL_FALL (AUX_TDC_TRIGSRC_STOP_POL_LOW) |
| #define | AUXTDC_STOP_AON_RTC_CH2 (AUX_TDC_TRIGSRC_STOP_SRC_AON_RTC_CH2) |
| #define | AUXTDC_STOP_AUX_COMPA (AUX_TDC_TRIGSRC_STOP_SRC_AUX_COMPA) |
| #define | AUXTDC_STOP_AUX_COMPB (AUX_TDC_TRIGSRC_STOP_SRC_AUX_COMPB) |
| #define | AUXTDC_STOP_ISRC_RESET (AUX_TDC_TRIGSRC_STOP_SRC_ISRC_RESET) |
| #define | AUXTDC_STOP_TIMER0_EV (AUX_TDC_TRIGSRC_STOP_SRC_TIMER0_EV) |
| #define | AUXTDC_STOP_TIMER1_EV (AUX_TDC_TRIGSRC_STOP_SRC_TIMER1_EV) |
| #define | AUXTDC_STOP_SMPH_AUTOTAKE_DONE (AUX_TDC_TRIGSRC_STOP_SRC_SMPH_AUTOTAKE_DONE) |
| #define | AUXTDC_STOP_ADC_DONE (AUX_TDC_TRIGSRC_STOP_SRC_ADC_DONE) |
| #define | AUXTDC_STOP_ADC_FIFO_ALMOST_FULL (AUX_TDC_TRIGSRC_STOP_SRC_ADC_FIFO_ALMOST_FULL) |
| #define | AUXTDC_STOP_OBSMUX0 (AUX_TDC_TRIGSRC_STOP_SRC_OBSMUX0) |
| #define | AUXTDC_STOP_OBSMUX1 (AUX_TDC_TRIGSRC_STOP_SRC_OBSMUX1) |
| #define | AUXTDC_STOP_AON_SW (AUX_TDC_TRIGSRC_STOP_SRC_AON_SW) |
| #define | AUXTDC_STOP_AON_PROG_WU (AUX_TDC_TRIGSRC_STOP_SRC_AON_PROG_WU) |
| #define | AUXTDC_STOP_AUXIO0 (AUX_TDC_TRIGSRC_STOP_SRC_AUXIO0) |
| #define | AUXTDC_STOP_AUXIO1 (AUX_TDC_TRIGSRC_STOP_SRC_AUXIO1) |
| #define | AUXTDC_STOP_AUXIO2 (AUX_TDC_TRIGSRC_STOP_SRC_AUXIO2) |
| #define | AUXTDC_STOP_AUXIO3 (AUX_TDC_TRIGSRC_STOP_SRC_AUXIO3) |
| #define | AUXTDC_STOP_AUXIO4 (AUX_TDC_TRIGSRC_STOP_SRC_AUXIO4) |
| #define | AUXTDC_STOP_AUXIO5 (AUX_TDC_TRIGSRC_STOP_SRC_AUXIO5) |
| #define | AUXTDC_STOP_AUXIO6 (AUX_TDC_TRIGSRC_STOP_SRC_AUXIO6) |
| #define | AUXTDC_STOP_AUXIO7 (AUX_TDC_TRIGSRC_STOP_SRC_AUXIO7) |
| #define | AUXTDC_STOP_AUXIO8 (AUX_TDC_TRIGSRC_STOP_SRC_AUXIO8) |
| #define | AUXTDC_STOP_AUXIO9 (AUX_TDC_TRIGSRC_STOP_SRC_AUXIO9) |
| #define | AUXTDC_STOP_AUXIO10 (AUX_TDC_TRIGSRC_STOP_SRC_AUXIO10) |
| #define | AUXTDC_STOP_AUXIO11 (AUX_TDC_TRIGSRC_STOP_SRC_AUXIO11) |
| #define | AUXTDC_STOP_AUXIO12 (AUX_TDC_TRIGSRC_STOP_SRC_AUXIO12) |
| #define | AUXTDC_STOP_AUXIO13 (AUX_TDC_TRIGSRC_STOP_SRC_AUXIO13) |
| #define | AUXTDC_STOP_AUXIO14 (AUX_TDC_TRIGSRC_STOP_SRC_AUXIO14) |
| #define | AUXTDC_STOP_AUXIO15 (AUX_TDC_TRIGSRC_STOP_SRC_AUXIO15) |
| #define | AUXTDC_STOP_ACLK_REF (AUX_TDC_TRIGSRC_STOP_SRC_ACLK_REF) |
| #define | AUXTDC_STOP_MCU_EV (AUX_TDC_TRIGSRC_STOP_SRC_MCU_EV) |
| #define | AUXTDC_STOP_TDC_PRE (AUX_TDC_TRIGSRC_STOP_SRC_TDC_PRE) |
| #define | AUXTDC_STARTPOL_RIS (AUX_TDC_TRIGSRC_START_POL_HIGH) |
| #define | AUXTDC_STARTPOL_FALL (AUX_TDC_TRIGSRC_START_POL_LOW) |
| #define | AUXTDC_START_AON_RTC_CH2 (AUX_TDC_TRIGSRC_START_SRC_AON_RTC_CH2) |
| #define | AUXTDC_START_AUX_COMPA (AUX_TDC_TRIGSRC_START_SRC_AUX_COMPA) |
| #define | AUXTDC_START_AUX_COMPB (AUX_TDC_TRIGSRC_START_SRC_AUX_COMPB) |
| #define | AUXTDC_START_ISRC_RESET (AUX_TDC_TRIGSRC_START_SRC_ISRC_RESET) |
| #define | AUXTDC_START_TIMER0_EV (AUX_TDC_TRIGSRC_START_SRC_TIMER0_EV) |
| #define | AUXTDC_START_TIMER1_EV (AUX_TDC_TRIGSRC_START_SRC_TIMER1_EV) |
| #define | AUXTDC_START_SMPH_AUTOTAKE_DONE (AUX_TDC_TRIGSRC_START_SRC_SMPH_AUTOTAKE_DONE) |
| #define | AUXTDC_START_ADC_DONE (AUX_TDC_TRIGSRC_START_SRC_ADC_DONE) |
| #define | AUXTDC_START_ADC_FIFO_ALMOST_FULL (AUX_TDC_TRIGSRC_START_SRC_ADC_FIFO_ALMOST_FULL) |
| #define | AUXTDC_START_OBSMUX0 (AUX_TDC_TRIGSRC_START_SRC_OBSMUX0) |
| #define | AUXTDC_START_OBSMUX1 (AUX_TDC_TRIGSRC_START_SRC_OBSMUX1) |
| #define | AUXTDC_START_AON_SW (AUX_TDC_TRIGSRC_START_SRC_AON_SW) |
| #define | AUXTDC_START_AON_PROG_WU (AUX_TDC_TRIGSRC_START_SRC_AON_PROG_WU) |
| #define | AUXTDC_START_AUXIO0 (AUX_TDC_TRIGSRC_START_SRC_AUXIO0) |
| #define | AUXTDC_START_AUXIO1 (AUX_TDC_TRIGSRC_START_SRC_AUXIO1) |
| #define | AUXTDC_START_AUXIO2 (AUX_TDC_TRIGSRC_START_SRC_AUXIO2) |
| #define | AUXTDC_START_AUXIO3 (AUX_TDC_TRIGSRC_START_SRC_AUXIO3) |
| #define | AUXTDC_START_AUXIO4 (AUX_TDC_TRIGSRC_START_SRC_AUXIO4) |
| #define | AUXTDC_START_AUXIO5 (AUX_TDC_TRIGSRC_START_SRC_AUXIO5) |
| #define | AUXTDC_START_AUXIO6 (AUX_TDC_TRIGSRC_START_SRC_AUXIO6) |
| #define | AUXTDC_START_AUXIO7 (AUX_TDC_TRIGSRC_START_SRC_AUXIO7) |
| #define | AUXTDC_START_AUXIO8 (AUX_TDC_TRIGSRC_START_SRC_AUXIO8) |
| #define | AUXTDC_START_AUXIO9 (AUX_TDC_TRIGSRC_START_SRC_AUXIO9) |
| #define | AUXTDC_START_AUXIO10 (AUX_TDC_TRIGSRC_START_SRC_AUXIO10) |
| #define | AUXTDC_START_AUXIO11 (AUX_TDC_TRIGSRC_START_SRC_AUXIO11) |
| #define | AUXTDC_START_AUXIO12 (AUX_TDC_TRIGSRC_START_SRC_AUXIO12) |
| #define | AUXTDC_START_AUXIO13 (AUX_TDC_TRIGSRC_START_SRC_AUXIO13) |
| #define | AUXTDC_START_AUXIO14 (AUX_TDC_TRIGSRC_START_SRC_AUXIO14) |
| #define | AUXTDC_START_AUXIO15 (AUX_TDC_TRIGSRC_START_SRC_AUXIO15) |
| #define | AUXTDC_START_ACLK_REF (AUX_TDC_TRIGSRC_START_SRC_ACLK_REF) |
| #define | AUXTDC_START_MCU_EV (AUX_TDC_TRIGSRC_START_SRC_MCU_EV) |
| #define | AUXTDC_START_TDC_PRE (AUX_TDC_TRIGSRC_START_SRC_TDC_PRE) |
| #define | AUXTDC_SAT_4096 (AUX_TDC_SATCFG_LIMIT_R12) |
| #define | AUXTDC_SAT_8192 (AUX_TDC_SATCFG_LIMIT_R13) |
| #define | AUXTDC_SAT_16384 (AUX_TDC_SATCFG_LIMIT_R14) |
| #define | AUXTDC_SAT_32768 (AUX_TDC_SATCFG_LIMIT_R15) |
| #define | AUXTDC_SAT_65536 (AUX_TDC_SATCFG_LIMIT_R16) |
| #define | AUXTDC_SAT_131072 (AUX_TDC_SATCFG_LIMIT_R17) |
| #define | AUXTDC_SAT_262144 (AUX_TDC_SATCFG_LIMIT_R18) |
| #define | AUXTDC_SAT_524288 (AUX_TDC_SATCFG_LIMIT_R19) |
| #define | AUXTDC_SAT_1048576 (AUX_TDC_SATCFG_LIMIT_R20) |
| #define | AUXTDC_SAT_2097152 (AUX_TDC_SATCFG_LIMIT_R21) |
| #define | AUXTDC_SAT_4194304 (AUX_TDC_SATCFG_LIMIT_R22) |
| #define | AUXTDC_SAT_8388608 (AUX_TDC_SATCFG_LIMIT_R23) |
| #define | AUXTDC_SAT_16777216 (AUX_TDC_SATCFG_LIMIT_R24) |
| #define | AUXTDC_NUM_SAT_VALS 16 |
Functions | |
| static uint32_t | AUXTDCStatusGet (uint32_t ui32Base) |
| Get the status of the AUX TDC internal state machine. More... | |
| void | AUXTDCConfigSet (uint32_t ui32Base, uint32_t ui32StartCondition, uint32_t ui32StopCondition) |
| Configure the operation of the AUX TDC. More... | |
| static bool | AUXTDCIdle (uint32_t ui32Base) |
| Check if the AUX TDC is in idle mode. More... | |
| static void | AUXTDCEnable (uint32_t ui32Base, uint32_t ui32RunMode) |
| Enable the AUX TDC for a measurement. More... | |
| static void | AUXTDCIdleForce (uint32_t ui32Base) |
| Force the AUX TDC back to Idle mode. More... | |
| uint32_t | AUXTDCMeasurementDone (uint32_t ui32Base) |
| Check if the AUX TDC is done measuring. More... | |
| static uint32_t | AUXTDCMeasurementGet (uint32_t ui32Base) |
| Get the value of the latest measurement. More... | |
| static void | AUXTDCLimitSet (uint32_t ui32Base, uint32_t ui32Limit) |
| Set the saturation limit of the measurement. More... | |
| static uint32_t | AUXTDCLimitGet (uint32_t ui32Base) |
| Get the saturation limit of the measurement. More... | |
| static bool | AUXTDCCounterEnable (uint32_t ui32Base) |
| Enables the counter if possible. More... | |
| static bool | AUXTDCCounterDisable (uint32_t ui32Base) |
| Disables the counter if possible. More... | |
| static bool | AUXTDCCounterSet (uint32_t ui32Base, uint32_t ui32Events) |
| Set the reset number of counter compare/stop event to ignore before taking a measurement. More... | |
| static uint32_t | AUXTDCCounterGet (uint32_t ui32Base) |
| Get the current number of counter compare/stop event to ignore before taking a measurement. More... | |