TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
l2capPacket_t Struct Reference

L2CAP packet structure. More...

Data Fields

uint16 CID
 local channel id
 
uint16 len
 length of information payload
 
uint8 * pPayload
 

Detailed Description

L2CAP packet structure.

Field Documentation

§ pPayload

uint8* pPayload

pointer to information payload. This contains the payload received from the upper layer protocol (outgoing packet), or delivered to the upper layer protocol (incoming packet).


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated