TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
l2capConnectReq_t Struct Reference

Connection Request format. More...

Data Fields

uint16 initCredits
 Indicates number of LE-frames that peer device can send.
 
uint16 mps
 Specifies maximum payload size that can be received on this channel.
 
uint16 mtu
 Specifies maximum SDU size that can be received on this channel.
 
uint16 psm
 LE PSM.
 
uint16 srcCID
 Represents CID on device sending request and receiving response.
 

Detailed Description

Connection Request format.


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated