TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
gattCharFormat_t Struct Reference

GATT Structure for Characteristic Presentation Format Value. More...

Data Fields

uint16 desc
 Description of this attribute as defined in a higher layer profile.
 
int8 exponent
 A sign integer which represents the exponent of an integer.
 
uint8 format
 Format of the value of this characteristic.
 
uint8 nameSpace
 Name space of the description.
 
uint16 unit
 Unit of this attribute as defined in the data dictionary.
 

Detailed Description

GATT Structure for Characteristic Presentation Format Value.


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated