TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields

Multi GAPRole Callback structure. More...

Data Fields

paramUpdateAppDecision_t pfnParamUpdateAppDecision
 When the app should decide on a param update request.
 
passThroughToApp_t pfnPassThrough
 When the event should be processed by the app instead of the GAP Role.
 
gapRolesStateNotify_t pfnStateChange
 Whenever the device changes state.
 

Detailed Description

Multi GAPRole Callback structure.

Peripheral GAPRole Callback structure.

This must be setup by the application and passed to the GAPRole when GAPRole_StartDevice is called.


The documentation for this struct was generated from the following files:
Copyright 2017, Texas Instruments Incorporated