![]() |
![]() |
|
TI BLE-Stack for Bluetooth 4.2 API Documentation
3.01.00.07
|
Peripheral layer interface.
Go to the source code of this file.
Data Structures | |
| struct | gapRolesCBs_t |
| Multi GAPRole Callback structure. More... | |
Macros | |
| #define | GAPROLE_ADV_CHANNEL_MAP 0x30C |
| Which channels to advertise on (Read/Write) More... | |
| #define | GAPROLE_ADV_DIRECT_ADDR 0x30B |
| Direct Advertisement Address (Read/Write) More... | |
| #define | GAPROLE_ADV_DIRECT_TYPE 0x30A |
| Direct Advertisement Type (Read/Write) More... | |
| #define | GAPROLE_ADV_EVENT_TYPE 0x309 |
| Advertisement Types (Read/Write) More... | |
| #define | GAPROLE_ADV_FILTER_POLICY 0x30D |
| Policy for filtering advertisements (Read/Write) More... | |
| #define | GAPROLE_ADV_NONCONN_ENABLED 0x31B |
| Enable / Disable non-connectable advertising (Read/Write) More... | |
| #define | GAPROLE_ADVERT_DATA 0x307 |
| Advertisement data (Read/Write) More... | |
| #define | GAPROLE_ADVERT_ENABLED 0x305 |
| Enable/Disable Connectable Advertising (Read/Write) More... | |
| #define | GAPROLE_ADVERT_OFF_TIME 0x306 |
| How long to remain off (in sec) after advertising stops before starting again (Read/Write) More... | |
| #define | GAPROLE_BD_ADDR 0x304 |
| Device Address read from the controller (Read-only) More... | |
| #define | GAPROLE_BD_ADDR_TYPE 0x31C |
| Address type of connected device (Read-only) More... | |
| #define | GAPROLE_CONN_BD_ADDR 0x315 |
| Address of connected device (Read-only) More... | |
| #define | GAPROLE_CONN_INTERVAL 0x316 |
| Connection Interval (n x 1.25 ms) of current connection (Read-only) More... | |
| #define | GAPROLE_CONN_LATENCY 0x317 |
| Slave Latency of current connection (Read-only) More... | |
| #define | GAPROLE_CONN_TERM_REASON 0x31D |
| Reason of the last connection terminated event. More... | |
| #define | GAPROLE_CONN_TIMEOUT 0x318 |
| Connection Interval (n x 10 ms) of current connection (Read-only) More... | |
| #define | GAPROLE_CONNHANDLE 0x30E |
| Connection Handle of current connected device (Read-only) More... | |
| #define | GAPROLE_IRK 0x301 |
| Identity Resolving Key (Read/Write) Size is uint8_t[KEYLEN]. More... | |
| #define | GAPROLE_LINK_PARAM_UPDATE_INITIATE_APP_PARAMS 2 |
| Initiate parameter update request, respond with local requested parameters only. | |
| #define | GAPROLE_LINK_PARAM_UPDATE_INITIATE_BOTH_PARAMS 1 |
| Initiate parameter update request, respond with best combination of local and remote parameters. | |
| #define | GAPROLE_LINK_PARAM_UPDATE_NUM_OPTIONS 6 |
| Used for parameter checking. | |
| #define | GAPROLE_LINK_PARAM_UPDATE_REJECT_REQUEST 5 |
| Reject all parameter update requests. | |
| #define | GAPROLE_LINK_PARAM_UPDATE_WAIT_APP_PARAMS 3 |
| Wait for parameter update request, respond with local requested parameters only. | |
| #define | GAPROLE_LINK_PARAM_UPDATE_WAIT_BOTH_PARAMS 4 |
| Wait for parameter update request, respond with best combination of local and remote parameters. | |
| #define | GAPROLE_LINK_PARAM_UPDATE_WAIT_REMOTE_PARAMS 0 |
| Wait for parameter update request, respond with remote's requested parameters. | |
| #define | GAPROLE_MAX_CONN_INTERVAL 0x312 |
| Maximum connection interval (n * 1.25 ms) to use when performing param update (Read/Write) More... | |
| #define | GAPROLE_MIN_CONN_INTERVAL 0x311 |
| Minimum connection interval (n * 1.25 ms) to use when performing param update (Read/Write) More... | |
| #define | GAPROLE_NO_ACTION 0 |
| Take no action upon unsuccessful parameter updates. | |
| #define | GAPROLE_PARAM_UPDATE_ENABLE 0x310 |
| Whether to request a connection parameter update upon connection (Read/Write) More... | |
| #define | GAPROLE_PARAM_UPDATE_REQ 0x319 |
| Used to send a Parameter Update Request (Write-only) More... | |
| #define | GAPROLE_PROFILEROLE 0x300 |
| This parameter will return GAP Role type (Read-only) More... | |
| #define | GAPROLE_RESEND_PARAM_UPDATE 1 |
| Continue to resend request until successful update. | |
| #define | GAPROLE_SCAN_RSP_DATA 0x308 |
| Scan Response Data (Read/Write) More... | |
| #define | GAPROLE_SIGNCOUNTER 0x303 |
| Sign Counter (Read/Write) More... | |
| #define | GAPROLE_SLAVE_LATENCY 0x313 |
| Slave latency to use when performing param update (Read/Write) More... | |
| #define | GAPROLE_SRK 0x302 |
| Signature Resolving Key (Read/Write) More... | |
| #define | GAPROLE_STATE 0x31A |
| Current Peripheral GAPRole state (Read-only) More... | |
| #define | GAPROLE_TERMINATE_LINK 2 |
| Terminate link upon unsuccessful parameter updates. | |
| #define | GAPROLE_TIMEOUT_MULTIPLIER 0x314 |
| Supervision timeout (n x 10 ms) to use when performing param update (Read/Write) More... | |
Typedefs | |
| typedef void(* | gapRolesParamUpdateCB_t) (uint16_t connInterval, uint16_t connSlaveLatency, uint16_t connTimeout) |
| Callback when the connection parameters are updated. More... | |
| typedef void(* | gapRolesStateNotify_t) (gaprole_States_t newState) |
| State Change Callback Type. More... | |
Enumerations | |
| enum | gaprole_States_t { GAPROLE_INIT = 0, GAPROLE_STARTED, GAPROLE_ADVERTISING, GAPROLE_ADVERTISING_NONCONN, GAPROLE_WAITING, GAPROLE_WAITING_AFTER_TIMEOUT, GAPROLE_CONNECTED, GAPROLE_CONNECTED_ADV, GAPROLE_ERROR } |
| GAP Peripheral Role States. More... | |
Functions | |
| bStatus_t | GAPRole_GetParameter (uint16_t param, void *pValue) |
| Get a GAP Role parameter. More... | |
| void | GAPRole_RegisterAppCBs (gapRolesParamUpdateCB_t *pParamUpdateCB) |
| Register application's callbacks. More... | |
| bStatus_t | GAPRole_SendUpdateParam (uint16_t minConnInterval, uint16_t maxConnInterval, uint16_t latency, uint16_t connTimeout, uint8_t handleFailure) |
| Update the parameters of an existing connection. More... | |
| bStatus_t | GAPRole_SetParameter (uint16_t param, uint8_t len, void *pValue) |
| Set a GAP Role parameter. More... | |
| bStatus_t | GAPRole_StartDevice (gapRolesCBs_t *pAppCallbacks) |
| Initialize the GAP layer. More... | |
| bStatus_t | GAPRole_TerminateConnection (void) |
| Terminates the existing connection. More... | |