![]() |
![]() |
TI BLE-Stack for Bluetooth 4.2 API Documentation
3.01.00.07
|
This module implements the Link Database Module. More...
Modules | |
LinkDB Callbacks | |
LinkDB Constants | |
LinkDB Data Structures | |
Files | |
file | linkdb.h |
LinkDB layer interface. | |
Macros | |
#define | linkDB_Authenticated(connectionHandle) linkDB_State( (connectionHandle), LINK_AUTHENTICATED ) |
Check to see if the physical link is authenticated. More... | |
#define | linkDB_Bonded(connectionHandle) linkDB_State( (connectionHandle), LINK_BOUND ) |
Check to see if the physical link is bonded. More... | |
#define | linkDB_Encrypted(connectionHandle) linkDB_State( (connectionHandle), LINK_ENCRYPTED ) |
Check to see if the physical link is encrypted. More... | |
#define | linkDB_Up(connectionHandle) linkDB_State( (connectionHandle), LINK_CONNECTED ) |
Check to see if a physical link is up (connected). More... | |
Functions | |
uint8 | linkDB_Add (uint8 taskID, uint16 connectionHandle, uint8 stateFlags, uint8 addrType, uint8 *pAddr, uint8 *pAddrPriv, uint8 connRole, uint16 connInterval, uint16 MTU) |
Adds a record to the link database. More... | |
uint8 | linkDB_Authen (uint16 connectionHandle, uint8 keySize, uint8 mitmRequired) |
Check to see if the physical link is encrypted and authenticated. More... | |
linkDBItem_t * | linkDB_Find (uint16 connectionHandle) |
Find the link. More... | |
linkDBItem_t * | linkDB_FindFirst (uint8 taskID) |
Find the first link that matches the taskID. More... | |
uint8 | linkDB_GetInfo (uint16 connectionHandle, linkDBInfo_t *pInfo) |
Get information about a link. More... | |
NODOC void | linkDB_Init (void) |
Initialize the Link Database. | |
uint16 | linkDB_MTU (uint16 connectionHandle) |
This function is used to get the MTU size of a link. More... | |
uint8 | linkDB_NumActive (void) |
Return the number of active connections. More... | |
uint8 | linkDB_NumConns (void) |
return the maximum number of connections supported. More... | |
void | linkDB_PerformFunc (pfnPerformFuncCB_t cb) |
Perform a function of each connection in the link database. More... | |
uint8 | linkDB_Register (pfnLinkDBCB_t pFunc) |
Register with linkDB. More... | |
uint8 | linkDB_Remove (uint16 connectionHandle) |
Remove a record from the link database. More... | |
uint8 | linkDB_Role (uint16 connectionHandle) |
Get the role of a physical link. More... | |
void | linkDB_SecurityModeSCOnly (uint8 state) |
Set a device into Secure Connection Only Mode. More... | |
uint8 | linkDB_State (uint16 connectionHandle, uint8 state) |
Check to see if a physical link is in a specific state. More... | |
uint8 | linkDB_Update (uint16 connectionHandle, uint8 newState, uint8 add) |
Update the stateFlags of a link record. More... | |
uint8 | linkDB_UpdateMTU (uint16 connectionHandle, uint16 newMtu) |
update the MTU size of a link or record. More... | |
This module implements the Link Database Module.
#define linkDB_Authenticated | ( | connectionHandle | ) | linkDB_State( (connectionHandle), LINK_AUTHENTICATED ) |
Check to see if the physical link is authenticated.
connectionHandle | - controller link connection handle. |
#define linkDB_Bonded | ( | connectionHandle | ) | linkDB_State( (connectionHandle), LINK_BOUND ) |
Check to see if the physical link is bonded.
connectionHandle | - controller link connection handle. |
#define linkDB_Encrypted | ( | connectionHandle | ) | linkDB_State( (connectionHandle), LINK_ENCRYPTED ) |
Check to see if the physical link is encrypted.
connectionHandle | - controller link connection handle. |
#define linkDB_Up | ( | connectionHandle | ) | linkDB_State( (connectionHandle), LINK_CONNECTED ) |
Check to see if a physical link is up (connected).
connectionHandle | - controller link connection handle. |
uint8 linkDB_Add | ( | uint8 | taskID, |
uint16 | connectionHandle, | ||
uint8 | stateFlags, | ||
uint8 | addrType, | ||
uint8 * | pAddr, | ||
uint8 * | pAddrPriv, | ||
uint8 | connRole, | ||
uint16 | connInterval, | ||
uint16 | MTU | ||
) |
Adds a record to the link database.
taskID | - Application task ID |
connectionHandle | - new record connection handle |
stateFlags | - LinkDB Connection State Flags |
addrType | - Device Address Type |
pAddr | - new address |
pAddrPriv | - private address (only if addrType is 0x02 or 0x03) |
connRole | - GAP Profile Roles |
connInterval | - connection's communications interval (n * 1.23 ms) |
MTU | - connection's MTU size |
uint8 linkDB_Authen | ( | uint16 | connectionHandle, |
uint8 | keySize, | ||
uint8 | mitmRequired | ||
) |
Check to see if the physical link is encrypted and authenticated.
connectionHandle | - controller link connection handle. |
keySize | - size of encryption keys. |
mitmRequired | - TRUE (yes) or FALSE (no). |
linkDBItem_t* linkDB_Find | ( | uint16 | connectionHandle | ) |
Find the link.
Uses the connection handle to search the link database.
connectionHandle | - controller link connection handle. |
linkDBItem_t* linkDB_FindFirst | ( | uint8 | taskID | ) |
Find the first link that matches the taskID.
taskID | - taskID of app |
uint8 linkDB_GetInfo | ( | uint16 | connectionHandle, |
linkDBInfo_t * | pInfo | ||
) |
Get information about a link.
Copies relevant link info into pInfo. Uses the connection handle to search the link database.
connectionHandle | - controller link connection handle. |
pInfo | - address of link info item to copy information |
uint16 linkDB_MTU | ( | uint16 | connectionHandle | ) |
This function is used to get the MTU size of a link.
connectionHandle | - controller link connection handle. |
uint8 linkDB_NumActive | ( | void | ) |
Return the number of active connections.
uint8 linkDB_NumConns | ( | void | ) |
return the maximum number of connections supported.
void linkDB_PerformFunc | ( | pfnPerformFuncCB_t | cb | ) |
Perform a function of each connection in the link database.
cb | - connection callback function. |
uint8 linkDB_Register | ( | pfnLinkDBCB_t | pFunc | ) |
Register with linkDB.
Register with this function to receive a callback when status changes on a connection. If the stateflag == 0, then the connection has been disconnected.
pFunc | - function pointer to callback function |
uint8 linkDB_Remove | ( | uint16 | connectionHandle | ) |
Remove a record from the link database.
connectionHandle | - new record connection handle |
uint8 linkDB_Role | ( | uint16 | connectionHandle | ) |
Get the role of a physical link.
connectionHandle | - controller link connection handle. |
void linkDB_SecurityModeSCOnly | ( | uint8 | state | ) |
Set a device into Secure Connection Only Mode.
state | - TRUE for Secure Connections Only Mode. FALSE to disable Secure Connections Only Mode. |
uint8 linkDB_State | ( | uint16 | connectionHandle, |
uint8 | state | ||
) |
Check to see if a physical link is in a specific state.
connectionHandle | - controller link connection handle. |
state | - LinkDB Connection State Flags state to look for. |
uint8 linkDB_Update | ( | uint16 | connectionHandle, |
uint8 | newState, | ||
uint8 | add | ||
) |
Update the stateFlags of a link record.
connectionHandle | - maximum number of connections. |
newState | - LinkDB Connection State Flags. This value is OR'd in to this field. |
add | - TRUE to set state into flags, FALSE to remove. |
uint8 linkDB_UpdateMTU | ( | uint16 | connectionHandle, |
uint16 | newMtu | ||
) |
update the MTU size of a link or record.
connectionHandle | - controller link connection handle. |
newMtu | - new MTU size. |