|
| uint32_t | CRYPTOAesLoadKey (uint32_t *pui32AesKey, uint32_t ui32KeyLocation) |
| | Write the key into the Key Ram. More...
|
| |
| uint32_t | CRYPTOAesCbc (uint32_t *pui32MsgIn, uint32_t *pui32MsgOut, uint32_t ui32MsgLength, uint32_t *pui32Nonce, uint32_t ui32KeyLocation, bool bEncrypt, bool bIntEnable) |
| | Start an AES-CBC operation (encryption or decryption). More...
|
| |
| uint32_t | CRYPTOAesCbcStatus (void) |
| | Check the result of an AES CBC operation. More...
|
| |
| uint32_t | CRYPTOAesEcb (uint32_t *pui32MsgIn, uint32_t *pui32MsgOut, uint32_t ui32KeyLocation, bool bEncrypt, bool bIntEnable) |
| | Start an AES-ECB operation (encryption or decryption). More...
|
| |
| uint32_t | CRYPTOAesEcbStatus (void) |
| | Check the result of an AES ECB operation. More...
|
| |
| uint32_t | CRYPTOCcmAuthEncrypt (bool bEncrypt, uint32_t ui32AuthLength, uint32_t *pui32Nonce, uint32_t *pui32PlainText, uint32_t ui32PlainTextLength, uint32_t *pui32Header, uint32_t ui32HeaderLength, uint32_t ui32KeyLocation, uint32_t ui32FieldLength, bool bIntEnable) |
| | Start CCM operation. More...
|
| |
| uint32_t | CRYPTOCcmAuthEncryptStatus (void) |
| | Check the result of an AES CCM operation. More...
|
| |
| uint32_t | CRYPTOCcmAuthEncryptResultGet (uint32_t ui32TagLength, uint32_t *pui32CcmTag) |
| | Get the result of an AES-CCM operation. More...
|
| |
| uint32_t | CRYPTOCcmInvAuthDecrypt (bool bDecrypt, uint32_t ui32AuthLength, uint32_t *pui32Nonce, uint32_t *pui32CipherText, uint32_t ui32CipherTextLength, uint32_t *pui32Header, uint32_t ui32HeaderLength, uint32_t ui32KeyLocation, uint32_t ui32FieldLength, bool bIntEnable) |
| | Start a CCM Decryption and Inverse Authentication operation. More...
|
| |
| uint32_t | CRYPTOCcmInvAuthDecryptStatus (void) |
| | Checks CCM decrypt and Inverse Authentication result. More...
|
| |
| uint32_t | CRYPTOCcmInvAuthDecryptResultGet (uint32_t ui32AuthLength, uint32_t *pui32CipherText, uint32_t ui32CipherTextLength, uint32_t *pui32CcmTag) |
| | Get the result of the CCM operation. More...
|
| |
| void | CRYPTODmaEnable (uint32_t ui32Channels) |
| | Enable Crypto DMA operation. More...
|
| |
| void | CRYPTODmaDisable (uint32_t ui32Channels) |
| | Disable Crypto DMA operation. More...
|
| |