Peripheral Sharing¶
Description¶
Sharing of peripheral hardware modules with the System CPU
This resource provides means to safely use any of the following hardware peripheral modules when these are shared between System CPU and Sensor Controller:
- ADC (input node shared with COMPB)
- COMPA and ISRC (cannot be used independently)
- COMPB (input node shared with ADC)
- TDC
A shared hardware peripheral module shall be acquired before use and released after use, by calling:
fwAcquirePeripheral(peripheral)before the first use of the peripheral’s procedures.fwReleasePeripheral(peripheral)after the last use of the peripheral’s procedures.
If task code or a System CPU execution thread require multiple peripheral hardware modules, these must be acquired in alphabetical order (that is as listed above) to prevent deadlock.
Configuration of shared peripherals must be done with caution, and should only be done in the Initialization Code if the System CPU restores the previous configuration before releasing the peripheral hardware module.
Examples¶
Sharing the ADC¶
// Acquire the ADC
fwAcquirePeripheral(PERIPHERAL_ADC);
// Select ADC input
adcSelectGpioInput(AUXIO_A_SENSOR_OUTPUT);
// Enable the ADC (fixed reference, 2.7 us sample time, manual trigger)
adcEnableSync(ADC_REF_FIXED, ADC_SAMPLE_TIME_2P7_US, ADC_TRIGGER_MANUAL);
// Sample the sensor and store the ADC value
adcGenManualTrigger();
adcReadFifo(output.adcValue);
// Disable the ADC
adcDisable();
// Release the ADC
fwReleasePeripheral(PERIPHERAL_ADC);
Procedures Overview¶
| Name | Brief description |
fwAcquirePeripheral() |
Waits for and acquires the specified shared AUX domain peripheral. More … |
fwReleasePeripheral() |
Releases the specified shared AUX domain peripheral. More … |
Constants¶
| Name | Description |
PERIPHERAL_ADC |
Semaphore used to acquire ADC (analog to digital converter) |
PERIPHERAL_COMPA_ISRC |
Semaphore used to acquire COMPA (continuous time comparator) and ISRC (current source) |
PERIPHERAL_COMPB |
Semaphore used to acquire COMPB (low-power clocked comparator) |
PERIPHERAL_TDC |
Semaphore used to acquire TDC (time to digital converter) |
Global Variables¶
None.