![]() |
![]() |
|
TI BLE-Stack for Bluetooth 4.2 API Documentation
3.01.00.07
|
Parameter Structure to add new Characteristic Description Response SNP_ADD_CHAR_DESC_DECL_RSP. More...
Data Fields | |
| uint16_t | handles [6] |
| Maximum handles returned is 6. One for each possible attribute added. Header will determine the number of actual handles returned. | |
| uint8_t | header |
| uint8_t | status |
| 1 Byte Command Status list of status generated by the SNP. | |
Parameter Structure to add new Characteristic Description Response SNP_ADD_CHAR_DESC_DECL_RSP.
snpAddCharDescDeclRsp_t::handles will be populated with attributes added based on the header, starting from LSB to MSB.
This packet structure is not used to create a NPI frame
| uint8_t header |
1 Byte Header bit field of request.
Defines which attributes are added.
SNP GATT Descriptors Header