TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Modules Pages
gattservapp.h
Go to the documentation of this file.
1 /******************************************************************************
2 
3  Group: WCS, BTS
4  $Target Device: DEVICES $
5 
6  ******************************************************************************
7  $License: BSD3 2009 $
8  ******************************************************************************
9  $Release Name: PACKAGE NAME $
10  $Release Date: PACKAGE RELEASE DATE $
11  *****************************************************************************/
12 
21 #ifndef GATTSERVAPP_H
22 #define GATTSERVAPP_H
23 
24 #ifdef __cplusplus
25 extern "C"
26 {
27 #endif
28 
29 /*********************************************************************
30  * INCLUDES
31  */
32 #include "bcomdef.h"
33 #include "osal.h"
34 
35 /*********************************************************************
36  * CONSTANTS
37  */
38 
47 #define GATT_CLIENT_CHAR_CFG_UPDATED_EVENT 0x00
48 
49 
56 #define GATT_PROP_BCAST 0x01
57 #define GATT_PROP_READ 0x02
58 #define GATT_PROP_WRITE_NO_RSP 0x04
59 #define GATT_PROP_WRITE 0x08
60 #define GATT_PROP_NOTIFY 0x10
61 #define GATT_PROP_INDICATE 0x20
62 #define GATT_PROP_AUTHEN 0x40
63 #define GATT_PROP_EXTENDED 0x80
64 
65 
71 #define GATT_EXT_PROP_RELIABLE_WRITE 0x0001
72 #define GATT_EXT_PROP_WRITABLE_AUX 0x0002
73 
74 
80 #define GATT_CLIENT_CFG_NOTIFY 0x0001
81 #define GATT_CLIENT_CFG_INDICATE 0x0002
82 
83 
89 #define GATT_SERV_CFG_BCAST 0x0001
90 
91 
93 #define GATT_CFG_NO_OPERATION 0x0000
94 
95 
99 #define GATT_FORMAT_BOOL 0x01
100 #define GATT_FORMAT_2BIT 0x02
101 #define GATT_FORMAT_NIBBLE 0x03
102 #define GATT_FORMAT_UINT8 0x04
103 #define GATT_FORMAT_UINT12 0x05
104 #define GATT_FORMAT_UINT16 0x06
105 #define GATT_FORMAT_UINT24 0x07
106 #define GATT_FORMAT_UINT32 0x08
107 #define GATT_FORMAT_UINT48 0x09
108 #define GATT_FORMAT_UINT64 0x0a
109 #define GATT_FORMAT_UINT128 0x0b
110 #define GATT_FORMAT_SINT8 0x0c
111 #define GATT_FORMAT_SINT12 0x0d
112 #define GATT_FORMAT_SINT16 0x0e
113 #define GATT_FORMAT_SINT24 0x0f
114 #define GATT_FORMAT_SINT32 0x10
115 #define GATT_FORMAT_SINT48 0x11
116 #define GATT_FORMAT_SINT64 0x12
117 #define GATT_FORMAT_SINT128 0x13
118 #define GATT_FORMAT_FLOAT32 0x14
119 #define GATT_FORMAT_FLOAT64 0x15
120 #define GATT_FORMAT_SFLOAT 0x16
121 #define GATT_FORMAT_FLOAT 0x17
122 #define GATT_FORMAT_DUINT16 0x18
123 #define GATT_FORMAT_UTF8S 0x19
124 #define GATT_FORMAT_UTF16S 0x1a
125 #define GATT_FORMAT_STRUCT 0x1b
126 
127 
132 #define GATT_NS_NONE 0x00
133 #define GATT_NS_BT_SIG 0x01
134 #define GATT_NS_BT_DESC_UNKNOWN 0x0000
135 
137 #define GATT_ALL_SERVICES 0xFFFFFFFF
139 
141 #define GATT_SERVICE 0x00000001
142 
144 #if defined ( TESTMODES )
145  // GATT Test Modes
146  #define GATT_TESTMODE_OFF 0 // Test mode off
147  #define GATT_TESTMODE_NO_RSP 1 // Ignore incoming request
148  #define GATT_TESTMODE_PREPARE_WRITE 2 // Forward Prepare Write Request right away
149  #define GATT_TESTMODE_MAX_MTU_SIZE 3 // Use Max ATT MTU size with Exchange MTU Rsp
150  #define GATT_TESTMODE_CORRUPT_PW_DATA 4 // Corrupt incoming Prepare Write Request data
151 #endif
152 
157 #define GATT_PARAM_NUM_PREPARE_WRITES 0
158 
160 #define PTR_TYPE unsigned int *
163 
166 #define GATT_LOCAL_READ 0xFF
167 #define GATT_LOCAL_WRITE 0xFE
169 
172 /*********************************************************************
173  * VARIABLES
174  */
175 
176 /*********************************************************************
177  * MACROS
178  */
179 
181 #define GATT_NUM_ATTRS( attrs ) ( sizeof( attrs ) / sizeof( gattAttribute_t ) )
182 
184 #define GATT_SERVICE_HANDLE( attrs ) ( (attrs)[0].handle )
185 
187 #define GATT_INCLUDED_HANDLE( attrs, i ) ( *((uint16 *)((attrs)[(i)].pValue)) )
188 
190 #define GATT_CCC_TBL( pValue ) ( (gattCharCfg_t *)(*((PTR_TYPE)(pValue))) )
191 
192 /*********************************************************************
193  * TYPEDEFS
194  */
195 
231 typedef bStatus_t (*pfnGATTReadAttrCB_t)( uint16 connHandle, gattAttribute_t *pAttr,
232  uint8 *pValue, uint16 *pLen, uint16 offset,
233  uint16 maxLen, uint8 method );
234 
266 typedef bStatus_t (*pfnGATTWriteAttrCB_t)( uint16 connHandle, gattAttribute_t *pAttr,
267  uint8 *pValue, uint16 len, uint16 offset,
268  uint8 method );
280 typedef bStatus_t (*pfnGATTAuthorizeAttrCB_t)( uint16 connHandle, gattAttribute_t *pAttr,
281  uint8 opcode );
282 
289 typedef struct
291 {
292  uint8 format;
293  int8 exponent;
294  uint16 unit;
295  uint8 nameSpace;
296  uint16 desc;
298 
300 typedef struct
301 {
302  uint16 connHandle;
303  uint8 value;
304 } gattCharCfg_t;
305 
312 typedef struct
313 {
318 
320 typedef struct
321 {
323  uint16 connHandle;
324  uint8 method;
326 
333 typedef struct
334 {
336  uint16 connHandle;
337  uint8 method;
338  uint16 attrHandle;
339  uint16 value;
341 
342 
344 typedef struct
345 {
346  uint16 connHandle;
349 
351 typedef struct
352 {
353  uint16 handle;
356 
358 typedef struct _serviceCBsList
359 {
363 
364 
365 /*********************************************************************
366  * VARIABLES
367  */
368 
371 
374 
377 /*********************************************************************
378  * API FUNCTIONS
379  */
380 
387 extern void GATTServApp_RegisterForMsg( uint8 taskID );
388 
405  uint16 numAttrs, uint8 encKeySize,
406  CONST gattServiceCBs_t *pServiceCBs );
407 
422 bStatus_t GATTServApp_DeregisterService( uint16 handle, gattAttribute_t **p2pAttrs );
423 
436  uint16 numAttrs, uint8 *pValue );
448 extern bStatus_t GATTServApp_AddService( uint32 services );
449 
459 extern bStatus_t GATTServApp_DelService( uint32 services );
460 
477 extern bStatus_t GATTServApp_SetParameter( uint8 param, uint8 len, void *pValue );
478 
491 extern bStatus_t GATTServApp_GetParameter( uint8 param, void *pValue );
492 
507 extern bStatus_t GATTServApp_UpdateCharCfg( uint16 connHandle, uint16 attrHandle, uint16 value );
508 
521 extern void GATTServApp_InitCharCfg( uint16 connHandle, gattCharCfg_t *charCfgTbl );
522 
538 extern uint16 GATTServApp_ReadCharCfg( uint16 connHandle, gattCharCfg_t *charCfgTbl );
539 
556 extern uint8 GATTServApp_WriteCharCfg( uint16 connHandle, gattCharCfg_t *charCfgTbl, uint16 value );
557 
576 extern bStatus_t GATTServApp_ProcessCCCWriteReq( uint16 connHandle, gattAttribute_t *pAttr,
577  uint8 *pValue, uint16 len, uint16 offset,
578  uint16 validCfg );
579 
598 extern bStatus_t GATTServApp_ProcessCharCfg( gattCharCfg_t *charCfgTbl, uint8 *pValue,
599  uint8 authenticated, gattAttribute_t *attrTbl,
600  uint16 numAttrs, uint8 taskId,
601  pfnGATTReadAttrCB_t pfnReadAttrCB );
602 
611 extern void GATTServApp_SendCCCUpdatedEvent( uint16 connHandle, uint16 attrHandle, uint16 value );
612 
626 extern bStatus_t GATTServApp_SendServiceChangedInd( uint16 connHandle, uint8 taskId );
627 
645 extern uint8 GATTServApp_ReadAttr( uint16 connHandle, gattAttribute_t *pAttr,
646  uint16 service, uint8 *pValue, uint16 *pLen,
647  uint16 offset, uint16 maxLen, uint8 method );
648 
662 extern uint8 GATTServApp_WriteAttr( uint16 connHandle, uint16 handle,
663  uint8 *pValue, uint16 len, uint16 offset,
664  uint8 method );
665 
679 extern bStatus_t GATTServApp_ReadRsp( uint16 connHandle, uint8 *pValue,
680  uint16 pLen, uint16 offset );
681 
688 extern void GATTServApp_SetParamValue( uint16 value );
689 
695 extern uint16 GATTServApp_GetParamValue( void );
696 
697 /*-------------------------------------------------------------------
698  * TASK API - These functions must only be called by OSAL.
699  */
700 
702 
713 extern void GATTServApp_Init( uint8 taskId );
714 
726 extern uint16 GATTServApp_ProcessEvent( uint8 taskId, uint16 events );
727 
737 extern pfnGATTAuthorizeAttrCB_t gattServApp_FindAuthorizeAttrCB( uint16 handle );
738 
749 extern bStatus_t gattServApp_EnqueuePrepareWriteReq( uint16 connHandle, attPrepareWriteReq_t *pReq );
750 
762 extern bStatus_t gattServApp_ProcessWriteLong( gattMsgEvent_t *pMsg, prepareWrites_t *pQueue, uint16 *pErrHandle );
763 
775 extern bStatus_t gattServApp_ProcessReliableWrites( gattMsgEvent_t *pMsg, prepareWrites_t *pQueue, uint16 *pErrHandle );
776 
790 extern bStatus_t gattServApp_buildReadByTypeRsp( uint16 connHandle, uint8 *pAttrValue, uint16 attrLen, uint16 attrHandle );
791 
801 extern prepareWrites_t *gattServApp_FindPrepareWriteQ( uint16 connHandle );
802 
813 extern uint8 gattServApp_IsWriteLong( attExecuteWriteReq_t *pReq, prepareWrites_t *pQueue );
814 
822 extern void gattServApp_ClearPrepareWriteQ( prepareWrites_t *pQueue );
823 
825 
826 /*********************************************************************
827 *********************************************************************/
828 
829 #ifdef __cplusplus
830 }
831 #endif
832 
833 #endif /* GATTSERVAPP_H */
834 
uint16 GATTServApp_GetParamValue(void)
Get a GATT Server Application Parameter value.
GATT Structure for Characteristic Presentation Format Value.
Definition: gattservapp.h:290
This API allows the software components in the Z-Stack to be written independently of the specifics o...
uint16 connHandle
Connection message was received on.
Definition: gattservapp.h:323
gattServiceCBsInfo_t serviceInfo
service handle/callbacks
Definition: gattservapp.h:361
GATT Server App event header format.
Definition: gattservapp.h:320
void GATTServApp_SetParamValue(uint16 value)
Set a GATT Server Application Parameter value. Use this function to change the default GATT parameter...
gattAttribute_t * GATTServApp_FindAttr(gattAttribute_t *pAttrTbl, uint16 numAttrs, uint8 *pValue)
Find the attribute record within a service attribute table for a given attribute value pointer...
pfnGATTAuthorizeAttrCB_t pfnAuthorizeAttrCB
Authorization callback function pointer.
Definition: gattservapp.h:316
Service callbacks list item.
Definition: gattservapp.h:358
void GATTServApp_SendCCCUpdatedEvent(uint16 connHandle, uint16 attrHandle, uint16 value)
Build and send the GATT_CLIENT_CHAR_CFG_UPDATED_EVENT to the application.
uint16 handle
Service handle - assigned internally by GATT Server.
Definition: gattservapp.h:353
Structure to keep Prepare Write Requests for each Client.
Definition: gattservapp.h:344
bStatus_t GATTServApp_GetParameter(uint8 param, void *pValue)
Get a GATT Server parameter.
pfnGATTWriteAttrCB_t pfnWriteAttrCB
Write callback function pointer.
Definition: gattservapp.h:315
prepareWrites_t * prepareWritesTbl
Server Prepare Write table (one entry per each physical link)
GATT Structure to keep CBs information for each service being registered.
Definition: gattservapp.h:351
uint8 value
Characteristic configuration value for this client.
Definition: gattservapp.h:303
bStatus_t GATTServApp_AddService(uint32 services)
Add function for the GATT Service.
pfnGATTReadAttrCB_t pfnReadAttrCB
Read callback function pointer.
Definition: gattservapp.h:314
bStatus_t(* pfnGATTReadAttrCB_t)(uint16 connHandle, gattAttribute_t *pAttr, uint8 *pValue, uint16 *pLen, uint16 offset, uint16 maxLen, uint8 method)
Callback function prototype to read an attribute value.
Definition: gattservapp.h:231
uint8 format
Format of the value of this characteristic.
Definition: gattservapp.h:292
bStatus_t GATTServApp_ReadRsp(uint16 connHandle, uint8 *pValue, uint16 pLen, uint16 offset)
If a service returns blePending to the read attribute call back invoked from GATTServApp, the service can later respond to with the value to be read using this API.
uint8 GATTServApp_WriteAttr(uint16 connHandle, uint16 handle, uint8 *pValue, uint16 len, uint16 offset, uint8 method)
Write attribute data.
struct _serviceCBsList * next
pointer to next service callbacks record
Definition: gattservapp.h:360
Structure for Client Characteristic Configuration.
Definition: gattservapp.h:300
osal_event_hdr_t hdr
GATT_SERV_MSG_EVENT and status.
Definition: gattservapp.h:322
uint16 connHandle
Client connection handle.
Definition: gattservapp.h:302
bStatus_t GATTServApp_ProcessCharCfg(gattCharCfg_t *charCfgTbl, uint8 *pValue, uint8 authenticated, gattAttribute_t *attrTbl, uint16 numAttrs, uint8 taskId, pfnGATTReadAttrCB_t pfnReadAttrCB)
Process Client Characteristic Configuration change.
uint16 GATTServApp_ReadCharCfg(uint16 connHandle, gattCharCfg_t *charCfgTbl)
Read the client characteristic configuration for a given client.
void GATTServApp_RegisterForMsg(uint8 taskID)
Register your task ID to receive event messages from the GATT Server Application. ...
attPrepareWriteReq_t * pPrepareWriteQ
Prepare Write Request queue.
Definition: gattservapp.h:347
void GATTServApp_InitCharCfg(uint16 connHandle, gattCharCfg_t *charCfgTbl)
Initialize the client characteristic configuration table.
uint16 value
attribute new value
Definition: gattservapp.h:339
uint16 connHandle
Connection message was received on.
Definition: gattservapp.h:336
Type definitions and macros for BLE stack.
bStatus_t GATTServApp_SetParameter(uint8 param, uint8 len, void *pValue)
Set a GATT Server parameter.
bStatus_t GATTServApp_SendServiceChangedInd(uint16 connHandle, uint8 taskId)
Send out a Service Changed Indication.
bStatus_t GATTServApp_DelService(uint32 services)
Delete function for the GATT Service.
uint16 connHandle
connection message was received on
Definition: gattservapp.h:346
uint16 attrHandle
attribute handle
Definition: gattservapp.h:338
serviceCBsList_t * serviceCBsList
Callbacks for services.
OSAL Event Header.
Definition: osal.h:92
GATT_CLIENT_CHAR_CFG_UPDATED_EVENT message format.
Definition: gattservapp.h:333
uint16 unit
Unit of this attribute as defined in the data dictionary.
Definition: gattservapp.h:294
uint8 nameSpace
Name space of the description.
Definition: gattservapp.h:295
struct _serviceCBsList serviceCBsList_t
Service callbacks list item.
GATT GATT_MSG_EVENT message format.
Definition: gatt.h:211
uint8 method
GATT type of command. Ref: GATT Server Message IDs.
Definition: gattservapp.h:324
bStatus_t GATTServApp_RegisterService(gattAttribute_t *pAttrs, uint16 numAttrs, uint8 encKeySize, CONST gattServiceCBs_t *pServiceCBs)
Register a service's attribute list and callback functions with the GATT Server Application.
bStatus_t GATTServApp_ProcessCCCWriteReq(uint16 connHandle, gattAttribute_t *pAttr, uint8 *pValue, uint16 len, uint16 offset, uint16 validCfg)
Process the client characteristic configuration write request for a given client. ...
osal_event_hdr_t hdr
GATT_SERV_MSG_EVENT and status.
Definition: gattservapp.h:335
GATT Attribute format.
Definition: gatt.h:240
Status_t bStatus_t
BLE Generic Status return.
Definition: bcomdef.h:227
CONST gattServiceCBs_t * pCBs
Service callback function pointers.
Definition: gattservapp.h:354
uint16 desc
Description of this attribute as defined in a higher layer profile.
Definition: gattservapp.h:296
Prepare Write Request format.
Definition: att.h:542
uint8 method
GATT_CLIENT_CHAR_CFG_UPDATED_EVENT.
Definition: gattservapp.h:337
int8 exponent
A sign integer which represents the exponent of an integer.
Definition: gattservapp.h:293
bStatus_t GATTServApp_UpdateCharCfg(uint16 connHandle, uint16 attrHandle, uint16 value)
Update the Client Characteristic Configuration for a given Client.
uint8 GATTServApp_WriteCharCfg(uint16 connHandle, gattCharCfg_t *charCfgTbl, uint16 value)
Write the client characteristic configuration for a given client.
GATT Structure for service callback functions.
Definition: gattservapp.h:312
bStatus_t(* pfnGATTAuthorizeAttrCB_t)(uint16 connHandle, gattAttribute_t *pAttr, uint8 opcode)
Callback function prototype to authorize a Read or Write operation on a given attribute.
Definition: gattservapp.h:280
Execute Write Request format.
Definition: att.h:568
bStatus_t GATTServApp_DeregisterService(uint16 handle, gattAttribute_t **p2pAttrs)
Deregister a service's attribute list and callback functions from the GATT Server Application...
bStatus_t(* pfnGATTWriteAttrCB_t)(uint16 connHandle, gattAttribute_t *pAttr, uint8 *pValue, uint16 len, uint16 offset, uint8 method)
Callback function prototype to write an attribute value.
Definition: gattservapp.h:266
uint8 GATTServApp_ReadAttr(uint16 connHandle, gattAttribute_t *pAttr, uint16 service, uint8 *pValue, uint16 *pLen, uint16 offset, uint16 maxLen, uint8 method)
Read an attribute. If the format of the attribute value is unknown to GATT Server, use the callback function provided by the Service.
Copyright 2017, Texas Instruments Incorporated