TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Structures | Macros | Typedefs | Functions | Variables
gattservapp.h File Reference

Detailed Description

GATTServApp layer interface.

Go to the source code of this file.

Data Structures

struct  _serviceCBsList
 Service callbacks list item. More...
 
struct  gattCharCfg_t
 Structure for Client Characteristic Configuration. More...
 
struct  gattCharFormat_t
 GATT Structure for Characteristic Presentation Format Value. More...
 
struct  gattClientCharCfgUpdatedEvent_t
 GATT_CLIENT_CHAR_CFG_UPDATED_EVENT message format. More...
 
struct  gattEventHdr_t
 GATT Server App event header format. More...
 
struct  gattServiceCBs_t
 GATT Structure for service callback functions. More...
 
struct  gattServiceCBsInfo_t
 GATT Structure to keep CBs information for each service being registered. More...
 
struct  prepareWrites_t
 Structure to keep Prepare Write Requests for each Client. More...
 

Macros

#define GATT_ALL_SERVICES   0xFFFFFFFF
 All profile services bit fields.
 
#define GATT_CCC_TBL(pValue)   ( (gattCharCfg_t *)(*((PTR_TYPE)(pValue))) )
 Client Characteristic Configuration table (from CCC attribute value pointer)
 
#define GATT_CFG_NO_OPERATION   0x0000
 No operation.
 
#define GATT_CLIENT_CFG_INDICATE   0x0002
 The Characteristic Value shall be indicated.
 
#define GATT_CLIENT_CFG_NOTIFY   0x0001
 The Characteristic Value shall be notified.
 
#define GATT_CLIENT_CHAR_CFG_UPDATED_EVENT   0x00
 Sent when a Client Characteristic Configuration is updated. This event is sent as an OSAL message defined as gattCharCfgUpdatedEvent_t.
 
#define GATT_EXT_PROP_RELIABLE_WRITE   0x0001
 Permits reliable writes of the Characteristic Value.
 
#define GATT_EXT_PROP_WRITABLE_AUX   0x0002
 Permits writes to the characteristic descriptor.
 
#define GATT_FORMAT_2BIT   0x02
 Unsigned 2 bit integer.
 
#define GATT_FORMAT_BOOL   0x01
 Unsigned 1 bit; 0 = false, 1 = true.
 
#define GATT_FORMAT_DUINT16   0x18
 IEEE-20601 format.
 
#define GATT_FORMAT_FLOAT   0x17
 IEEE-11073 32 bit FLOAT.
 
#define GATT_FORMAT_FLOAT32   0x14
 IEEE-754 32 bit floating point.
 
#define GATT_FORMAT_FLOAT64   0x15
 IEEE-754 64 bit floating point.
 
#define GATT_FORMAT_NIBBLE   0x03
 Unsigned 4 bit integer.
 
#define GATT_FORMAT_SFLOAT   0x16
 IEEE-11073 16 bit SFLOAT.
 
#define GATT_FORMAT_SINT12   0x0d
 Signed 12 bit integer.
 
#define GATT_FORMAT_SINT128   0x13
 Signed 128 bit integer.
 
#define GATT_FORMAT_SINT16   0x0e
 Signed 16 bit integer.
 
#define GATT_FORMAT_SINT24   0x0f
 Signed 24 bit integer.
 
#define GATT_FORMAT_SINT32   0x10
 Signed 32 bit integer.
 
#define GATT_FORMAT_SINT48   0x11
 Signed 48 bit integer.
 
#define GATT_FORMAT_SINT64   0x12
 Signed 64 bit integer.
 
#define GATT_FORMAT_SINT8   0x0c
 Signed 8 bit integer.
 
#define GATT_FORMAT_STRUCT   0x1b
 Opaque structure.
 
#define GATT_FORMAT_UINT12   0x05
 Unsigned 12 bit integer.
 
#define GATT_FORMAT_UINT128   0x0b
 Unsigned 128 bit integer.
 
#define GATT_FORMAT_UINT16   0x06
 Unsigned 16 bit integer.
 
#define GATT_FORMAT_UINT24   0x07
 Unsigned 24 bit integer.
 
#define GATT_FORMAT_UINT32   0x08
 Unsigned 32 bit integer.
 
#define GATT_FORMAT_UINT48   0x09
 Unsigned 48 bit integer.
 
#define GATT_FORMAT_UINT64   0x0a
 Unsigned 64 bit integer.
 
#define GATT_FORMAT_UINT8   0x04
 Unsigned 8 bit integer.
 
#define GATT_FORMAT_UTF16S   0x1a
 UTF-16 string.
 
#define GATT_FORMAT_UTF8S   0x19
 UTF-8 string.
 
#define GATT_INCLUDED_HANDLE(attrs, i)   ( *((uint16 *)((attrs)[(i)].pValue)) )
 The handle of the first included service (i = 1) is the value of the second attribute.
 
#define GATT_LOCAL_READ   0xFF
 GATT local read.
 
#define GATT_LOCAL_WRITE   0xFE
 GATT local write.
 
#define GATT_NS_BT_DESC_UNKNOWN   0x0000
 The description is unknown.
 
#define GATT_NS_BT_SIG   0x01
 Bluetooth SIG namespace.
 
#define GATT_NS_NONE   0x00
 No namespace.
 
#define GATT_NUM_ATTRS(attrs)   ( sizeof( attrs ) / sizeof( gattAttribute_t ) )
 The number of attribute records in a given attribute table.
 
#define GATT_PARAM_NUM_PREPARE_WRITES   0
 RW uint8.
 
#define GATT_PROP_AUTHEN   0x40
 Permits signed writes to the Characteristic Value.
 
#define GATT_PROP_BCAST   0x01
 Permits broadcasts of the Characteristic Value.
 
#define GATT_PROP_EXTENDED   0x80
 Additional characteristic properties are defined in the Characteristic Extended Properties Descriptor.
 
#define GATT_PROP_INDICATE   0x20
 Permits indications of a Characteristic Value with acknowledgement.
 
#define GATT_PROP_NOTIFY   0x10
 Permits notifications of a Characteristic Value without acknowledgement.
 
#define GATT_PROP_READ   0x02
 Permits reads of the Characteristic Value.
 
#define GATT_PROP_WRITE   0x08
 Permits writes of the Characteristic Value with response.
 
#define GATT_PROP_WRITE_NO_RSP   0x04
 Permits writes of the Characteristic Value without response.
 
#define GATT_SERV_CFG_BCAST   0x0001
 The Characteristic Value shall be broadcast when the server is in the broadcast procedure if advertising data resources are available.
 
#define GATT_SERVICE   0x00000001
 GATT Services bit fields.
 
#define GATT_SERVICE_HANDLE(attrs)   ( (attrs)[0].handle )
 The handle of a service is the handle of the first attribute.
 

Typedefs

typedef bStatus_t(* pfnGATTAuthorizeAttrCB_t) (uint16 connHandle, gattAttribute_t *pAttr, uint8 opcode)
 Callback function prototype to authorize a Read or Write operation on a given attribute. More...
 
typedef bStatus_t(* pfnGATTReadAttrCB_t) (uint16 connHandle, gattAttribute_t *pAttr, uint8 *pValue, uint16 *pLen, uint16 offset, uint16 maxLen, uint8 method)
 Callback function prototype to read an attribute value. More...
 
typedef bStatus_t(* pfnGATTWriteAttrCB_t) (uint16 connHandle, gattAttribute_t *pAttr, uint8 *pValue, uint16 len, uint16 offset, uint8 method)
 Callback function prototype to write an attribute value. More...
 
typedef struct _serviceCBsList serviceCBsList_t
 Service callbacks list item.
 

Functions

bStatus_t GATTServApp_AddService (uint32 services)
 Add function for the GATT Service. More...
 
bStatus_t GATTServApp_DelService (uint32 services)
 Delete function for the GATT Service. More...
 
bStatus_t GATTServApp_DeregisterService (uint16 handle, gattAttribute_t **p2pAttrs)
 Deregister a service's attribute list and callback functions from the GATT Server Application. More...
 
gattAttribute_t * GATTServApp_FindAttr (gattAttribute_t *pAttrTbl, uint16 numAttrs, uint8 *pValue)
 Find the attribute record within a service attribute table for a given attribute value pointer. More...
 
bStatus_t GATTServApp_GetParameter (uint8 param, void *pValue)
 Get a GATT Server parameter. More...
 
uint16 GATTServApp_GetParamValue (void)
 Get a GATT Server Application Parameter value. More...
 
void GATTServApp_InitCharCfg (uint16 connHandle, gattCharCfg_t *charCfgTbl)
 Initialize the client characteristic configuration table. More...
 
bStatus_t GATTServApp_ProcessCCCWriteReq (uint16 connHandle, gattAttribute_t *pAttr, uint8 *pValue, uint16 len, uint16 offset, uint16 validCfg)
 Process the client characteristic configuration write request for a given client. More...
 
bStatus_t GATTServApp_ProcessCharCfg (gattCharCfg_t *charCfgTbl, uint8 *pValue, uint8 authenticated, gattAttribute_t *attrTbl, uint16 numAttrs, uint8 taskId, pfnGATTReadAttrCB_t pfnReadAttrCB)
 Process Client Characteristic Configuration change. More...
 
uint8 GATTServApp_ReadAttr (uint16 connHandle, gattAttribute_t *pAttr, uint16 service, uint8 *pValue, uint16 *pLen, uint16 offset, uint16 maxLen, uint8 method)
 Read an attribute. If the format of the attribute value is unknown to GATT Server, use the callback function provided by the Service. More...
 
uint16 GATTServApp_ReadCharCfg (uint16 connHandle, gattCharCfg_t *charCfgTbl)
 Read the client characteristic configuration for a given client. More...
 
bStatus_t GATTServApp_ReadRsp (uint16 connHandle, uint8 *pValue, uint16 pLen, uint16 offset)
 If a service returns blePending to the read attribute call back invoked from GATTServApp, the service can later respond to with the value to be read using this API. More...
 
void GATTServApp_RegisterForMsg (uint8 taskID)
 Register your task ID to receive event messages from the GATT Server Application. More...
 
bStatus_t GATTServApp_RegisterService (gattAttribute_t *pAttrs, uint16 numAttrs, uint8 encKeySize, CONST gattServiceCBs_t *pServiceCBs)
 Register a service's attribute list and callback functions with the GATT Server Application. More...
 
void GATTServApp_SendCCCUpdatedEvent (uint16 connHandle, uint16 attrHandle, uint16 value)
 Build and send the GATT_CLIENT_CHAR_CFG_UPDATED_EVENT to the application. More...
 
bStatus_t GATTServApp_SendServiceChangedInd (uint16 connHandle, uint8 taskId)
 Send out a Service Changed Indication. More...
 
bStatus_t GATTServApp_SetParameter (uint8 param, uint8 len, void *pValue)
 Set a GATT Server parameter. More...
 
void GATTServApp_SetParamValue (uint16 value)
 Set a GATT Server Application Parameter value. Use this function to change the default GATT parameter values. More...
 
bStatus_t GATTServApp_UpdateCharCfg (uint16 connHandle, uint16 attrHandle, uint16 value)
 Update the Client Characteristic Configuration for a given Client. More...
 
uint8 GATTServApp_WriteAttr (uint16 connHandle, uint16 handle, uint8 *pValue, uint16 len, uint16 offset, uint8 method)
 Write attribute data. More...
 
uint8 GATTServApp_WriteCharCfg (uint16 connHandle, gattCharCfg_t *charCfgTbl, uint16 value)
 Write the client characteristic configuration for a given client. More...
 

Variables

prepareWrites_t * prepareWritesTbl
 Server Prepare Write table (one entry per each physical link)
 
serviceCBsList_t * serviceCBsList
 Callbacks for services.
 
Copyright 2017, Texas Instruments Incorporated