Data Fields
SHA2CC26X2_Object_ Struct Reference

SHA2CC26XX Object. More...

#include <SHA2CC26X2.h>

Data Fields

bool isOpen
 
int_fast16_t returnStatus
 
SHA2_ReturnBehavior returnBehavior
 
uint32_t semaphoreTimeout
 
SHA2_CallbackFxn callbackFxn
 
SHA2_Operation operation
 
SHA2_OperationType operationType
 
SwiP_Struct callbackSwi
 

Detailed Description

SHA2CC26XX Object.

The application must not access any member variables of this structure!

Field Documentation

§ isOpen

bool SHA2CC26X2_Object_::isOpen

§ returnStatus

int_fast16_t SHA2CC26X2_Object_::returnStatus

§ returnBehavior

SHA2_ReturnBehavior SHA2CC26X2_Object_::returnBehavior

§ semaphoreTimeout

uint32_t SHA2CC26X2_Object_::semaphoreTimeout

§ callbackFxn

SHA2_CallbackFxn SHA2CC26X2_Object_::callbackFxn

§ operation

SHA2_Operation SHA2CC26X2_Object_::operation

§ operationType

SHA2_OperationType SHA2CC26X2_Object_::operationType

§ callbackSwi

SwiP_Struct SHA2CC26X2_Object_::callbackSwi

The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated