Data Fields
SHA2CC26X2_HWAttrs_ Struct Reference

SHA2CC26XX Hardware Attributes. More...

#include <SHA2CC26X2.h>

Data Fields

uint8_t intPriority
 Crypto Peripheral's interrupt priority. More...
 
uint32_t swiPriority
 SHA2 SWI priority. The higher the number, the higher the priority. The minimum is 0 and the maximum is 15 by default. The maximum can be reduced to save RAM by adding or modifying Swi.numPriorities in the kernel configuration file. More...
 

Detailed Description

SHA2CC26XX Hardware Attributes.

SHA226XX hardware attributes should be included in the board file and pointed to by the SHA2_config struct.

Field Documentation

§ intPriority

uint8_t SHA2CC26X2_HWAttrs_::intPriority

Crypto Peripheral's interrupt priority.

The CC26xx uses three of the priority bits, meaning ~0 has the same effect as (7 << 5).

(7 << 5) will apply the lowest priority.

(1 << 5) will apply the highest priority.

Setting the priority to 0 is not supported by this driver.

HWI's with priority 0 ignore the HWI dispatcher to support zero-latency interrupts, thus invalidating the critical sections in this driver.

§ swiPriority

uint32_t SHA2CC26X2_HWAttrs_::swiPriority

SHA2 SWI priority. The higher the number, the higher the priority. The minimum is 0 and the maximum is 15 by default. The maximum can be reduced to save RAM by adding or modifying Swi.numPriorities in the kernel configuration file.


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated