![]() |
![]() |
NVS attributes. More...
#include <NVS.h>
Data Fields | |
| void * | regionBase |
| size_t | regionSize |
| size_t | sectorSize |
NVS attributes.
The address of an NVS_Attrs structure is passed to NVS_getAttrs().
'regionBase' is the base address of the region if directly accessible by the MCU. If the flash region is within external flash (e.g., SPI flash), this field will be set to NVS_REGION_NOT_ADDRESSABLE.
'regionSize' is the size, in bytes, of the NVS region that the application chooses to manage.
'sectorSize' is the size of the sector erase page. This attribute is device specific.
| void* NVS_Attrs::regionBase |
| size_t NVS_Attrs::regionSize |
Base address of flash region to manage
| size_t NVS_Attrs::sectorSize |
Region size (in bytes)