![]() |
![]() |
Format of LCD commands used by the LCD controller. More...
#include <LCDDogm1286.h>
Data Fields | |
| char | displayStartLine |
| char | adcSet |
| char | outputMode |
| char | displayType |
| char | lcdBias |
| char | powerControl |
| char | boosterRadio0 |
| char | boosterRadio1 |
| char | contrastSet0 |
| char | contrastSet1 |
| char | contrastSet2 |
| char | staticIndicator0 |
| char | staticIndicator1 |
| char | displayEn |
| char | setPage |
| char | columnHi |
| char | columnLo |
Format of LCD commands used by the LCD controller.
| char LCD_Command::displayStartLine |
| char LCD_Command::adcSet |
| char LCD_Command::outputMode |
| char LCD_Command::displayType |
| char LCD_Command::lcdBias |
| char LCD_Command::powerControl |
| char LCD_Command::boosterRadio0 |
| char LCD_Command::boosterRadio1 |
| char LCD_Command::contrastSet0 |
| char LCD_Command::contrastSet1 |
| char LCD_Command::contrastSet2 |
| char LCD_Command::staticIndicator0 |
| char LCD_Command::staticIndicator1 |
| char LCD_Command::displayEn |
| char LCD_Command::setPage |
| char LCD_Command::columnHi |
| char LCD_Command::columnLo |