![]() |
![]() |
I2C Parameters. More...
#include <I2C.h>
Data Fields | |
| I2C_TransferMode | transferMode |
| I2C_CallbackFxn | transferCallbackFxn |
| I2C_BitRate | bitRate |
| void * | custom |
I2C Parameters.
I2C parameters are used with the I2C_open() call. Default values for these parameters are set using I2C_Params_init().
If I2C_TransferMode is set to I2C_MODE_BLOCKING, I2C_transfer() function calls will block thread execution until the transaction has completed. In this case, the transferCallbackFxn parameter will be ignored.
If I2C_TransferMode is set to I2C_MODE_CALLBACK, I2C_transfer() will not block thread execution, but it will call the function specified by transferCallbackFxn upon transfer completion. Sequential calls to I2C_transfer() in I2C_MODE_CALLBACK will put the I2C_Transaction structures onto an internal queue that automatically starts queued transactions after the previous transaction has completed. This queuing occurs regardless of any error state from previous transactions.
I2C_BitRate specifies the I2C bus rate used for I2C communications.
| I2C_TransferMode I2C_Params_::transferMode |
Blocking or Callback mode
| I2C_CallbackFxn I2C_Params_::transferCallbackFxn |
Callback function pointer
| I2C_BitRate I2C_Params_::bitRate |
I2C bus bit rate
| void* I2C_Params_::custom |
Custom argument used by driver implementation