![]() |
![]() |
ECC Parameters. More...
#include <ECDH.h>
Data Fields | |
| ECDH_ReturnBehavior | returnBehavior |
| ECDH_CallbackFxn | callbackFxn |
| uint32_t | timeout |
| void * | custom |
ECC Parameters.
ECC Parameters are used to with the ECDH_open() call. Default values for these parameters are set using ECDH_Params_init().
| ECDH_ReturnBehavior ECDH_Params_::returnBehavior |
Blocking, callback, or polling return behavior
| ECDH_CallbackFxn ECDH_Params_::callbackFxn |
Callback function pointer
| uint32_t ECDH_Params_::timeout |
Timeout of the operation
| void* ECDH_Params_::custom |
Custom argument used by driver implementation