#include <DisplaySharp.h>
§ spiIndex
| uint32_t DisplaySharp_HWAttrs::spiIndex |
§ csPin
| PIN_Id DisplaySharp_HWAttrs::csPin |
§ extcominPin
| PIN_Id DisplaySharp_HWAttrs::extcominPin |
§ powerPin
| PIN_Id DisplaySharp_HWAttrs::powerPin |
§ enablePin
| PIN_Id DisplaySharp_HWAttrs::enablePin |
§ pixelHeight
| uint16_t DisplaySharp_HWAttrs::pixelHeight |
§ pixelWidth
| uint16_t DisplaySharp_HWAttrs::pixelWidth |
§ displayBuf
| void* DisplaySharp_HWAttrs::displayBuf |
The documentation for this struct was generated from the following file: