Data Fields
AESCCMCC26XX_Object Struct Reference

AESCCMCC26XX Object. More...

#include <AESCCMCC26XX.h>

Data Fields

bool isOpen
 
int8_t macVerifyResult
 
AESCCM_ReturnBehavior returnBehavior
 
AESCCM_OperationType operationType
 
uint32_t semaphoreTimeout
 
AESCCM_CallbackFxn callbackFxn
 
AESCCM_Operationoperation
 
SwiP_Struct callbackSwi
 

Detailed Description

AESCCMCC26XX Object.

The application must not access any member variables of this structure!

Field Documentation

§ isOpen

bool AESCCMCC26XX_Object::isOpen

§ macVerifyResult

int8_t AESCCMCC26XX_Object::macVerifyResult

§ returnBehavior

AESCCM_ReturnBehavior AESCCMCC26XX_Object::returnBehavior

§ operationType

AESCCM_OperationType AESCCMCC26XX_Object::operationType

§ semaphoreTimeout

uint32_t AESCCMCC26XX_Object::semaphoreTimeout

§ callbackFxn

AESCCM_CallbackFxn AESCCMCC26XX_Object::callbackFxn

§ operation

AESCCM_Operation* AESCCMCC26XX_Object::operation

§ callbackSwi

SwiP_Struct AESCCMCC26XX_Object::callbackSwi

The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated