class="memitem:ad4ba613e4bb4c308046385069649380a">bool isProtected  

Detailed Description

ADCCC26XX Object.

The application must not access any member variables of this structure!

Field Documentation

§ pinState

PIN_State ADCCC26XX_Object::pinState

Pin state object

§ pinHandle

PIN_Handle ADCCC26XX_Object::pinHandle

Pin handle

§ isOpen

bool ADCCC26XX_Object::isOpen

Flag if the instance is in use

§ isProtected

bool ADCCC26XX_Object::isProtected

Flag to indicate if thread safety is ensured by the driver


The documentation for this struct was generated from the following file: Copyright 2017, Texas Instruments Incorporated