![]() |
![]() |
ADC Parameters. More...
#include <ADCBuf.h>
Data Fields | |
| uint32_t | blockingTimeout |
| uint32_t | samplingFrequency |
| ADCBuf_Return_Mode | returnMode |
| ADCBuf_Callback | callbackFxn |
| ADCBuf_Recurrence_Mode | recurrenceMode |
| void * | custom |
ADC Parameters.
ADC Parameters are used to with the ADCBuf_open() call. Default values for these parameters are set using ADCBuf_Params_init().
| uint32_t ADCBuf_Params_::blockingTimeout |
Timeout for semaphore in ADCBuf_RETURN_MODE_BLOCKING
| uint32_t ADCBuf_Params_::samplingFrequency |
The frequency at which the ADC will produce a sample
| ADCBuf_Return_Mode ADCBuf_Params_::returnMode |
Return mode for all conversions