Modules | Macros
ECJPAKE_control command and status codes

Modules

 Status Codes
 
 Command Codes
 

Macros

#define ECJPAKE_CMD_RESERVED   (32)
 
#define ECJPAKE_STATUS_RESERVED   (-32)
 

Detailed Description

These ECJPAKE macros are reservations for ECJPAKE.h

Macro Definition Documentation

§ ECJPAKE_CMD_RESERVED

#define ECJPAKE_CMD_RESERVED   (32)

Common ECJPAKE_control command code reservation offset. ECJPAKE driver implementations should offset command codes with ECJPAKE_CMD_RESERVED growing positively

Example implementation specific command codes:

#define ECJPAKEXYZ_CMD_COMMAND0 ECJPAKE_CMD_RESERVED + 0
#define ECJPAKEXYZ_CMD_COMMAND1 ECJPAKE_CMD_RESERVED + 1

§ ECJPAKE_STATUS_RESERVED

#define ECJPAKE_STATUS_RESERVED   (-32)

Common ECJPAKE_control status code reservation offset. ECJPAKE driver implementations should offset status codes with ECJPAKE_STATUS_RESERVED growing negatively.

Example implementation specific status codes:

#define ECJPAKEXYZ_STATUS_ERROR0 ECJPAKE_STATUS_RESERVED - 0
#define ECJPAKEXYZ_STATUS_ERROR1 ECJPAKE_STATUS_RESERVED - 1
#define ECJPAKEXYZ_STATUS_ERROR2 ECJPAKE_STATUS_RESERVED - 2
Copyright 2017, Texas Instruments Incorporated