|
bStatus_t | GAPBondMgr_FindAddr (uint8_t *pDevAddr, GAP_Peer_Addr_Types_t addrType, uint8_t *pIdx, GAP_Peer_Addr_Types_t *pIdentityAddrType, uint8_t *pIdentityAddr) |
| Search for an address in the bonding table. If the address is a random private resolvable address, attempt to resolve the random address against all IRK's in bonding table. As output parameters, return the following: More...
|
|
bStatus_t | GAPBondMgr_GetParameter (uint16_t param, void *pValue) |
|
bStatus_t | GAPBondMgr_Pair (uint16_t connHandle) |
|
bStatus_t | GAPBondMgr_PasscodeRsp (uint16_t connectionHandle, uint8_t status, uint32_t passcode) |
|
void | GAPBondMgr_Register (gapBondCBs_t *pCB) |
|
bStatus_t | GAPBondMgr_ServiceChangeInd (uint16_t connectionHandle, uint8_t setParam) |
|
bStatus_t | GAPBondMgr_SetParameter (uint16_t param, uint8_t len, void *pValue) |
|
This module implements the GAP Bond Manager
§ GAPBondMgr_FindAddr()
Search for an address in the bonding table. If the address is a random private resolvable address, attempt to resolve the random address against all IRK's in bonding table. As output parameters, return the following:
- index into bonding table if the address (or resolved address) is found
- identity address type if a resolved address was found. Only valid if the input address is random private resolvable
- identity address if a resolved address was found. Only valid if the input address is random private resolvable
Note that the output parameters are optional. If it is not desired for them to be returned, a NULL pointer can safely be passed.
- Parameters
-
pDevAddr | peer's address |
addrType | peer's address type |
pIdx | pointer to byte to put the bond index if found |
pIdentityAddrType | pointer to byte to put the identity address type if applicable |
pIdentityAddr | pointer to buffer to put the identity address type if applicable |
- Returns
- SUCCESS if the address was found or resolved to an address in the bonding table
-
INVALIDPARAMETER if a NULL address is passed in
-
bleGAPNotFound if the address was not found and didn't resolve to any addresses in the bonding table
§ GAPBondMgr_GetParameter()
bStatus_t GAPBondMgr_GetParameter |
( |
uint16_t |
param, |
|
|
void * |
pValue |
|
) |
| |
Get a GAP Bond Manager parameter.
- Note
- The "pValue" field must point to a "uint16_t".
- Parameters
-
param | Profile parameter ID: GAP Bond Manager Parameters |
pValue | pointer to location to get the value. This is dependent on the parameter ID and WILL be cast to the appropriate data type (example: data type of uint16_t will be cast to uint16_t pointer). |
- Returns
- SUCCESS
-
INVALIDPARAMETER
§ GAPBondMgr_Pair()
bStatus_t GAPBondMgr_Pair |
( |
uint16_t |
connHandle | ) |
|
Start (or re-start) the pairing process
This API can be used to initiate pairing in cases where it is not started automatically by the gapbondmgr or to re-pair after the initial pairing has occurred if, for example, the pairing requirements have changed.
- Note
- Pairing will occur automatically if GAPBOND_PAIRING_MODE is set to GAPBOND_PAIRING_MODE_INITIATE or GAPBOND_PAIRING_MODE is set to GAPBOND_PAIRING_MODE_WAIT_FOR_REQ and a pairing request is received. In these cases, this API is not needed and will fail since pairing is already in progress.
- Parameters
-
connHandle | connection handle to initiate pairing with |
- Returns
- SUCCESS
-
bleAlreadyInRequestedMode already pairing
§ GAPBondMgr_PasscodeRsp()
bStatus_t GAPBondMgr_PasscodeRsp |
( |
uint16_t |
connectionHandle, |
|
|
uint8_t |
status, |
|
|
uint32_t |
passcode |
|
) |
| |
Respond to a passcode request.
- Parameters
-
connectionHandle | connection handle of the connected device or 0xFFFF if all devices in database. |
status | SUCCESS if passcode is available, otherwise see Pairing failure status values. |
passcode | integer value containing the passcode. |
- Returns
- SUCCESS bond record found and changed,
-
bleIncorrectMode Link not found.
-
INVALIDPARAMETER : passcode is out of range
-
bleMemAllocError : heap is out of memory
§ GAPBondMgr_Register()
Register callback functions with the bond manager.
- Parameters
-
pCB | pointer to callback function structure. |
§ GAPBondMgr_ServiceChangeInd()
bStatus_t GAPBondMgr_ServiceChangeInd |
( |
uint16_t |
connectionHandle, |
|
|
uint8_t |
setParam |
|
) |
| |
Set/clear the service change indication in a bond record.
- Parameters
-
connectionHandle | connection handle of the connected device or 0xFFFF if all devices in database. |
setParam | TRUE to set the service change indication, FALSE to clear it. |
- Returns
- SUCCESS bond record found and changed,
-
bleNoResources bond record not found
-
bleNotConnected connection not found connectionHandle is invalid (for non-0xFFFF connectionHandle).
§ GAPBondMgr_SetParameter()
bStatus_t GAPBondMgr_SetParameter |
( |
uint16_t |
param, |
|
|
uint8_t |
len, |
|
|
void * |
pValue |
|
) |
| |
Set a GAP Bond Manager parameter.
- Note
- The "len" field must be set to the size of a "uint16_t" and the "pValue" field must point to a "uint16_t".
- Parameters
-
param | GAP Bond Manager Parameters |
len | length of data to write |
pValue | pointer to data to write. This is dependent on the parameter ID and WILL be cast to the appropriate data type (example: data type of uint16_t will be cast to uint16_t pointer). |
- Returns
- SUCCESS
-
INVALIDPARAMETER