14.2. Hector SLAM Application
SLAM (Simultaneous Localization and Mapping) is a critical technology in Robotics applications. It helps map unknown environment and localize a robot using a pre-built map. There are many open-source SLAM algorithms with camera and 2D/3D Lidar and they can run on J7 in Docker container. For example, in this demo, it is demonstrated how to build and run Hector SLAM on J7 in Docker container. 2D Lidar data, which was collected from TurtleBot3 is provided for this demo.
Figure 1 shows the output map by Hector SLAM on the 2D Lidar data from TurtleBot3. For more details on Hector SLAM, please refer to http://wiki.ros.org/hector_slam.
14.2.1. How to Run the Hector SLAM Application
14.2.1.1. Run the Hector SLAM on J7
Download 2D Lidar data.
root@am6x-sk:~/j7ros_home$ make lidar2d_download
2D Lidar data is saved in $HOME/j7ros_home/data/lidar2d.
Clone the Hector SLAM git repository. Run the followings on the J7 host Linux:
root@am6x-sk:~/j7ros_home$ export SLAM_ROOT=/opt/robotics_sdk/ros1/slam root@am6x-sk:~/j7ros_home$ $SLAM_ROOT/j7_setup_hector_slam.sh
It clones the Hector SLAM git repository and applies the patch to run it on the 2D Lidar data provided.
Launch the Docker image. For setting up the ROS 1 environment on J7 host, please follow Docker Setup for ROS 1.
root@am6x-sk:~/j7ros_home$ ./docker_run_ros1.sh
Compile the Hector SLAM inside the Docker container:
root@am6x-sk:~/j7ros_home/ros_ws$ catkin_make --source /opt/robotics_sdk/ros1 --force-cmake
Run the hector SLAM
root@am6x-sk:~/j7ros_home/ros_ws$ roslaunch hector_slam_launch tutorial_j7.launch
14.2.1.2. Visualize map and pose on Ubuntu PC
For setting up the ROS 1 environment on the remote PC, please follow Docker Setup for ROS 1.
As done on the J7 host Linux, clone the Hector SLAM git repository:
user@pc:~/j7ros_home$ export SLAM_ROOT=$HOME/j7ros_home/ros_ws/src/robotics_sdk/ros1/slam user@pc:~/j7ros_home$ $SLAM_ROOT/j7_setup_hector_slam.sh
Launch the Docker image.
user@pc:~/j7ros_home$ ./docker_run_ros1.sh
Compile the Hector SLAM:
root@pc-docker:~/j7ros_home/ros_ws$ catkin_make --source ./src/robotics_sdk/ros1/slam/hector_slam
To display map and pose, run:
root@pc-docker:~/j7ros_home/ros_ws$ roslaunch hector_slam_launch map_rviz.launch