13. Visual Localization

This application performs the ego vehicle localization that estimates an ego vehicle’s 6-DOF (Degree of Freedom) pose from calibrated camera images using a 3D sparse map created offline. The 3D sparse map consists of a set of key points with (X, Y, Z) positions and 64-dimensional descriptors. To localize the ego vehicle’s pose, key points are detected with descriptors from the input camera image and these key points are matched against the key points in the map. The ego vehicle’s pose is estimated using the Perspective-n-Point (PnP) approach.

Key-point descriptor plays critical role in the visual localization. In this demo, we use a deep neural network to learn hand computed feature descriptor like KAZE in a supervised manner. We refer such descriptor as DKAZE. The DAKZE network was used to create key features and their descriptors for the sparse 3D map and is also used to detect key feature points with descriptors for every input image in the localization process. For more details about the DKAZE network and the localization process, refer to Vision Apps User Guide.

For this demo, we provide the data set that has been created using Carla simulator. This data set includes an input rosbag file and the sparse 3D map crated offline, etc. The input rosbag file consists of a sequence of images in YUV422 (UYVY) format. Since the sparse 3D map should cover the area where the input image is being captured for localization. This demo does not work for live camera input with the provided sparse 3D map.

Figure 1. Visual Localization demo: block diagram

13.1. How to Run the Application in ROS 1

13.1.1. Run the Visual Localization Demo

[J7] For setting up the ROS 1 environment on J7 host, please follow Docker Setup for ROS 1. To launch ti_vl node with playing back a ROSBAG file, run the following inside the Docker container on J7 target:

roslaunch ti_vl bag_visloc.launch

[Visualization on Ubuntu PC] For setting up the ROS 1 environment on remote PC, please follow Docker Setup for ROS 1.

To display the top-down image with overlaid vehicle trajectory and pose in 3D space using RViz on PC, run:

roslaunch ti_viz_nodes rviz_visloc.launch

13.2. Launch File Parameters

Parameter

Description

Value

rosparam file

Algorithm configuration parameters (see “ROSPARAM Parameters” section)

config/params.yaml

input_topic

Subscribe topic name for input camera image

camera/image_raw

out_image_topic

Publish topic name topic for top-down image with overlaid vehicle trajectory

vis_localize/out_image

out_pose_topic

Publish topic name topic for vehicle pose

vis_localize/pose

map_topic

Publish topic name for feature points in offline map

vis_localize/map

exportPerfStats

Flag for exporting the performance data to a file: 0 - disable, 1 - enable

0, 1

13.3. ROSPARM Parameters

13.3.1. Basic input, DL model Parameters

Parameter

Description

Value

input_format

Input image format, 0: YUV420, 1: YUV422

0, 1

lut_file_path

LDC rectification table path

String

dl_model_path

Path to the feature detection DL model

String

width

Input image width

Integer

height

Input image height

Integer

out_width

Output semantic segmentation output (tensor) width

Integer

out_height

Output semantic segmentation output (tensor) height

Integer

pipeline_depth

OpenVX graph pipeline depth

1 ~ 8

13.3.2. Visual Localization Parameters

The following shows the parameters necessary for visual localization. The default values are for the test data from a Carla simulator that we provide.

Parameter

Description

Value

top_view_img_path

Path to top-down view image, on which vehicle trajectory is overlaid

String

input_voxel_info_path

Path to voxel info binary file

String

input_map_feat_pt_path

Path to binary file that has map key points’ 3D position

String

input_map_feat_desc_path

Path to binary file that has map key points’ descriptor

String

input_upsample_wt_path

Path to binary file that has upsampling coefficients for descriptor

String

input_upsample_bias_path

Path to binary file that has upsampling bias for descriptor

String

score_th

Score threshold for picking good key points

Integer

num_map_feat:

Number of key points in a map

Integer

max_frame_feat

Max number of key points for a frame

Integer

num_voxels

Number of voxels

Integer

filter_scale_pw2

Scale of filter coefficients for input_upsample_wt_path

Integer

hi_res_desc_scale_pw2

Scale of descriptors for input_map_feat_desc_path

Integer

pose_calc_skip_flag

Pose calculation skip flag (Should be 0)

0, 1

13.4. Processing Blocks

Referring to Figure 1, below are the descriptions of the processing blocks implemented in this application:

  1. The first step is to process input images. J7 LDC (Lens Distortion Correction) hardware accelerator (HWA) changes image format as well a removes lens distortion. The input format to the application is YUV422 (UYVY) format. It is converted to YUV420 (NV12) by the LDC.

  2. Input images are resized to a smaller resolution, which is specified by dl_width and dl_height in params.yaml, for the DKAZE network. The MSC (Multi-Scaler) HWA resizes the images to a desired size.

  3. The pre-processing block converts YUV420 (NV12) to RGB, which is expected input format for the DKAZE network.

  4. The DKAZE network is accelerated by C7x/MMA with DLR runtime, and outputs feature score tensor and feature descriptor tensor.

  5. Two output tensors from the DAKZE network go to the pose calculation (PoseCalc) block, which runs on C6x. This block estimates the ego-vehicle’s pose.

  6. The estimate pose goes to the pose visualization (PoseViz) block, which runs on C6x too. This block creates the top-down output image with overlaid vehicle’s trajectory. This output image is published along with the estimated pose.

13.5. Known Issues

  1. The provided sparse 3D map is for the input bag file we provide. Both the input bag file and the sparse 3D map are created using CARLA simulator. Since the sparse 3D map should cover the area where the input image is being captured for localization. This demo does not work for live camera input with the provided sparse 3D map.