ZED Stereo Camera ROS Node

ZED stereo camera ROS node based on OpenCV VideoCapture API for publishing left and right raw images and their camera_info.

Usage

  1. Obtain the factory camera calibration data file for your ZED camera with a script provided. Find the serial number of the ZED camera. The serial number can be found on the ZED camera box.

    ./script/download_calib_file.sh <serial_number>
    

    where <serial_number> is the serial number of the ZED camera.

    Then place the downloaded calibration data file (SNxxxx.conf) under config folder.

  2. Generate camera_info YAML files, and undistortion & rectification look-up-table (LUT) files which are required in offloading the undistortion/rectification on J7 VPAC/LDC hardware accelerator.

    Run the following script:

    python2 ./script/generate_rect_map.py -i SNxxxx.conf -m <camera_mode>
    

    where

    • SNxxxx.conf is the factory calibration data file obtained from Step 1, and

    • <camera_mode> is camera mode. Valid <camera_mode>: 2K, FHD, HD, HD2, VGA (see Launch File Parameters section for description). If the -m argument is not provided, by default the tool will iterate for the following three camera modes: HD, HD2, and FHD.

    This script parses the calibration data and generates the following files:

    • config/<SN_string>_<camera_mode>_camera_info_{left,right}.yaml: camera_info for left and right raw image,

    • config/<SN_string>_<camera_mode>_remap_LUT_{left,right}.bin: undistortion and rectification remap LUT for left and right raw images.

  3. Update launch/zed_capture.launch to modify zed_sn_str parameter. Also update relevant parameters in nodes/*/params.yaml files for each of demo applications.

  4. Build the ZED camera ROS node

    cd $CATKIN_WS
    catkin_make
    source devel/setup.bash
    
  5. Launch the ZED camera node

    roslaunch zed_capture zed_capture.launch
    

Launch File Parameters

Parameter Description Value
zed_sn_str ZED camera serial number string string
device_name camera device name. Typically /dev/video2 on the target with TI Edge AI string
camera_mode ZED camera mode '2K' (2208x1242)
_ _ 'FHD' (1920x1080)
_ _ 'HD' (1280x720)
_ _ 'HD2' (1280x720)*
_ _ 'VGA' (672x376)
frame_rate frame rate at which raw images are published int
encoding image encoding 'yuv422' (default) or 'bgr8'

‘HD2’ is a newly added mode that provides 720p resolution for experiments that need a longer focal length than the native ‘HD’. The images are obtained by center-cropping the original 1080p images captured from the ‘FHD’ mode.

When encoding is set to ‘yuv422’, the pixel format YUV422::YUYV from the ZED camera is converted to YUV422::UYVY format considering the compatibility with LDC hardware accelerator.

Data Collection Steps

  1. Connect the ZED camera to UBS 3 port (a USB type-A to type-C adaptor is required on J7 EVM). Check if the camera is recognized with ls /dev/video*. In a Ubuntu PC with a built-in webcam, the stereo camera can be recognized as /dev/video2.

  2. If necessary, update launch/zed_capture.launch to change video device, camera mode, frame rate, and etc.

  3. On the first terminal, launch the ZED capture node with following, and keep it running:

    $ roslaunch zed_capture zed_capture.launch
    
  4. On the second terminal, to capture into ROS bag files, run one of two examples below

    # Collect 15 seconds of data and stop itself
    $ roslaunch zed_capture recordbag.launch
    # Save into a series of bag files, each keeping 15 seconds of data, until terminated with Ctrl+C
    $ roslaunch zed_capture recordbag_split.launch
    
  5. (Optional to check the ROS topics) On 3rd terminal,

    $ rostopic list
    $ rqt_image_view /camera/left/image_raw
    

By default, ROS bag files are stored under ${HOME}/.ros folder.

Note: It is not recommended combining the zed_capture node and ROSBAG capture into a single launch file, since it takes some several seconds for the ZED camera to settle down its ISP tuning after the ZED camera node is started.