Robotics Software Development Kit¶
TI Robotics Development Framework¶

The TI Robotics Software Development Kit (SDK) runs in a Docker container environment on J7 Processor SDK Linux provided with TI Edge AI base image. We provide detailed steps for setting a Docker container environment for ROS Melodic along with the TI Vision Apps Library (see next section). The Robotics SDK allows:
Optimized software implementation of computation-intensive software blocks (including deep-learning, vision, perception, and ADAS) on deep-learning core (C7x/MMA), DSP cores, hardware accelerators built-in on the Jacinto 7 processors.
Application software can be complied directly on the Jacinto 7 target using APIs optimized on the Jacinto 7 cores and hardware accelerators along with many open-source libraries and packages including, for example, OpenCV, Point-Cloud Library (PCL), and many more.
Figure below is a representative deep-learning and compute-intensive application developed with the TI Robotics SDK.
TI Vision Apps Library¶
TI Vision Apps Library is a set of APIs for the target deployment that are derived from the Jacinto 7 Processor SDK RTOS which includes:
TI OpenVX kernels and infrastructure
TI deep-learning (TIDL) applications
Imaging and vision applications
Advanced driver-assistance systems (ADAS) applications
Perception applications
The TI Vision Apps Library is included in the pre-built base image for TI Edge AI Development Kit 0.5.
Open-Source Deep-Learning Runtime¶
The Edge AI Development Kit 0.5 also supports the following open-source deep-learning runtime:
TVM/Neo-AI-DLR
TFLite Runtime
ONNX Runtime
For more details on open-source deep-learning runtime on J7/TDA4x, please check TI Edge AI Cloud. We provides two demo applications that include a deep-learning model that is implemented in the TVM/Neo-AI-DLR framework.
Setting Up Robotics SDK Docker Container Environment¶
See Setting Up Robotics SDK Environment
Note: git.ti.com has some issue in rendering markdown files. We highly recommend to use the section in the User Guide Documentation
Sensor Driver Nodes¶
Change Log¶
See CHANGELOG.md
Limitations and Known Issues¶
RViz visualization is displayed on a remote Ubuntu PC.
Ctrl+C termination of a ROS node or a ROS launch session can be sometimes slow.
Stereo Vision Demo
Output disparity map may have artifacts that are common to block-based stereo algorithms. e.g., noise in the sky, texture-less area, repeated patterns, etc.
While the confidence map from SDE has 8 values between 0 (least confident) to 7 (most confident), the confidence map from the multi-layer SDE refinement has only 2 values, 0 and 7. Therefore, it would not appear as fine as the SDE’s confidence map.
The semantic segmentation model used in
ti_semseg_cnnandti_estopnodes was trained with Cityscapes dataset first, and re-trained with a small dataset collected from a particular stereo camera (ZED camera, HD mode) for a limited scenarios with coarse annotation. Therefore, the model can show limited accuracy performance if a different camera model is used and/or when it is applied to different environment scenes.