VXLIB Build Process

Back

 

VXLIB is provided with concerto makefile-based compilation/link (build).

The following can be built using the make command (along with specific targets).

 

GNU Makefile

A concerto based makefile is provided for rebuilding VXLIB libraries via the GNU make utility. This file is located in the top folder. The makefile provides a list of all tools, common build utilities and build rules required for generating VXLIB libraries.

Follow the instructions at GNU Make Build Process for more details.

 

Copyright 2025, Texas Instruments Incorporated