BAM Plugins (not currently supported on J7 SOCs)

Back

 

Some selected VXLIB kernels also contain a bam_plugin folder which contains the files necessary to plugin the respective kernel into the BAM block based processing framework. In order to build the bam_plugin library, DMAUTILS_INSTALL_DIR should be defined in the make system due to dependent header files. Currently, these bam plugins are utilized to provide DMA acceleration of VXLIB kernels within the TI OpenVX (TIOVX) framework. If VXLIB is not being used in conjuction with TIOVX, then the bam_plugins can be ignored and left unused.

This table lists each VXLIB kernel and indicates if it has BAM plugin support. The plugin files are located in the bam_plugin folder in each kernel directory.

Kernel BAM Plugin Support
VXLIB_absDiff_i16s_i16s_o16s YES
VXLIB_absDiff_i8u_i8u_o8u YES
VXLIB_accumulateImage_i8u_io16s
VXLIB_accumulateSquareImage_i8u_io16s
VXLIB_accumulateWeightedImage_i8u_io8u
VXLIB_add_i16s_i16s_o16s YES
VXLIB_add_i8u_i8u_o8u YES
VXLIB_add_i8u_i16s_o16s YES
VXLIB_add_i8u_i8u_o16s YES
VXLIB_addSquare_i8u_i16s_o16s YES
VXLIB_addWeight_i8u_i8u_o8u YES
VXLIB_and_i8u_i8u_o8u YES
VXLIB_box_3x3_i8u_o8u YES
VXLIB_cannyNMS_i16s_i16s_i16u_o8u YES
VXLIB_channelCopy_1to1_i8u_o8u YES
VXLIB_channelCombine_2to1_i8u_o8u YES
VXLIB_channelCombine_3to1_i8u_o8u YES
VXLIB_channelCombine_4to1_i8u_o8u YES
VXLIB_channelCombine_yuyv_i8u_o8u YES
VXLIB_channelExtract_1of2_i8u_o8u YES
VXLIB_channelExtract_1of3_i8u_o8u YES
VXLIB_channelExtract_1of4_i8u_o8u YES
VXLIB_colorConvert_IYUVtoNV12_i8u_o8u YES
VXLIB_colorConvert_IYUVtoRGB_i8u_o8u YES
VXLIB_colorConvert_IYUVtoRGBX_i8u_o8u YES
VXLIB_colorConvert_IYUVtoYUV4_i8u_o8u YES
VXLIB_colorConvert_NVXXtoIYUV_i8u_o8u YES
VXLIB_colorConvert_NVXXtoRGB_i8u_o8u YES
VXLIB_colorConvert_NVXXtoRGBX_i8u_o8u YES
VXLIB_colorConvert_NVXXtoYUV4_i8u_o8u YES
VXLIB_colorConvert_RGBtoIYUV_i8u_o8u YES
VXLIB_colorConvert_RGBtoNV12_i8u_o8u YES
VXLIB_colorConvert_RGBtoRGBX_i8u_o8u YES
VXLIB_colorConvert_RGBtoYUV4_i8u_o8u YES
VXLIB_colorConvert_RGBXtoIYUV_i8u_o8u YES
VXLIB_colorConvert_RGBXtoNV12_i8u_o8u YES
VXLIB_colorConvert_RGBXtoRGB_i8u_o8u YES
VXLIB_colorConvert_RGBXtoYUV4_i8u_o8u YES
VXLIB_colorConvert_YUVXtoIYUV_i8u_o8u YES
VXLIB_colorConvert_YUVXtoNV12_i8u_o8u YES
VXLIB_colorConvert_YUVXtoRGB_i8u_o8u YES
VXLIB_colorConvert_YUVXtoRGBX_i8u_o8u YES
VXLIB_convertDepth_i16s_o8u YES
VXLIB_convertDepth_i8u_o16s YES
VXLIB_convolve_3x3_i8u_c16s_o16s
VXLIB_convolve_3x3_i8u_c16s_o8u
VXLIB_convolve_5x5_i8u_c16s_o16s
VXLIB_convolve_5x5_i8u_c16s_o8u
VXLIB_convolve_7x7_i8u_c16s_o16s
VXLIB_convolve_7x7_i8u_c16s_o8u
VXLIB_convolve_i8u_c16s_o16s YES
VXLIB_convolve_i8u_c16s_o8u YES
VXLIB_dilate_3x3_i8u_o8u YES
VXLIB_dilate_MxN_i8u_i8u_o8u YES
VXLIB_doubleThreshold_i16u_i8u YES
VXLIB_edgeTracing_i8u
VXLIB_equalizeHist_i8u_o8u
VXLIB_erode_3x3_i8u_o8u YES
VXLIB_erode_MxN_i8u_i8u_o8u YES
VXLIB_fastCorners_i8u
VXLIB_fastCornersDetect_i8u
VXLIB_fastCornersScore_i8u
VXLIB_fastCornersNMS_i8u
VXLIB_gaussian_3x3_i8u_o8u YES
VXLIB_gaussian_5x5_br_i8u_o8u
VXLIB_gaussian_5x5_i8u_o8u
VXLIB_halfScaleGaussian_5x5_i8u_o8u YES
VXLIB_halfScaleGaussian_5x5_i8u_o8u_o8u
VXLIB_halfScaleGaussian_5x5_br_i8u_o8u_o8u
VXLIB_harrisCornersDetect_i32f
VXLIB_harrisCornersNMS_i32f
VXLIB_harrisCornersScore_i16s_i16s_o32f YES
VXLIB_harrisCornersScore_i32s_i32s_o32f YES
VXLIB_histogram_i8u_o32u YES
VXLIB_histogramCdfLut_i32u_o8u
VXLIB_histogramSimple_i8u_o32u YES
VXLIB_integralImage_i8u_o32u YES
VXLIB_magnitude_i16s_i16s_o16s YES
VXLIB_meanStdDev_i8u_o32f YES
VXLIB_median_3x3_i8u_o8u YES
VXLIB_median_MxN_i8u_i8u_o8u YES
VXLIB_minMaxLoc_i16s YES
VXLIB_minMaxLoc_i8u YES
VXLIB_multiply_i16s_i16s_o16s YES
VXLIB_multiply_i8u_i8u_o8u YES
VXLIB_multiply_i8u_i16s_o16s YES
VXLIB_multiply_i8u_i8u_o16s YES
VXLIB_normL1_i16s_i16s_o16u YES
VXLIB_normL2_i16s_i16s_o16u YES
VXLIB_not_i8u_o8u YES
VXLIB_or_i8u_i8u_o8u YES
VXLIB_phase_i16s_i16s_o8u YES
VXLIB_remapBilinear_bc_i8u_i32f_o8u
VXLIB_remapNearest_bc_i8u_i32f_o8u
VXLIB_scaleImageBilinear_i8u_o8u
VXLIB_scaleImageBilinear_bc_i8u_o8u
VXLIB_scaleImageBilinear_br_i8u_o8u
VXLIB_scaleImageNearest_i8u_o8u YES
VXLIB_scharr_3x3_i8u_o16s_o16s
VXLIB_sobelX_3x3_i8u_o16s YES
VXLIB_sobelY_3x3_i8u_o16s YES
VXLIB_sobel_3x3_i8u_o16s_o16s YES
VXLIB_sobel_5x5_i8u_o16s_o16s YES
VXLIB_sobel_7x7_i8u_o16s_o16s YES
VXLIB_sobel_7x7_i8u_o32s_o32s YES
VXLIB_subtract_i16s_i16s_o16s YES
VXLIB_subtract_i8u_i8u_o8u YES
VXLIB_subtract_i8u_i16s_o16s YES
VXLIB_subtract_i8u_i8u_o16s YES
VXLIB_tableLookup_i16s_o16s YES
VXLIB_tableLookup_i8u_o8u YES
VXLIB_thresholdBinary_i8u_o8u YES
VXLIB_thresholdRange_i8u_o8u YES
VXLIB_trackFeaturesLK_i8u
VXLIB_warpAffineBilinear_bc_i8u_c32f_o8u
VXLIB_warpAffineBilinear_i8u_c32f_o8u
VXLIB_warpAffineNearest_bc_i8u_c32f_o8u
VXLIB_warpAffineNearest_i8u_c32f_o8u
VXLIB_warpPerspectiveBilinear_bc_i8u_c32f_o8u
VXLIB_warpPerspectiveBilinear_i8u_c32f_o8u
VXLIB_warpPerspectiveNearest_bc_i8u_c32f_o8u
VXLIB_warpPerspectiveNearest_i8u_c32f_o8u
VXLIB_xor_i8u_i8u_o8u YES

Copyright 2025, Texas Instruments Incorporated