TIOVX User Guide
vx_parameter.h File Reference

Implementation of Parameter object. More...

Go to the source code of this file.

Data Structures

struct  tivx_parameter_t
 Parameter object internal state. More...
 

Functions

vx_bool ownIsValidDirection (vx_enum dir)
 This returns true if the direction is a valid enum. More...
 
vx_bool ownIsValidTypeMatch (vx_enum expected, vx_enum supplied)
 This returns true if the supplied type matches the expected type with some fuzzy rules.
 
vx_bool ownIsValidState (vx_enum state)
 This returns true if the supplied state is a valid enum.
 

Detailed Description

Implementation of Parameter object.

Definition in file vx_parameter.h.