TIOVX User Guide
|
Implementation of Meta Format Object. More...
Go to the source code of this file.
Data Structures | |
struct | tivx_meta_format_t |
Meta Format object internal state. More... | |
Functions | |
vx_status | ownReleaseMetaFormat (vx_meta_format *meta) |
Releases a meta-format object. More... | |
vx_meta_format | ownCreateMetaFormat (vx_context context) |
Creates a metaformat object. More... | |
vx_bool | ownIsMetaFormatEqual (vx_meta_format meta1, vx_meta_format meta2, vx_enum ref_type) |
Check for equivalence between two meta format objects. More... | |
Implementation of Meta Format Object.
Definition in file vx_meta_format.h.
vx_status ownReleaseMetaFormat | ( | vx_meta_format * | meta | ) |
Releases a meta-format object.
[in] | meta | meta format object |
vx_meta_format ownCreateMetaFormat | ( | vx_context | context | ) |
Creates a metaformat object.
[in] | context | The overall context object. |
vx_bool ownIsMetaFormatEqual | ( | vx_meta_format | meta1, |
vx_meta_format | meta2, | ||
vx_enum | ref_type | ||
) |
Check for equivalence between two meta format objects.
This API is used to check for equivalence between two meta format objects. The function returns true if they are equal and false if not.
[in] | meta1 | First meta format object to be compared. |
[in] | meta2 | Second meta format object to be compared. |
[in] | ref_type | Type of both meta format objects to be compared. Note: this must be the same for each meta object. This information cannot be extracted from the meta object because the type gets set at verify time and this could be called prior. |