![]() |
TIOVX User Guide
|
The OpenVX Bidirectional Parameters extension API. More...
#include <VX/vx.h>Go to the source code of this file.
Enumerations | |
| enum | vx_bidirectional_enum_e |
| Extra enums. | |
Functions | |
| vx_node VX_API_CALL | vxAccumulateImageNode (vx_graph graph, vx_image input, vx_image accum) |
| [Graph] Creates an accumulate node. More... | |
| VX_API_ENTRY vx_node VX_API_CALL | vxAccumulateWeightedImageNodeX (vx_graph graph, vx_image input, vx_float32 alpha, vx_image accum) |
| [Graph] Creates a weighted accumulate node. More... | |
| VX_API_ENTRY vx_node VX_API_CALL | vxAccumulateSquareImageNodeX (vx_graph graph, vx_image input, vx_uint32 shift, vx_image accum) |
| [Graph] Creates an accumulate square node. More... | |
The OpenVX Bidirectional Parameters extension API.
Definition in file vx_khr_bidirectional_parameters.h.