TIOVX User Guide
|
Implementation of Image object. More...
Go to the source code of this file.
Data Structures | |
struct | tivx_image_map_info_t |
Information about a image mapping. More... | |
struct | tivx_image_t |
Image object internal state. More... | |
Functions | |
vx_status | ownInitVirtualImage (vx_image img, vx_uint32 width, vx_uint32 height, vx_df_image format) |
function to initialize virtual image's parameters More... | |
uint32_t | ownImageGetBufferSize (tivx_obj_desc_image_t *obj_desc) |
function to retreive the buffer size of an image More... | |
Implementation of Image object.
Definition in file vx_image.h.