TIOVX User Guide
|
Platform APIs. More...
#include <tivx_obj_desc_priv.h>
Go to the source code of this file.
Data Structures | |
struct | tivx_shm_obj_count_t |
Struct containing object descriptor allocation counts. Allows for a log to be kept of the object descriptors used throughout runtime. More... | |
Enumerations | |
enum | tivx_platform_lock_type_e { TIVX_PLATFORM_LOCK_OBJ_DESC_TABLE = 0, TIVX_PLATFORM_LOCK_CONTEXT, TIVX_PLATFORM_LOCK_DATA_REF_QUEUE, TIVX_PLATFORM_LOCK_LOG_RT_INDEX, TIVX_PLATFORM_LOCK_LOG_RT, TIVX_PLATFORM_LOCK_MAX } |
Types of system level locks. More... | |
Functions | |
int32_t | tivxPlatformGetShmSize (uint32_t *shm_size) |
Get size of TIOVX object descriptor memory carveout. More... | |
void | ownTableIncrementValue (vx_enum resource_name) |
Increment count of given resource. More... | |
void | ownTableDecrementValue (vx_enum resource_name) |
Decrement count of given resource. More... | |
vx_enum | ownPlatformGetTargetId (const char *target_name) |
Convert a target name to a specific target ID. More... | |
void | ownPlatformGetTargetName (vx_enum target_id, char *target_name) |
Convert a specific target ID to a target name. More... | |
vx_bool | ownPlatformTargetMatch (const char *kernel_target_name, const char *target_string) |
Match a user specified target_string with kernel suported target name. More... | |
void | ownPlatformGetObjDescTableInfo (tivx_obj_desc_table_info_t *table_info) |
Return shared memory info which holds the object descriptors. More... | |
void | ownPlatformGetLogRtShmInfo (void **shm_base, uint32_t *shm_size) |
Return shared memory info which holds the run-time logger buffer. More... | |
void | ownPlatformSystemLock (vx_enum lock_id) |
Take a system level lock. More... | |
void | ownPlatformSystemUnlock (vx_enum lock_id) |
Release system level lock. | |
vx_status | ownPlatformInit (void) |
Init Platform module. | |
void | ownPlatformDeInit (void) |
DeInit Platform module. | |
void | ownPlatformPrintf (const char *format) |
Print given string. | |
void | ownPlatformCreateTargets (void) |
Function to set the target configuration. More... | |
void | ownPlatformDeleteTargets (void) |
Function to destroy created targets. | |
void | ownPlatformActivate (void) |
Utility function to enable Platform specific things Currently Used for EVE algorithm to enable EDMA. | |
void | ownPlatformDeactivate (void) |
Utility function to disable Platform specific things Currently Used for EVE algorithm to disable EDMA. | |
void | ownPlatformTaskInit (void) |
Utility function to call OS-specific task init functions. | |
Platform APIs.
Definition in file tivx_platform.h.