TIOVX User Guide
|
Implementation of Object descriptor Queue Object APIs. More...
Go to the source code of this file.
Functions | |
vx_status | ownObjDescQueueCreate (uint16_t *obj_desc_id) |
Create a object descriptor queue and return its obj_desc_id. | |
vx_status | ownObjDescQueueRelease (uint16_t *obj_desc_id) |
Release a object descriptor queue. | |
vx_status | ownObjDescQueueEnqueue (uint16_t obj_desc_q_id, uint16_t obj_desc_id) |
Enqueue a obj_desc_id into a object descriptor queue. | |
vx_status | ownObjDescQueueGetCount (uint16_t obj_desc_q_id, uint32_t *count) |
Get number of elements in a object descriptor queue. | |
vx_status | ownObjDescQueueDequeue (uint16_t obj_desc_q_id, uint16_t *obj_desc_id) |
Dequeue a obj_desc_id from a object descriptor queue. | |
vx_status | ownObjDescQueueAddBlockedNode (uint16_t obj_desc_q_id, uint16_t node_id) |
Add 'node_id' to a list of blocked nodes associated with this object descriptor ID. | |
vx_status | ownObjDescQueueExtractBlockedNodes (uint16_t obj_desc_q_id, tivx_obj_desc_queue_blocked_nodes_t *out_blocked_nodes) |
Extract nodes blocked on this object descriptor queue ID. More... | |
Implementation of Object descriptor Queue Object APIs.
NOTE: The APIs in this module dont do any locking for Q/DQ and other operations. User of this API should take local CPU and/or multi-CPU locks
Definition in file tivx_obj_desc_queue.h.
vx_status ownObjDescQueueExtractBlockedNodes | ( | uint16_t | obj_desc_q_id, |
tivx_obj_desc_queue_blocked_nodes_t * | out_blocked_nodes | ||
) |
Extract nodes blocked on this object descriptor queue ID.
Adds to out_blocked_nodes, make sure out_blocked_nodes->num_nodes is set to 0 before calling this API