TIOVX User Guide

Implementation of resource log API. More...

Go to the source code of this file.

Functions

void ownLogResourceInit (void)
 Initialize max value structs.
 
void ownLogResourceDeInit (void)
 De-Initialize max value structs.
 
void ownLogResourceAlloc (const char *resource_name, uint16_t num_allocs)
 Allocate new resource.
 
void ownLogResourceFree (const char *resource_name, uint16_t num_frees)
 Free resource.
 
void ownLogSetResourceUsedValue (const char *resource_name, uint16_t value)
 Set max value of resource.
 

Detailed Description

Implementation of resource log API.

Definition in file tivx_log_resource.h.