TIOVX User Guide
|
Interface file for utility functions for the Kernel. More...
Go to the source code of this file.
Macros | |
#define | TIVX_KERNEL_COMMON_VALID_RECT_MAX_IMAGE (5u) |
Maximum number of images (input/output) supported in calculating valid rectangles. | |
Functions | |
vx_status | tivxPublishKernels (vx_context context, const Tivx_Host_Kernel_List *kernel_list, uint32_t num_kernels) |
Publishes the kernels list on the host side. | |
vx_status | tivxUnPublishKernels (vx_context context, const Tivx_Host_Kernel_List *kernel_list, uint32_t num_kernels) |
Unpublishes the kernels list on the host side. | |
static void | tivxKernelValidRectParams_init (tivxKernelValidRectParams *prms) |
Function to initialize Valid Rect Parameter structure Currently the entire structure is memset to 0. More... | |
vx_status | tivxKernelConfigValidRect (tivxKernelValidRectParams *prms) |
Function to calculate and configure valid region This API loops over all the input and output image's valid rectangles and figures out overlapping rectangle and sets it as valid rectangle in the output image. More... | |
void | tivxKernelsHostUtilsAddKernelTargetDsp (vx_kernel kernel) |
Function to add platform-specific DSP kernel target. More... | |
void | tivxKernelsHostUtilsAddKernelTargetMcu (vx_kernel kernel) |
Function to add platform-specific R5F kernel target. More... | |
Interface file for utility functions for the Kernel.
Definition in file tivx_kernels_host_utils.h.