TIOVX User Guide
|
Interface to Event APIs. More...
Go to the source code of this file.
Macros | |
#define | TIVX_EVENT_TIMEOUT_NO_WAIT (0u) |
Constant to indicate tivxEventPend() should only check and not wait for event to arrive. | |
#define | TIVX_EVENT_TIMEOUT_WAIT_FOREVER (0xFFFFFFFFu) |
Constant to indicate tivxEventPend() should only wait forever for the event to arrive. | |
Typedefs | |
typedef struct tivx_vx_event_t * | tivx_event |
Typedef for a event. | |
Functions | |
vx_status | tivxEventCreate (tivx_event *event) |
Create a event. More... | |
vx_status | tivxEventDelete (tivx_event *event) |
Delete a event. More... | |
vx_status | tivxEventPost (tivx_event event) |
Post a event. More... | |
vx_status | tivxEventWait (tivx_event event, uint32_t timeout) |
Pend on a event. More... | |
vx_status | tivxEventClear (tivx_event event) |
Clear any pending events. More... | |
Interface to Event APIs.
Definition in file tivx_event.h.