TIOVX User Guide
vx_event_user_event Struct Reference

Parameter structure returned with event of type VX_EVENT_USER_EVENT. More...

#include <vx_khr_pipelining.h>

Data Fields

void * user_event_parameter
 User defined parameter value. This is used to pass additional user defined parameters with a user event.
 

Detailed Description

Parameter structure returned with event of type VX_EVENT_USER_EVENT.

Definition at line 420 of file vx_khr_pipelining.h.


The documentation for this struct was generated from the following file: